This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
![]() | ||||||
Develop on Arm® Cortex®-M4 | What's next | |||||
![]() |
Install the IDE | ![]() |
Install STM32Cube MP1 package | ![]() |
Modify, rebuild and reload a firmware | ![]() |
1. Overview[edit source]
This stage will explain you how to modify, rebuild and reload a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.
2. Import an existing example in SW4STM32 IDE[edit source]
- Open System Workbench for STM32 IDE
File:SW4STM32 workspace.png
SW4STM32 workspace
- Open the import screen File > Import... and select Existing Project into Workspace
File:SW4STM32 import.png
SW4STM32 import screen
- Browse and select OpenAMP_TTY_echo application example
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo - Click finish
- The OpenAMP_TTY_echo project is open and you can browse inside using the left pan
File:SW4STM32 workspace project open.png
SW4STM32 workspace with project open
3. Build the example[edit source]
- Click the build button (the little hammer in the toolbar)
File:SW4STM32 workspace project build.png
SW4STM32 build the project
- If the following screen appear, click OK
File:SW4STM32 workspace project warning.png
SW4STM32 Warning: This board already exists
- Build is finished with no error
File:SW4STM32 workspace project build finished.png
SW4STM32 build finished with no error
4. Execute the example[edit source]
5. Modify the example[edit source]
6. Rebuild and reload the example[edit source]
![]() |
![]() |
![]() |