This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleProposedVersion
![]() | ||||||||
Let's start | Develop on Arm® Cortex®-A7 | |||||||
![]() |
Unpack the board | ![]() |
Populate the target and boot the image | ![]() |
Execute basic commands | ![]() |
Use the demo launcher | ![]() |
1. Overview[edit source]
This stage will explain you how to connect the Linux terminal of your board to your host computer through the ST-LINK/V2-1.
Then you will see how to execute basic commands with the Linux command line interface in order to be familiarized with the Linux console.
2. The serial terminal[edit source]
The serial terminal will allow you to communicate with the board trough a UART serial interface.
- Install minicom
sudo apt-get install minicom
- Get the ttyACM device instance that need to be used to access the ST-LINK/V2-1
ls /dev/ttyACM* /dev/ttyACM0
- Connect the minicom to the /dev/ttyACM0 device
minicom -D /dev/ttyACM0 Welcome to minicom 2.7 OPTIONS: I18n Compiled on Nov 15 2018, 20:18:47. Port /dev/ttyACM0, 15:56:03 Press CTRL-A Z for help on special keys
- Press the reset button to reset the board. You should see logs displayed in the minicom window
Put some starting logs here
3. Basic commands[edit source]
3.1. Printing distribution specific information[edit source]
lsb_release -a LSB Version: core-4.1-noarch:core-4.1-arm Distributor ID: openstlinux-weston Description: ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.4+openstlinux-4.14-rocko-mp1-18-11-26 Release: 2.4+openstlinux-4.14-rocko-mp1-18-11-26 Codename: rocko
Where:
LSB Version | Version of LSB (Linux Standard Base) against which distribution is compliant |
Distributor ID | String identifier of distributor |
Description | Single line text description of distribution |
Release | Release number of distribution |
Codename | Codename according to distribution release |
3.2. Printing system information[edit source]
uname -a Linux stm32mp1-boards-rev[b/c] 4.14.48 #1 SMP PREEMPT Tue Nov 27 14:41:52 UTC 2018 armv7l armv7l armv7l GNU/Linux
Where:
Linux | Kernel name |
stm32mp1-boards-rev[b/c] | Network node hostname |
4.14.48 | Kernel release |
#1 SMP PREEMPT Tue Nov 27 14:41:52 UTC 2018 | Kernel version |
armv7l | Machine hardware name |
GNU/Linux | Operating system |
3.3. Printing Linux kernel and GCC versions[edit source]
cat /proc/version Linux version 4.14.48 (xxxx@yyyy) (gcc version 7.3.0 (GCC)) #1 SMP PREEMPT Tue Nov 27 14:41:52 UTC 2018
Where:
Linux | Kernel name |
version 4.14.48 | Kernel release |
(xxxx@yyyy) | Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened |
(gcc version 7.3.0 (GCC) ) | Version of the GCC compiler used to compile the kernel |
#1 SMP PREEMPT Tue Nov 27 14:41:52 UTC 2018 | Kernel version; type of kernel (SMP) and date and time of the kernel compilation |
3.4. Printing the amount of disk space available on all mounted file systems[edit source]
df -h Filesystem Size Used Avail Use% Mounted on /dev/root 719M 347M 334M 52% / devtmpfs 372M 0 372M 0% /dev tmpfs 436M 0 436M 0% /dev/shm tmpfs 436M 14M 423M 4% /run tmpfs 436M 0 436M 0% /sys/fs/cgroup tmpfs 436M 4.0K 436M 1% /tmp /dev/mmcblk0p4 58M 7.7M 46M 15% /boot tmpfs 436M 160K 436M 1% /var/volatile /dev/mmcblk0p7 15G 14G 0 100% /usr/local /dev/mmcblk0p5 15M 8.7M 4.7M 65% /vendor tmpfs 88M 0 88M 0% /run/user/0
Where:
Filesystem | Source of the mount point, usually a device |
Size | Total size in human readable format (e.g. 1K, 234M, 2G) |
Used | Used size in human readable format |
Available | Available size in human readable format |
Use% | Percentage of used size divided by the total size |
Mounted on | Mount point |
3.5. ssh connection (only if Ethernet cable is connected)[edit source]
![]() |
![]() |
![]() |