Last edited 4 years ago

Standard SDK directory structure: Difference between revisions


Latest revision as of 15:12, 15 April 2020

This article describes the structure of the OpenSTLinux standard SDK installation directory:

SDK
├── environment-setup-<target>-<distro>-linux-gnueabi  Environment setup script
├── site-config-<target>-<distro>-linux-gnueabi        Configuration file for the target
├── sysroots                                           Root file systems
│   ├── <target>-<distro>-linux-gnueabi                Target sysroot (libraries, headers, and symbols)
│   │   ├── bin
│   │   ├── boot
│   │   ├── config
│   │   ├── dev
│   │   ├── etc
│   │   ├── home
│   │   ├── lib
│   │   ├── media
│   │   ├── mnt
│   │   ├── proc
│   │   ├── run
│   │   ├── sbin
│   │   ├── sys
│   │   ├── tmp
│   │   ├── usr
│   │   └── var
│   └── <host machine>-<distro>_sdk-linux              Native sysroot (libraries, headers, and symbols)
│       ├── bin
│       ├── environment-setup.d
│       ├── etc
│       ├── lib
│       ├── sbin
│       ├── usr
│       └── var
└── version-<target>-<distro>-linux-gnueabi            Version file for the target

Where:

The installed SDK consists of:

  • an environment setup script for the SDK
  • a configuration file for the target
  • a version file for the target
  • the root file systems (sysroots) needed to develop objects for the target system