Registered User |
Registered User mNo edit summary |
||
(4 intermediate revisions by 2 users not shown) | |||
Line 43: | Line 43: | ||
* Download {{Highlight|latest }} [https://www.st.com/en/development-tools/stm32cubeprog.html#getsoftware-scroll STM32CubeProgrammer] in the following directory<br> '''$HOME/STM32MPU_workspace/tmp''' | * Download {{Highlight|latest }} [https://www.st.com/en/development-tools/stm32cubeprog.html#getsoftware-scroll STM32CubeProgrammer] in the following directory<br> '''$HOME/STM32MPU_workspace/tmp''' | ||
{{Warning | {{EcosystemRelease | revision=2.0.0}} | {{Warning | {{EcosystemRelease | revision=2.0.0| range=and after }} requires STM32CubeProgrammer V2.4 or upper }} | ||
* Uncompress the archive file to get the STM32CubeProgrammer installers | * Uncompress the archive file to get the STM32CubeProgrammer installers | ||
Line 74: | Line 74: | ||
{{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | {{SoftwareLicenseAgreement | distribution=OpenSTLinux}} | ||
======For {{EcosystemRelease | revision=2.1.0}}====== | |||
{{Warning|Only microSD card SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.}} | |||
* Create your STM32MP15 Starter Package directory on your host computer | |||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0 | |||
{{PC$}} mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package | |||
{{PC$}} cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package | |||
* Download the [{{EcosystemRelease/Package | revision=2.1.0| package=Images package | request=url}}/{{EcosystemRelease/Package | revision=2.1.0| package=Images package | request=name}} STM32MP15-Ecosystem-v2.1.0 Starter Package] to the following directory:<br> '''$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package''' | |||
* Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | |||
{{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.1.0| package=Images package | request=name}} | |||
<div class="mw-collapsible mw-collapsed"> | |||
======For {{EcosystemRelease | revision=2.0.0}}====== | ======For {{EcosystemRelease | revision=2.0.0}}====== | ||
{{Warning| | <div class="mw-collapsible-content"> | ||
{{Warning|Only microSD card SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.}} | |||
* Create your STM32MP15 Starter Package directory on your host computer | * Create your STM32MP15 Starter Package directory on your host computer | ||
Line 84: | Line 99: | ||
* Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | * Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files | ||
{{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.0.0| package=Images package | request=name}} | {{PC$}} tar xvf {{EcosystemRelease/Package | revision=2.0.0| package=Images package | request=name}} | ||
</div> | |||
<noinclude> | <noinclude> |
Latest revision as of 10:46, 18 November 2020
1. Open a terminal
Open a terminal on the host computer.

All the commands preceded by PC $> have to be executed from the host computer terminal.
- Create your STM32MPU workspace directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace
PC $> cd $HOME/STM32MPU_workspace
2. Check the host computer Internet access
- An Internet access through http and https protocols must be provided.
The command below allows to check for Internet access through http/https protocols:
PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
If an 'OK' message is returned, the network is well configured.
In such case, skip the rest of this section.
Any other likely situation indicates the need for a proxy for http/https protocols.
The best solution to set a proxy for http/https protocols is via the shell variables http_proxy and https_proxy:
PC $> export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
PC $> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Check again the Internet access with command:
PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
3. Install the tools
3.1. STM32CubeProgrammer
![]() |
|
- Create your STM32MPU tools directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
- Create a temporary directory in your STM32MPU workspace
PC $> mkdir $HOME/STM32MPU_workspace/tmp
- Download latest STM32CubeProgrammer in the following directory
$HOME/STM32MPU_workspace/tmp
![]() |
ecosystem release ≥ v2.0.0 ![]() |
- Uncompress the archive file to get the STM32CubeProgrammer installers
PC $> cd $HOME/STM32MPU_workspace/tmp
PC $> unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as the installation directory, when it's requested by the installer
PC $> ./SetupSTM32CubeProgrammer-x.y.z.linux
Screenshots, done with STM32CubeProgrammer V2.5.0, are given as examples below:



- Add the STM32CubeProgrammer binary path to your PATH environment variable
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
- Check that the STM32CubeProgrammer tool is properly installed and accessible
PC $> STM32_Programmer_CLI --h
-------------------------------------------------------------------
STM32CubeProgrammer vx.y.z
-------------------------------------------------------------------
3.2. USB serial link
- Install the libusb on your host computer
PC $> sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows
PC $> cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules
PC $> sudo cp *.* /etc/udev/rules.d/
4. Download the image
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.
![]() |
To download a package, it is recommended to be logged in to your "myst" account [1]. If, trying to download, you encounter a “403 error”, you could try to empty your browser cache to workaround the problem. We are working on the resolution of this problem. We apologize for this inconvenience |
4.1. For ecosystem release unknown revision 2.1.0 
![]() |
Only microSD card SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended. |
- Create your STM32MP15 Starter Package directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package
- Download the [unknown revision/unknown revision STM32MP15-Ecosystem-v2.1.0 Starter Package] to the following directory:
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.1.0/Starter-Package - Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
unknown revisionPC $> tar xvf