Registered User mNo edit summary |
Registered User mNo edit summary |
||
(One intermediate revision by the same user not shown) | |||
Line 6: | Line 6: | ||
{{Warning|For more specific information, go through the Distribution Package article relative to your STM32 microprocessors Series: [[:Category:Distribution Package]]}} | {{Warning|For more specific information, go through the Distribution Package article relative to your STM32 microprocessors Series: [[:Category:Distribution Package]]}} | ||
==STM32MP15-Ecosystem-v2. | ==STM32MP15-Ecosystem-v2.1.0 release== | ||
<onlyinclude> | <onlyinclude> | ||
* The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision ('''{{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}}'''). | |||
* The installation relies on the ''repo'' command. In case the Repo tool (a Google-built repository management tool that runs on top of git) is not yet installed and configured on the host PC, refer to the [[PC prerequisites]] article. | |||
* The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the [[How to avoid proxy issues]] article. | |||
* Install the STM32MP1 OpenSTLinux distribution | |||
{| class="st-table" | |||
|- | |||
! !! style="text-align:center;" |STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v2.1.0 release | |||
|- | |||
| Installation || <span id="Download"></span> | |||
* Go to the host PC directory where to install the Distribution Package (''<Distribution Package installation directory>''). Example, if following the [[Example of directory structure for Packages|proposition to organize the working directory]]: | |||
$ cd <working directory path>/Distribution-Package | |||
* Create the OpenSTLinux distribution installation sub-directory: | |||
$ mkdir {{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}} | |||
$ cd {{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}} | |||
* Initialize repo in the current directory (More details on 'repo init' [https://source.android.com/setup/develop/repo#init here]). | |||
$ repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/{{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}} | |||
'''Note:''' "ERROR 404" may appear during "repo init" command without any impact on the process <br> | |||
* Synchronize the local project directories with the remote repositories specified in the manifest (more details on 'repo sync' [https://source.android.com/setup/develop/repo#sync here])<br> | |||
$ repo sync | |||
'''Note:''' ''Distribution package'' needs around 140MB to be installed (and around 25GB once ''distribution package'' is compiled).<br> | |||
|- | |||
| Release note || | |||
Details about the content of this software package are available in the '''associated''' [[STM32MP15 ecosystem release note - v2.1.0|STM32MP15 ecosystem release note]]. | |||
[[File:Archive_box.png|25px|link=]] If interested in previous releases, go through the [[STM32MP1_Distribution_Package_-_OpenSTLinux_distribution#Archives| archives]] of the ecosystem release note. | |||
|} | |||
* The '''OpenSTLinux distribution installation directory''' is in the ''<Distribution Package installation directory>, and is named ''{{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}}'': | |||
{{Green|{{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}}}} {{Highlight|OpenSTLinux distribution}} | |||
├── {{Green|layers}} | |||
│ ├── {{Green|meta-openembedded}} {{Highlight|Collection of layers for the OpenEmbedded-Core universe ([[OpenEmbedded]] standard)}} | |||
│ ├── {{Green|meta-qt5}} {{Highlight|QT5 layer for OpenEmbedded (standard)}} | |||
│ ├── {{Green|meta-st}} | |||
│ │ ├── {{Green|meta-st-openstlinux}} {{Highlight|STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution}} | |||
│ │ ├── {{Green|meta-st-stm32mp}} {{Highlight|STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices}} | |||
│ │ │ ├── {{Green|recipes-bsp}} | |||
│ │ │ │ ├── {{Green|alsa}} {{Highlight|Recipes for ALSA control configuration}} | |||
│ │ │ │ ├── {{Green|drivers}} {{Highlight|Recipes for Vivante GCNANO GPU kernel drivers}} | |||
│ │ │ │ ├── {{Green|trusted-firmware-a}} {{Highlight|Recipes for TF-A}} | |||
│ │ │ │ └── {{Green|u-boot}} {{Highlight|Recipes for U-Boot}} | |||
│ │ │ ├── {{Green|recipes-extended}} | |||
│ │ │ │ ├── {{Green|linux-examples}} {{Highlight|Recipes for Linux examples for STM32 MPU devices}} | |||
│ │ │ │ ├── {{Green|m4coredump}} {{Highlight|Recipes for script to manage coredump of cortexM4}} | |||
│ │ │ │ └── {{Green|m4projects}} {{Highlight|Recipes for firmware examples for Cortex M4}} | |||
│ │ │ ├── {{Green|recipes-graphics}} | |||
│ │ │ │ ├── {{Green|gcnano-userland}} {{Highlight|Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend)}} | |||
│ │ │ │ └── [...] | |||
│ │ │ ├── {{Green|recipes-kernel}} | |||
│ │ │ │ ├── {{Green|linux}} {{Highlight|Recipes for Linux kernel}} | |||
│ │ │ │ └── {{Green|linux-firmware}} {{Highlight|Recipes for Linux firmwares (example, Bluetooth firmware)}} | |||
│ │ │ ├── {{Green|recipes-security}} | |||
│ │ │ │ └── {{Green|optee}} {{Highlight|Recipes for OPTEE}} | |||
│ │ │ ├── {{Green|recipes-st}} | |||
│ │ │ │ └── {{Green|images}} {{Highlight|Recipes for the ''bootfs'' and ''userfs'' partitions binaries}} | |||
│ │ │ └── [...] | |||
│ │ ├── {{Green|meta-st-stm32mp-addons}} {{Highlight|STMicroelectronics layer that helps managing the STM32CubeMX integration}} | |||
│ │ └── {{Green|scripts}} | |||
│ │ ├── envsetup.sh {{Highlight|'''Environment setup script''' for Distribution Package}} | |||
│ │ └── [...] | |||
│ ├── {{Green|meta-timesys}} {{Highlight|Timesys layer for OpenEmbedded (standard)}} | |||
│ └── {{Green|openembedded-core}} {{Highlight|Core metadata for current versions of [[OpenEmbedded]] (standard)}} | |||
{{InternalInfo| Additional layer for internal usage | |||
└── st-hands-on STMicroelectronics layer that contains the reference source code for the hands-on | |||
}} | |||
</onlyinclude> | |||
==Archives [[File:Archive_box.png|25px|link=]]== | |||
{{EcosystemFlow/Archives}} | |||
<div class="mw-collapsible mw-collapsed"> | |||
===STM32MP15-Ecosystem-v2.0.0 release=== | |||
<div class="mw-collapsible-content"> | |||
* The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision ('''{{EcosystemRelease/Package | revision=2.0.0 | package=OpenSTLinux distribution | request=name}}'''). | * The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision ('''{{EcosystemRelease/Package | revision=2.0.0 | package=OpenSTLinux distribution | request=name}}'''). | ||
* The installation relies on the ''repo'' command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the [[PC prerequisites]] article. | * The installation relies on the ''repo'' command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the [[PC prerequisites]] article. | ||
Line 87: | Line 172: | ||
└── st-hands-on STMicroelectronics layer that contains the reference source code for the hands-on | └── st-hands-on STMicroelectronics layer that contains the reference source code for the hands-on | ||
}} | }} | ||
{{NoIndex}} | {{NoIndex}} |
Latest revision as of 18:45, 12 November 2020
This article aims to give the following information:
- How to download and install the latest OpenSTLinux distribution for the STM32 microprocessors Series
- Where to find the associated release note
- Where to find the previous releases (archives)
![]() |
For more specific information, go through the Distribution Package article relative to your STM32 microprocessors Series: Category:Distribution Package |
1. STM32MP15-Ecosystem-v2.1.0 release[edit source]
- The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision (Template:EcosystemRelease/Package).
- The installation relies on the repo command. In case the Repo tool (a Google-built repository management tool that runs on top of git) is not yet installed and configured on the host PC, refer to the PC prerequisites article.
- The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the How to avoid proxy issues article.
- Install the STM32MP1 OpenSTLinux distribution
STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v2.1.0 release | |
---|---|
Installation |
$ cd <working directory path>/Distribution-Package
Template:EcosystemRelease/Package $ cd Template:EcosystemRelease/Package$ mkdir
https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/Template:EcosystemRelease/Package$ repo init -u
$ repo sync
|
Release note |
Details about the content of this software package are available in the associated STM32MP15 ecosystem release note.
|
- The OpenSTLinux distribution installation directory is in the <Distribution Package installation directory>, and is named Template:EcosystemRelease/Package:
Template:EcosystemRelease/Package OpenSTLinux distribution ├── layers │ ├── meta-openembedded Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard) │ ├── meta-qt5 QT5 layer for OpenEmbedded (standard) │ ├── meta-st │ │ ├── meta-st-openstlinux STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution │ │ ├── meta-st-stm32mp STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices │ │ │ ├── recipes-bsp │ │ │ │ ├── alsa Recipes for ALSA control configuration │ │ │ │ ├── drivers Recipes for Vivante GCNANO GPU kernel drivers │ │ │ │ ├── trusted-firmware-a Recipes for TF-A │ │ │ │ └── u-boot Recipes for U-Boot │ │ │ ├── recipes-extended │ │ │ │ ├── linux-examples Recipes for Linux examples for STM32 MPU devices │ │ │ │ ├── m4coredump Recipes for script to manage coredump of cortexM4 │ │ │ │ └── m4projects Recipes for firmware examples for Cortex M4 │ │ │ ├── recipes-graphics │ │ │ │ ├── gcnano-userland Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) │ │ │ │ └── [...] │ │ │ ├── recipes-kernel │ │ │ │ ├── linux Recipes for Linux kernel │ │ │ │ └── linux-firmware Recipes for Linux firmwares (example, Bluetooth firmware) │ │ │ ├── recipes-security │ │ │ │ └── optee Recipes for OPTEE │ │ │ ├── recipes-st │ │ │ │ └── images Recipes for the bootfs and userfs partitions binaries │ │ │ └── [...] │ │ ├── meta-st-stm32mp-addons STMicroelectronics layer that helps managing the STM32CubeMX integration │ │ └── scripts │ │ ├── envsetup.sh Environment setup script for Distribution Package │ │ └── [...] │ ├── meta-timesys Timesys layer for OpenEmbedded (standard) │ └── openembedded-core Core metadata for current versions of OpenEmbedded (standard)
2. Archives
[edit source]
This wiki is for the v2 ecosystem releases. For information about the previous ecosystem releases, please go through the Wiki archives.