This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(5 intermediate revisions by one other user not shown) | |||
Line 10: | Line 10: | ||
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]]. | The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]]. | ||
{| class=" | {| class="st-table" style="text-align: center;" | ||
|- style="background: {{STLightGrey}};" | |||
! rowspan="2" style="text-align: center; width: 12%;" | '''Domain''' | |||
! rowspan="2" style="text-align: center; width: 12%;" | '''Peripheral''' | |||
! colspan="4" style="text-align: center; width: 51%;" | '''Runtime allocation''' | |||
! rowspan="2" style="text-align: center; width: 25%;" | '''Comment''' | |||
|- | |||
| style="color: white; text-align: center; background: {{STMediumGrey}}; width: 15%;" | <small>Instance</small> | |||
| style="color: white; text-align: center; background: {{STPink}}; width: 12%;" | <small>Cortex-A7<br />secure<br /> (OP-TEE)</small> | |||
| style="color: white; text-align: center; background: {{STDarkBlue}}; width: 12%;" | <small>Cortex-A7<br />non-secure<br /> (Linux)</small> | |||
| style="color: white; text-align: center; background: {{STLightBlue}}; width: 12%;" | <small>Cortex-M4<br /><br /> (STM32Cube)</small> | |||
|- | |||
</onlyinclude> | </onlyinclude> | ||
|} | |||
<noinclude> | <noinclude> | ||
{{NoIndex}} | |||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{PublicationRequestId| 7808 | 2018-06-18 | AnneJ}} | |||
</noinclude> | </noinclude> |
Latest revision as of 14:27, 19 August 2020
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |