This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User |
Registered User |
||
Line 42: | Line 42: | ||
<pre> | <pre> | ||
U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000) | U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000) | ||
CPU: | CPU: STM32MP157CAC Rev.B | ||
Model: STMicroelectronics | Model: STMicroelectronics STM32MP157C-DK2 Discovery Board | ||
Board: stm32mp1 in trusted mode (st, | Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2) | ||
Board: MB1272 | Board: MB1272 Var2.0 Rev.C-01 | ||
DRAM: 512 MiB | DRAM: 512 MiB | ||
Clocks: | Clocks: | ||
- MPU : | - MPU : 650 MHz | ||
- MCU : 208.878 MHz | - MCU : 208.878 MHz | ||
- AXI : 266.500 MHz | - AXI : 266.500 MHz | ||
Line 105: | Line 69: | ||
mmc0 is current device | mmc0 is current device | ||
Scanning mmc 0:4... | Scanning mmc 0:4... | ||
Found /mmc0_extlinux/ | Found /mmc0_extlinux/stm32mp157c-dk2_extlinux.conf | ||
Retrieving file: /mmc0_extlinux/ | Retrieving file: /mmc0_extlinux/stm32mp157c-dk2_extlinux.conf | ||
706 bytes read in | 706 bytes read in 39 ms (17.6 KiB/s) | ||
Retrieving file: /splash.bmp | Retrieving file: /splash.bmp | ||
18244 bytes read in | 18244 bytes read in 39 ms (456.1 KiB/s) | ||
Select the boot mode | Select the boot mode | ||
1: OpenSTLinux | 1: OpenSTLinux | ||
2: | 2: stm32mp157c-dk2-a7-examples | ||
3: | 3: stm32mp157c-dk2-m4-examples | ||
Enter choice: 1: OpenSTLinux | Enter choice: 1: OpenSTLinux | ||
Retrieving file: /uInitrd | Retrieving file: /uInitrd | ||
3632439 bytes read in | 3632439 bytes read in 192 ms (18 MiB/s) | ||
Retrieving file: /uImage | Retrieving file: /uImage | ||
7309840 bytes read in | 7309840 bytes read in 349 ms (20 MiB/s) | ||
append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 | append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 | ||
Retrieving file: / | Retrieving file: /stm32mp157c-dk2.dtb | ||
72638 bytes read in 42 ms (1.6 MiB/s) | |||
## Booting kernel from Legacy Image at c2000000 ... | ## Booting kernel from Legacy Image at c2000000 ... | ||
Image Name: Linux-5.4.31 | Image Name: Linux-5.4.31 | ||
Line 134: | Line 98: | ||
XIP Kernel Image | XIP Kernel Image | ||
Loading Ramdisk to cfc89000, end cffffd37 ... OK | Loading Ramdisk to cfc89000, end cffffd37 ... OK | ||
Loading Device Tree to cfc74000, end | Loading Device Tree to cfc74000, end cfc88bbd ... OK | ||
Starting kernel ... | Starting kernel ... | ||
Line 140: | Line 104: | ||
[ 0.000000] Booting Linux on physical CPU 0x0 | [ 0.000000] Booting Linux on physical CPU 0x0 | ||
[ 0.000000] Linux version 5.4.31 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020 | [ 0.000000] Linux version 5.4.31 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020 | ||
[ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d | |||
[ 0.000000] CPU: div instructions available: patching division code | |||
[...] | [...] | ||
[ 6. | [ 5.635752] EXT4-fs (mmcblk0p6): recovery complete | ||
[ 6. | [ 5.641146] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null) | ||
[ 6. | /init: eval: line 1: resize_enabled: not found | ||
[ 6. | [ 6.136734] systemd[1]: System time before build time, advancing clock. | ||
[ 6.277018] NET: Registered protocol family 10 | |||
[ 6.323818] Segment Routing with IPv6 | |||
[ 6.374449] systemd[1]: systemd 244.3+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS -ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) | |||
[ 6.396282] systemd[1]: Detected architecture arm. | |||
Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 (dunfell)! | Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 (dunfell)! | ||
[ 6. | [ 6.534284] systemd[1]: Set hostname to <stm32mp1>. | ||
[ 6. | [ 6.547703] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0 | ||
[ 6. | [ 6.555015] systemd[1]: Set hardware watchdog to 32s. | ||
[ 7. | [ 7.427085] systemd[1]: Unnecessary job for /dev/ttySTM0 was removed. | ||
[ 7. | [ 7.440799] systemd[1]: Created slice system-getty.slice. | ||
[ OK ] Created slice system-getty.slice. | |||
[ 7.482766] systemd[1]: Created slice system-serial\x2dgetty.slice. | |||
[ OK ] Created slice system-serial\x2dgetty.slice. | |||
[ 7.522459] systemd[1]: Created slice User and Session Slice. | |||
[ OK ] Created slice User and Session Slice. | |||
[ 7.561023] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. | |||
[ OK ] Started Dispatch Password …ts to Console Directory Watch. | |||
[ 7.600914] systemd[1]: Started Forward Password Requests to Wall Directory Watch. | |||
[...] | [...] | ||
[ OK ] Started Serial Getty on ttySTM0. | |||
[ OK ] Reached target Login Prompts. | |||
Starting Weston Wayland Compositor (on tty7)... | |||
[ OK ] Started Sound Service. | |||
[ OK ] Reached target Multi-User System. | |||
Starting Update UTMP about System Runlevel Changes... | Starting Update UTMP about System Runlevel Changes... | ||
[ OK ] Started Update UTMP about System Runlevel Changes. | [ OK ] Started Update UTMP about System Runlevel Changes. | ||
Line 160: | Line 143: | ||
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 stm32mp1 ttySTM0 | ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 stm32mp1 ttySTM0 | ||
root@stm32mp1: | root@stm32mp1: | ||
</pre> | </pre> |
Revision as of 15:15, 23 July 2020
1. Overview[edit source]
This stage explains how to connect the Linux terminal of your board to your host computer through the ST-LINK/V2-1.
Then you will see how to execute basic commands with the Linux command line interface in order to be familiarized with the Linux console.
2. The serial terminal[edit source]
The serial terminal allows to communicate with the board trough a UART serial interface.
- Install minicom
PC $> sudo apt-get install minicom
- Get the ttyACM device instance that need to be used to access the ST-LINK/V2-1
PC $> ls /dev/ttyACM*
/dev/ttyACM0
- Connect the minicom to the /dev/ttyACM0 device
PC $> minicom -D /dev/ttyACM0
Welcome to minicom 2.7
OPTIONS: I18n
Compiled on Nov 15 2018, 20:18:47.
Port /dev/ttyACM0, 15:56:03
Press CTRL-A Z for help on special keys
- Press the reset button to reset the board. You should see boot log displayed in the minicom window
For ecosystem release v2.0.0 :
U-Boot 2020.01-stm32mp-r1 (Jan 06 2020 - 20:56:31 +0000) CPU: STM32MP157CAC Rev.B Model: STMicroelectronics STM32MP157C-DK2 Discovery Board Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2) Board: MB1272 Var2.0 Rev.C-01 DRAM: 512 MiB Clocks: - MPU : 650 MHz - MCU : 208.878 MHz - AXI : 266.500 MHz - PER : 24 MHz - DDR : 533 MHz WDT: Started with servicing (32s timeout) NAND: 0 MiB MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1 Loading Environment from MMC... OK In: serial Out: serial Err: serial Net: eth0: ethernet@5800a000 Hit any key to stop autoboot: 0 Boot over mmc0! switch to partitions #0, OK mmc0 is current device Scanning mmc 0:4... Found /mmc0_extlinux/stm32mp157c-dk2_extlinux.conf Retrieving file: /mmc0_extlinux/stm32mp157c-dk2_extlinux.conf 706 bytes read in 39 ms (17.6 KiB/s) Retrieving file: /splash.bmp 18244 bytes read in 39 ms (456.1 KiB/s) Select the boot mode 1: OpenSTLinux 2: stm32mp157c-dk2-a7-examples 3: stm32mp157c-dk2-m4-examples Enter choice: 1: OpenSTLinux Retrieving file: /uInitrd 3632439 bytes read in 192 ms (18 MiB/s) Retrieving file: /uImage 7309840 bytes read in 349 ms (20 MiB/s) append: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 Retrieving file: /stm32mp157c-dk2.dtb 72638 bytes read in 42 ms (1.6 MiB/s) ## Booting kernel from Legacy Image at c2000000 ... Image Name: Linux-5.4.31 Created: 2020-04-08 7:08:47 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 7309776 Bytes = 7 MiB Load Address: c2000040 Entry Point: c2000040 Verifying Checksum ... OK ## Flattened Device Tree blob at c4000000 Booting using the fdt blob at 0xc4000000 XIP Kernel Image Loading Ramdisk to cfc89000, end cffffd37 ... OK Loading Device Tree to cfc74000, end cfc88bbd ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 5.4.31 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d [ 0.000000] CPU: div instructions available: patching division code [...] [ 5.635752] EXT4-fs (mmcblk0p6): recovery complete [ 5.641146] EXT4-fs (mmcblk0p6): mounted filesystem with ordered data mode. Opts: (null) /init: eval: line 1: resize_enabled: not found [ 6.136734] systemd[1]: System time before build time, advancing clock. [ 6.277018] NET: Registered protocol family 10 [ 6.323818] Segment Routing with IPv6 [ 6.374449] systemd[1]: systemd 244.3+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS -ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 6.396282] systemd[1]: Detected architecture arm. Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 (dunfell)! [ 6.534284] systemd[1]: Set hostname to <stm32mp1>. [ 6.547703] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0 [ 6.555015] systemd[1]: Set hardware watchdog to 32s. [ 7.427085] systemd[1]: Unnecessary job for /dev/ttySTM0 was removed. [ 7.440799] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 7.482766] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 7.522459] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 7.561023] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 7.600914] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [...] [ OK ] Started Serial Getty on ttySTM0. [ OK ] Reached target Login Prompts. Starting Weston Wayland Compositor (on tty7)... [ OK ] Started Sound Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. [ OK ] Started Weston Wayland Compositor (on tty7). ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 stm32mp1 ttySTM0 root@stm32mp1:
3. Basic commands[edit source]
3.1. Printing distribution specific information[edit source]
For ecosystem release v2.0.0 :
initramfs = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-multimedia = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-networking = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-webserver = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-filesystems = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-perl = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-st-stm32mp = HEAD:b86c2f2e092830f011a813d7f2c8fb076b2cbe66 meta-qt5 = HEAD:ac7514e2bc295c97faa86d24e8823829257adbb8 meta-st-openstlinux = HEAD:0124236609b3c1c56df265d7986919df4deb1814 meta = HEAD:1795f30d8ab73d35710ca99064c51190dc84853eBoard $> cat /etc/build ----------------------- Build Configuration: | ----------------------- BB_VERSION = 1.46.0 BUILD_SYS = x86_64-linux NATIVELSBSTRING = universal TARGET_SYS = arm-ostl-linux-gnueabi MACHINE = stm32mp1 DISTRO = openstlinux-weston DISTRO_VERSION = 3.1-openstlinux-5.4-dunfell-mp1-20-06-24 TUNE_FEATURES = arm vfp cortexa7 neon vfpv4 thumb callconvention-hard TARGET_FPU = hard MANIFESTVERSION = ostl-20-06-24-rc7-1-gcb1de90 DISTRO_CODENAME = dunfell ACCEPT_EULA_stm32mp1 = 1 GCCVERSION = 9.% PREFERRED_PROVIDER_virtual/kernel = linux-stm32mp PREFERRED_VERSION_linux-stm32mp = ----------------------- Layer Revisions: | ---------------------- meta-python = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-oe = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-gnome = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-xfce = HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456 meta-
3.2. Printing system information[edit source]
For ecosystem release v2.0.0 :
Linux stm32mp1 5.4.31 #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020 armv7l armv7l armv7l GNU/LinuxBoard $> uname -a
3.3. Printing Linux kernel and GCC versions[edit source]
For ecosystem release v2.0.0 :
Linux version 5.4.31 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Wed Apr 8 07:08:47 UTC 2020Board $> cat /proc/version
3.4. Printing the amount of disk space available on all mounted file systems[edit source]
Board $> df -h
Filesystem Size Used Avail Use% Mounted on
devtmpfs 148M 0 148M 0% /dev
/dev/mmcblk0p6 690M 416M 229M 65% /
tmpfs 214M 64K 214M 1% /dev/shm
tmpfs 214M 8.8M 205M 5% /run
tmpfs 214M 0 214M 0% /sys/fs/cgroup
tmpfs 214M 4.0K 214M 1% /tmp
/dev/mmcblk0p4 58M 14M 41M 25% /boot
/dev/mmcblk0p5 15M 6.7M 6.8M 50% /vendor
tmpfs 214M 144K 214M 1% /var/volatile
/dev/mmcblk0p7 14G 39M 13G 1% /usr/local
tmpfs 43M 0 43M 0% /run/user/0
3.5. ssh connection (only if Ethernet cable is connected)[edit source]
- Get the IP address of your board
UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0 valid_lft 159045sec preferred_lft 159045sec inet6 xxxx::xx:xx:xx:xx/64 scope link valid_lft forever preferred_lft foreverBoard $> ip addr show eth0 3: eth0: <BROADCAST,MULTICAST,
- On the host computer connect the terminal to the board using ssh
xx.xx.xx.xx root@stm32mp1:~#PC $> ssh root@