This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
(One intermediate revision by the same user not shown) | |||
Line 1: | Line 1: | ||
This article describes the structure of the OpenSTLinux standard SDK installation directory: | This article describes the structure of the OpenSTLinux standard SDK installation directory: | ||
Line 57: | Line 49: | ||
* a version file for the target | * a version file for the target | ||
* the root file systems (sysroots) needed to develop objects for the target system | * the root file systems (sysroots) needed to develop objects for the target system | ||
<noinclude> | |||
{{NoIndex}} | |||
[[Category:Sub-articles]] | |||
{{PublicationRequestId | 7656 | 2018-06-11 | PhilipS}} | |||
</noinclude> |
Latest revision as of 16:12, 15 April 2020
This article describes the structure of the OpenSTLinux standard SDK installation directory:
SDK ├── environment-setup-<target>-<distro>-linux-gnueabi Environment setup script ├── site-config-<target>-<distro>-linux-gnueabi Configuration file for the target ├── sysroots Root file systems │ ├── <target>-<distro>-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ ├── bin │ │ ├── boot │ │ ├── config │ │ ├── dev │ │ ├── etc │ │ ├── home │ │ ├── lib │ │ ├── media │ │ ├── mnt │ │ ├── proc │ │ ├── run │ │ ├── sbin │ │ ├── sys │ │ ├── tmp │ │ ├── usr │ │ └── var │ └── <host machine>-<distro>_sdk-linux Native sysroot (libraries, headers, and symbols) │ ├── bin │ ├── environment-setup.d │ ├── etc │ ├── lib │ ├── sbin │ ├── usr │ └── var └── version-<target>-<distro>-linux-gnueabi Version file for the target
Where:
<target> | Target architecture for cross-toolchain; examples (non exhaustive list):
|
<distro> | Distribution; examples (non-exhaustive list):
|
<host machine> | Host machine on which the SDK is installed; examples (non-exhaustive list):
|
The installed SDK consists of:
- an environment setup script for the SDK
- a configuration file for the target
- a version file for the target
- the root file systems (sysroots) needed to develop objects for the target system