This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User No edit summary |
||
Line 1: | Line 1: | ||
This article aims to give the following information: | This article aims to give the following information: | ||
* How to download and install the '''latest''' OpenSTLinux distribution for the STM32 microprocessors Series | * How to download and install the '''latest''' OpenSTLinux distribution for the STM32 microprocessors Series | ||
Line 23: | Line 13: | ||
* Install the STM32MP1 OpenSTLinux distribution | * Install the STM32MP1 OpenSTLinux distribution | ||
{| class=" | {| class="st-table" | ||
|- | |- | ||
! !! STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.1.0 release | ! !! style="text-align:center;" |STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.1.0 release | ||
|- | |- | ||
| Installation || <span id="Download"></span> | | Installation || <span id="Download"></span> | ||
Line 55: | Line 45: | ||
Details about the content of this software package are available in the '''associated''' [[STM32MP15 ecosystem release note - v1.1.0|STM32MP15 ecosystem release note]]. | Details about the content of this software package are available in the '''associated''' [[STM32MP15 ecosystem release note - v1.1.0|STM32MP15 ecosystem release note]]. | ||
If interested in previous releases, go through the [[ | [[File:Archive_box.png|25px|link=]] If interested in previous releases, go through the [[STM32MP1_Distribution_Package_-_OpenSTLinux_distribution#Archives| archives]] of the ecosystem release note. | ||
|} | |} | ||
Line 99: | Line 89: | ||
</onlyinclude> | </onlyinclude> | ||
==Archives== | ==Archives [[File:Archive_box.png|25px|link=]]== | ||
<div class="mw-collapsible mw-collapsed"> | <div class="mw-collapsible mw-collapsed"> | ||
===STM32MP15-Ecosystem-v1.0.0 release=== | ===STM32MP15-Ecosystem-v1.0.0 release=== | ||
Line 108: | Line 98: | ||
* Install the STM32MP1 OpenSTLinux distribution | * Install the STM32MP1 OpenSTLinux distribution | ||
{| class=" | {| class="st-table" | ||
|- | |- | ||
! !! STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.0.0 release | ! !! style="text-align:center;" |STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.0.0 release | ||
|- | |- | ||
| Installation || <span id="Download"></span> | | Installation || <span id="Download"></span> | ||
Line 152: | Line 142: | ||
| Release note || | | Release note || | ||
Details about the content of this software package are available in the '''associated''' [[STM32MP15 ecosystem release note - v1.0.0|STM32MP15 ecosystem release note]]. | Details about the content of this software package are available in the '''associated''' [[STM32MP15 ecosystem release note - v1.0.0|STM32MP15 ecosystem release note]]. | ||
|} | |} | ||
Line 197: | Line 185: | ||
[[Category:Sub-articles]] | [[Category:Sub-articles]] | ||
{{UpdateNeededForNewRelease| | |||
* Copy the current release (first chapter) in the "Archives" chapter | |||
* Make the following modifications in this copy: | |||
** Change the "Download" span id to "Download <name of the old release>" (example: "Download STM32MP15-Ecosystem-v1.0.0 release") | |||
* Make the following modifications in the first chapter: | |||
** Change the name of the manifest file | |||
** Change the link to the release note | |||
** Change the path and the description of the installation directory | |||
}} |
Revision as of 16:18, 10 October 2019
This article aims to give the following information:
- How to download and install the latest OpenSTLinux distribution for the STM32 microprocessors Series
- Where to find the associated release note
- Where to find the previous releases (archives)
1. STM32MP15-Ecosystem-v1.1.0 release[edit source]
- The STM32MP1 OpenSTLinux distribution is delivered through a manifest repository location and a manifest revision (openstlinux-4.19-thud-mp1-19-10-09).
- The installation relies on the repo command. In case the Repo tool (a Google-built repository management tool that runs on top of Git) is not yet installed and configured on the host PC, refer to the PC prerequisites article.
- The OpenSTLinux distribution is massively using open source software (OSS) packages that are downloaded from a variety of open source repositories; so it is required that the IT infrastructure proxies do not forbid such accesses. If some proxy-related issues are suspected, refer to the How to avoid proxy issues article.
- Install the STM32MP1 OpenSTLinux distribution
STM32MP1 Distribution Package OpenSTLinux distribution - STM32MP15-Ecosystem-v1.1.0 release | |
---|---|
Installation |
$ cd <working directory path>/Distribution-Package
$ mkdir openstlinux-4.19-thud-mp1-19-10-09
$ cd openstlinux-4.19-thud-mp1-19-10-09
$ repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-4.19-thud-mp1-19-10-09
Note: "ERROR 404" may appear during "repo init" command without any impact on the process
$ repo sync
Note: Distribution package needs around 140MB to be installed (and around 25GB once distribution package is compiled). |
Release note |
Details about the content of this software package are available in the associated STM32MP15 ecosystem release note.
|
- The OpenSTLinux distribution installation directory is in the <Distribution Package installation directory>, and is named openstlinux-4.19-thud-mp1-19-10-09:
openstlinux-4.19-thud-mp1-19-10-09 OpenSTLinux distribution ├── layers │ ├── meta-openembedded Collection of layers for the OpenEmbedded-Core universe (OpenEmbedded standard) │ ├── meta-qt5 QT5 layer for OpenEmbedded (standard) │ ├── meta-st │ │ ├── meta-st-openstlinux STMicroelectronics layer that contains the frameworks and images settings for the OpenSTLinux distribution │ │ ├── meta-st-stm32mp STMicroelectronics layer that contains the description of the BSP for the STM32 MPU devices │ │ │ ├── recipes-bsp │ │ │ │ ├── alsa Recipes for ALSA control configuration │ │ │ │ ├── drivers Recipes for Vivante GCNANO GPU kernel drivers │ │ │ │ ├── trusted-firmware-a Recipes for TF-A │ │ │ │ └── u-boot Recipes for U-Boot │ │ │ ├── recipes-extended │ │ │ │ ├── linux-examples Recipes for Linux examples for STM32 MPU devices │ │ │ │ ├── m4coredump Recipes for script to manage coredump of cortexM4 │ │ │ │ └── m4projects Recipes for firmware examples for Cortex M4 │ │ │ ├── recipes-graphics │ │ │ │ ├── gcnano-userland Recipes for Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) │ │ │ │ └── [...] │ │ │ ├── recipes-kernel │ │ │ │ ├── linux Recipes for Linux kernel │ │ │ │ └── linux-firmware Recipes for Linux firmwares (example, Bluetooth firmware) │ │ │ ├── recipes-security │ │ │ │ └── optee Recipes for OPTEE │ │ │ ├── recipes-st │ │ │ │ └── images Recipes for the bootfs and userfs partitions binaries │ │ │ └── [...] │ │ ├── meta-st-stm32mp-addons STMicroelectronics layer that helps managing the STM32CubeMX integration │ │ └── scripts │ │ ├── envsetup.sh Environment setup script for Distribution Package │ │ └── [...] │ ├── meta-timesys Timesys layer for OpenEmbedded (standard) │ └── openembedded-core Core metadata for current versions of OpenEmbedded (standard)
2. Archives
[edit source]
Expand