Approved version. Approved on: 16:04, 27 January 2020
- Last edited 3 years ago ago
Unpack the STM32MP157x-EV1 board
< Getting started | STM32MP1 boards | STM32MP157x-EV1 | Let's start
1 Overview[edit]
This first stage explains the way to unpack the STM32MP157x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides you high level information about how to connect them together.
2 Out of the box[edit]
3 Equipment[edit]
The following table lists the required equipment to start playing with your STM32MP157x-EV1 board.
Some of them are delivered with the STM32MP157x-EV1 Evaluation board. The others need to be purchased separately.
STM32MP157x-EV1 Evaluation board | Full feature board for the STM32MP15 microprocessor device | Delivered |
MicroSD card | To be populated with the OpenSTLinux Distribution (Linux software) and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed |
Delivered |
Power Supply 5V/3A | The power supply should be able to output 5V / 3A (15W) | Delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-EV1 Evaluation board to the PC through the USB micro-B (ST-LINK/V2-1) |
Not delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-EV1 Evalutation board to an USB OTG device. | Not delivered |
Laptop | Assumed a Linux PC running Ubuntu 16.04 | Not delivered |
Ethernet cable (optional) | Used to connect the STM32MP157x-EV1 Evaluation board through ssh | Not delivered |
4 Connection[edit]
- Connect the micro USB Type-B to USB Type-A cable between your laptop and the ST-LINK/V2-1 port of the board
- Connect the power supply
- Connect the micro USB Type-B to USB Type-A between your laptop and the USB Type-C™ OTG port of the board
- Optionally connect the Ethernet cable between your Ethernet network and the Ethernet port of the board
- Remove jumper JP1 and place jumpers JP4 and JP5 as shown below to allow debug through ST-LINK/V2-1