This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Let's start | Develop on Arm® Cortex®-A7 | |||||||
Unpack the board | Populate the target and boot the image | Execute basic commands | Use the demo launcher |
1 Overview[edit source]
This stage explains how to connect the Linux terminal of your board to your host computer through the ST-LINK/V2-1.
Then you will see how to execute basic commands with the Linux command line interface in order to be familiarized with the Linux console.
2 The serial terminal[edit source]
The serial terminal allows to communicate with the board trough a UART serial interface.
- Install minicom
sudo apt-get install minicom
- Get the ttyACM device instance that need to be used to access the ST-LINK/V2-1
ls /dev/ttyACM* /dev/ttyACM0
- Connect the minicom to the /dev/ttyACM0 device
minicom -D /dev/ttyACM0 Welcome to minicom 2.7 OPTIONS: I18n Compiled on Nov 15 2018, 20:18:47. Port /dev/ttyACM0, 15:56:03 Press CTRL-A Z for help on special keys
- Press the reset button to reset the board. You should see boot log displayed in the minicom window
For ecosystem release v1.1.0 :
NOTICE: CPU: STM32MP157CAC Rev.B NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board NOTICE: Board: MB1272 Var2 Rev.C-01 INFO: Reset reason (0x14): INFO: Pad Reset from NRST INFO: Using SDMMC INFO: Instance 1 INFO: Boot used partition fsbl1 NOTICE: BL2: v2.0-r1.5(debug): NOTICE: BL2: Built : 13:13:37, Oct 2 2018 INFO: BL2: Doing platform setup INFO: PMIC version = 0x10 INFO: RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.45 INFO: Memory size = 0x20000000 (512 MB) INFO: BL2 runs SP_MIN setup INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2fff0000 INFO: Image id=4 loaded: 0x2fff0000 - 0x30000000 INFO: BL2: Loading image id 5 INFO: Loading image id=5 at address 0xc0100000 INFO: STM32 Image size : 805258 WARNING: Skip signature check (header option) INFO: Image id=5 loaded: 0xc0100000 - 0xc01c498a INFO: read version 0 current version 0 NOTICE: BL2: Booting BL32 INFO: Entry point address = 0x2fff0000 INFO: SPSR = 0x1d3 INFO: PMIC version = 0x10 NOTICE: SP_MIN: v2.0-r1.5(debug): NOTICE: SP_MIN: Built : 13:13:37, Oct 2 2018 INFO: ARM GICv2 driver initialized INFO: stm32mp HSI (18): Secure only INFO: stm32mp HSE (20): Secure only INFO: stm32mp PLL2 (27): Secure only INFO: stm32mp PLL2_R (30): Secure only INFO: SP_MIN: Initializing runtime services INFO: SP_MIN: Preparing exit to normal world U-Boot 2018.11-stm32mp-r3 (Nov 14 2018 - 16:10:06 +0000) CPU: STM32MP157CAC Rev.B Model: STMicroelectronics STM32MP157C-DK2 Discovery Board Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2) Board: MB1272 Var2 Rev.C-01 DRAM: 512 MiB Clocks: - MPU : 650 MHz - MCU : 208.878 MHz - AXI : 266.500 MHz - PER : 24 MHz - DDR : 533 MHz NAND: 0 MiB MMC: STM32 SDMMC2: 0, STM32 SDMMC2: 1 Loading Environment from EXT4... OK In: serial Out: serial Err: serial Net: eth0: ethernet@5800a000 Hit any key to stop autoboot: 0 Boot over mmc0! switch to partitions #0, OK mmc0 is current device Scanning mmc 0:4... Found U-Boot script /boot.scr.uimg 1553 bytes read in 1 ms (1.5 MiB/s) ## Executing script at c4100000 Scanning mmc 0:4... Found /mmc0_stm32mp157c-dk2_extlinux/extlinux.conf Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/extlinux.conf 614 bytes read in 1 ms (599.6 KiB/s) Retrieving file: /splash.bmp 46180 bytes read in 3 ms (14.7 MiB/s) Select the boot mode 1: stm32mp157c-dk2-sdcard 2: stm32mp157c-dk2-a7-examples-sdcard 3: stm32mp157c-dk2-m4-examples-sdcard Enter choice: 1: stm32mp157c-dk2-sdcard Retrieving file: /uImage 6652480 bytes read in 295 ms (21.5 MiB/s) append: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 Retrieving file: /stm32mp157c-dk2.dtb 68852 bytes read in 4 ms (16.4 MiB/s) ## Booting kernel from Legacy Image at c2000000 ... Image Name: Linux-4.19.49 Created: 2019-06-09 7:17:25 UTC Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 6652416 Bytes = 6.3 MiB Load Address: c2000040 Entry Point: c2000040 Verifying Checksum ... OK ## Flattened Device Tree blob at c4000000 Booting using the fdt blob at 0xc4000000 XIP Kernel Image ... OK Using Device Tree in place at c4000000, end c4013cf3 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.49 (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157C-DK2 Discovery Board [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. ... [ 3.110076] Run /sbin/init as init process [ 3.115137] hub 2-1:1.0: USB hub found [ 3.117776] hub 2-1:1.0: 4 ports detected [ 3.358998] systemd[1]: System time before build time, advancing clock. [ 3.455504] NET: Registered protocol family 10 [ 3.495900] Segment Routing with IPv6 [ 3.521434] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -ID) [ 3.542498] systemd[1]: Detected architecture arm. Welcome to ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-10-09 (thud)! [ 3.601262] systemd[1]: Set hostname to <stm32mp1>. [ 3.613928] systemd[1]: Hardware watchdog 'STM32 Independent Watchdog', version 0 [ 3.621153] systemd[1]: Set hardware watchdog to 30s. [ 4.269410] systemd[1]: Unnecessary job for dev-ttySTM0.device was removed. [ 4.277529] systemd[1]: Listening on initctl Compatibility Named Pipe. ... [ OK ] Started Getty on tty1. [ OK ] Reached target Login Prompts. [ OK ] Reached target Sound Card. [ OK ] Started Load/Save RF Kill Switch Status. [ OK ] Started Login Service. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. [ OK ] Started Hostname Service. ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-10-09 stm32mp1 ttySTM0 stm32mp1 login: root (automatic login) root@stm32mp1:~#
For ecosystem release v1.0.0 :
NOTICE: CPU: STM32MP157CAC Rev.B NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board NOTICE: Board: MB1272 Var2 Rev.C-01 INFO: Reset reason (0x14): INFO: Pad Reset from NRST INFO: Using SDMMC INFO: Instance 1 INFO: Boot used partition fsbl1 INFO: Product_below_2v5=1: HSLVEN update is INFO: destructive, no update as VDD>2.7V NOTICE: BL2: v2.0(debug): NOTICE: BL2: Built : 13:13:37, Oct 2 2018 INFO: BL2: Doing platform setup INFO: PMIC version = 0x10 INFO: RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.41 INFO: Memory size = 0x20000000 (512 MB) INFO: BL2 runs SP_MIN setup INFO: BL2: Loading image id 4 INFO: Loading image id=4 at address 0x2fff0000 INFO: Image id=4 loaded: 0x2fff0000 - 0x30000000 INFO: BL2: Loading image id 5 INFO: Loading image id=5 at address 0xc0100000 INFO: STM32 Image size : 748404 WARNING: Skip signature check (header option) INFO: Image id=5 loaded: 0xc0100000 - 0xc01b6b74 INFO: read version 0 current version 0 NOTICE: BL2: Booting BL32 INFO: Entry point address = 0x2fff0000 INFO: SPSR = 0x1d3 INFO: PMIC version = 0x10 NOTICE: SP_MIN: v2.0(debug): NOTICE: SP_MIN: Built : 13:13:37, Oct 2 2018 INFO: ARM GICv2 driver initialized INFO: stm32mp HSI (18): Secure only INFO: stm32mp HSE (20): Secure only INFO: stm32mp PLL2 (27): Secure only INFO: stm32mp PLL2_R (30): Secure only INFO: SP_MIN: Initializing runtime services INFO: SP_MIN: Preparing exit to normal world U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000) CPU: STM32MP157CAC Rev.B Model: STMicroelectronics STM32MP157C-DK2 Discovery Board Board: stm32mp1 in trusted mode (st,stm32mp157c-dk2) Board: MB1272 Var2 Rev.C-01 Watchdog enabled DRAM: 512 MiB Clocks: - MPU : 650 MHz - MCU : 208.878 MHz - AXI : 266.500 MHz - PER : 24 MHz - DDR : 533 MHz NAND: 0 MiB MMC: STM32 SDMMC2: 0, STM32 SDMMC2: 1 In: serial Out: serial Err: serial Net: eth0: ethernet@5800a000 Boot over mmc0! Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Scanning mmc 0:4... Found U-Boot script /boot.scr.uimg 1553 bytes read in 0 ms ## Executing script at c4100000 Scanning mmc 0:4... Found /mmc0_stm32mp157c-dk2_extlinux/extlinux.conf Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/extlinux.conf 616 bytes read in 1 ms (601.6 KiB/s) Retrieving file: /mmc0_stm32mp157c-dk2_extlinux/../splash.bmp 46180 bytes read in 3 ms (14.7 MiB/s) Select the boot mode 1: stm32mp157c-dk2-sdcard 2: stm32mp157c-dk2-a7-examples-sdcard 3: stm32mp157c-dk2-m4-examples-sdcard Enter choice: 1: stm32mp157c-dk2-sdcard Retrieving file: /uImage 6569464 bytes read in 290 ms (21.6 MiB/s) append: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 Retrieving file: /stm32mp157c-dk2.dtb 69510 bytes read in 4 ms (16.6 MiB/s) ## Booting kernel from Legacy Image at c2000000 ... Image Name: Linux-4.19.9 Image Type: ARM Linux Kernel Image (uncompressed) Data Size: 6569400 Bytes = 6.3 MiB Load Address: c2000040 Entry Point: c2000040 Verifying Checksum ... OK ## Flattened Device Tree blob at c4000000 Booting using the fdt blob at 0xc4000000 XIP Kernel Image ... OK Using Device Tree in place at c4000000, end c4013f85 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.19.9 (oe-user@oe-host) (gcc version 8.2.0 (GCC))8 [ 0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d [ 0.000000] CPU: div instructions available: patching division code [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructie [ 0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157C-DK2 Discod [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] Reserved memory: created DMA memory pool at 0x10000000, size 0 MB [ 0.000000] OF: reserved mem: initialized node mcuram2@0x10000000, compatibll [ 0.000000] Reserved memory: created DMA memory pool at 0x10040000, size 0 MB [ 0.000000] OF: reserved mem: initialized node vdev0vring0@10040000, compatil [ 0.000000] Reserved memory: created DMA memory pool at 0x10042000, size 0 MB [ 0.000000] OF: reserved mem: initialized node vdev0vring1@10042000, compatil [ 0.000000] Reserved memory: created DMA memory pool at 0x10044000, size 0 MB [ 0.000000] OF: reserved mem: initialized node vdev0buffer@10044000, compatil [ 0.000000] Reserved memory: created DMA memory pool at 0x30000000, size 0 MB [ 0.000000] OF: reserved mem: initialized node mcuram@0x30000000, compatiblel [ 0.000000] Reserved memory: created DMA memory pool at 0x38000000, size 0 MB [ 0.000000] OF: reserved mem: initialized node retram@0x38000000, compatiblel [ 0.000000] cma: Reserved 128 MiB at 0xd4000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. ... [ OK ] Reached target Login Prompts. [ OK ] Started Avahi mDNS/DNS-SD Stack. [ OK ] Reached target Multi-User System. Starting Update UTMP about System Runlevel Changes... [ OK ] Started Update UTMP about System Runlevel Changes. ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-t0 stm32mp1 login: root (automatic login) root@stm32mp1:~#
3 Basic commands[edit source]
3.1 Printing distribution specific information[edit source]
For ecosystem release v1.1.0 :
lsb_release -a LSB Version: core-5.0-noarch:core-5.0-arm Distributor ID: openstlinux-weston Description: ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-10-09 Release: 2.6-openstlinux-4.19-thud-mp1-19-10-09 Codename: thud
For ecosystem release v1.0.0 :
lsb_release -a LSB Version: core-5.0-noarch:core-5.0-arm Distributor ID: openstlinux-weston Description: ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-02-20 Release: 2.6-openstlinux-4.19-thud-mp1-19-02-20 Codename: thud
3.2 Printing system information[edit source]
For ecosystem release v1.1.0 :
uname -a
Linux stm32mp1 4.19.49 #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019 armv7l armv7l armv7l GNU/Linux
For ecosystem release v1.0.0 :
uname -a
Linux stm32mp1 4.19.9 #2 SMP PREEMPT Wed Feb 6 19:24:47 CET 2019 armv7l armv7l armv7l GNU/Linux
3.3 Printing Linux kernel and GCC versions[edit source]
For ecosystem release v1.1.0 :
cat /proc/version
Linux version 4.19.49 (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019
For ecosystem release v1.0.0 :
cat /proc/version
Linux version 4.19.9 (host@computer) (gcc version 8.2.0 (GCC)) #2 SMP PREEMPT Wed Feb 6 19:24:47 CET 2019
3.4 Printing the amount of disk space available on all mounted file systems[edit source]
df -h Filesystem Size Used Avail Use% Mounted on /dev/root 719M 341M 340M 51% / devtmpfs 150M 0 150M 0% /dev tmpfs 214M 0 214M 0% /dev/shm tmpfs 214M 12M 203M 6% /run tmpfs 214M 0 214M 0% /sys/fs/cgroup tmpfs 214M 4.0K 214M 1% /tmp /dev/mmcblk0p4 58M 8.2M 46M 16% /boot /dev/mmcblk0p7 14G 67M 13G 1% /usr/local /dev/mmcblk0p5 15M 8.2M 5.3M 61% /vendor tmpfs 214M 84K 214M 1% /var/volatile tmpfs 43M 0 43M 0% /run/user/0
3.5 ssh connection (only if Ethernet cable is connected)[edit source]
- Get the IP address of your board
ip addr show eth0 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0 valid_lft 159045sec preferred_lft 159045sec inet6 xxxx::xx:xx:xx:xx/64 scope link valid_lft forever preferred_lft forever
- On the host computer connect the terminal to the board using ssh
ssh root@xx.xx.xx.xx
root@stm32mp1:~#