1. Usage
Historically, the Grey template was used to color text in pages, with the "classic MediaWiki grey" color. It is now mapped on the STDarkGrey template that is a STMicroelectronics corporate color.
Usage: {{Grey|<text to color>}}
Where <text to color> is the text to format in grey. If this template is called with no text, the hexadecimal code of the color is returned.
![]() |
Do not use this template anymore: use the STDarkGrey template instead. |
2. Basic examples
You type | You get |
---|---|
Coloring text in "classic MediaWiki" grey: it is now mapped on the STDarkGrey template
This was a {{Grey|"classic MediaWiki" color: grey: █}}: it is now mapped on the ST dark grey. |
This was a "classic MediaWiki" color: grey: █: it is now mapped on the ST dark grey. |
Getting the hexadecimal code of the color
{{Grey}} is the hexadecimal code of STMicroelectronics dark grey. |
#464650 is the hexadecimal code of STMicroelectronics dark grey. |
3. More examples
You type | You get |
---|---|
Grey and bold
This was a {{Grey|'''"classic MediaWiki"'''}} color: '''{{Grey|grey: █}}''': it is now mapped on the ST dark grey. |
This was a "classic MediaWiki" color: grey: █: it is now mapped on the ST dark grey. |
Grey and italic
This was a {{Grey|''"classic MediaWiki"''}} color: ''{{Grey|grey: █}}'': it is now mapped on the ST dark grey. |
This was a "classic MediaWiki" color: grey: █: it is now mapped on the ST dark grey. |
4. Code
#464650