Last edited 2 years ago

STDarkGrey

1 Usage

The STDarkGrey template is used to color text in pages, with the STMicroelectronics corporate primary color shade of dark grey (█).

Usage:  {{STDarkGrey|<text to color>|tint=<tint>}}

Where:

  • <text to color> is the text to format in dark grey. If this template is called with no text, the hexadecimal code of the color is returned.
  • <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
    • 75: 75% of the original color tint
    • 50: 50% of the original color tint
    • 25: 25% of the original color tint

2 Basic examples

You type You get
Coloring text in dark grey
This is a {{STDarkGrey|STMicroelectronics corporate color: shade of dark grey: █}}

This is a STMicroelectronics corporate color: shade of dark grey: █

Coloring text in 75% tint of dark grey
This is a {{STDarkGrey|STMicroelectronics corporate color: 75% tint of dark grey: █ | tint=75}}

This is a STMicroelectronics corporate color: 75% tint of dark grey: █

Coloring text in 50% tint of dark grey
This is a {{STDarkGrey|STMicroelectronics corporate color: 50% tint of dark grey: █ | tint=50}}

This is a STMicroelectronics corporate color: 50% tint of dark grey: █

Coloring text in 25% tint of dark grey
This is a {{STDarkGrey|STMicroelectronics corporate color: 25% tint of dark grey: █ | tint=25}}

This is a STMicroelectronics corporate color: 25% tint of dark grey: █

Getting the hexadecimal code of the color
{{STDarkGrey}} is the hexadecimal code of STMicroelectronics dark grey.

#464650 is the hexadecimal code of STMicroelectronics dark grey.

Getting the hexadecimal code of the 75% tint of the color
{{STDarkGrey | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of dark grey.

#74747C is the hexadecimal code of STMicroelectronics 75% tint of dark grey.

Getting the hexadecimal code of the 50% tint of the color
{{STDarkGrey | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of dark grey.

#A2A2A7 is the hexadecimal code of STMicroelectronics 50% tint of dark grey.

Getting the hexadecimal code of the 25% tint of the color
{{STDarkGrey | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of dark grey.

#D1D1D3 is the hexadecimal code of STMicroelectronics 25% tint of dark grey.

3 More examples

You type You get
dark grey and bold
This is a {{STDarkGrey|'''STMicroelectronics'''}} corporate color: '''{{STDarkGrey|shade of dark grey: █}}'''

This is a STMicroelectronics corporate color: shade of dark grey: █

dark grey and italic
This is a {{STDarkGrey|''STMicroelectronics''}} corporate color: ''{{STDarkGrey|shade of dark grey: █}}''

This is a STMicroelectronics corporate color: shade of dark grey: █

4 Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5 Code

#464650

No categories assignedEdit