Revision as of 14:01, 8 October 2019 by Registered User (→‎Printing system information)

STM32MP157C-EV1.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1. Overview[edit source]

This stage explains how to connect the Linux terminal of your board to your host computer through the ST-LINK/V2-1.
Then you can see how to execute basic commands with the Linux command line interface in order to be familiarized with the Linux console.

2. The serial terminal[edit source]

The serial terminal allows you to communicate with the board trough an UART serial interface.

  • Install minicom
 sudo apt-get install minicom
  • Get the ttyACM device instance that needs to be used to access the ST-LINK/V2-1
 ls /dev/ttyACM*
/dev/ttyACM0
  • Connect the minicom to the /dev/ttyACM0 device
 minicom -D /dev/ttyACM0
Welcome to minicom 2.7

OPTIONS: I18n 
Compiled on Nov 15 2018, 20:18:47.
Port /dev/ttyACM0, 15:56:03

Press CTRL-A Z for help on special keys
  • Press the reset button to reset the board. You should see logs displayed in the minicom window
NOTICE:  CPU: STM32MP157AAA Rev.B
NOTICE:  Model: STMicroelectronics STM32MP157C eval daughter on eval mother
NOTICE:  Board: MB1263 Var1 Rev.C-01
INFO:    Reset reason (0x14):
INFO:      Pad Reset from NRST
INFO:    Using SDMMC
INFO:      Instance 1
INFO:    Boot used partition fsbl1
INFO:    Product_below_2v5=1: HSLVEN update is
INFO:      destructive, no update as VDD>2.7V
NOTICE:  BL2: v2.0(debug):
NOTICE:  BL2: Built : 13:13:37, Oct  2 2018
INFO:    BL2: Doing platform setup
INFO:    PMIC version = 0x10
INFO:    RAM: DDR3-1066/888 bin G 2x4Gb 533MHz v1.41
INFO:    Memory size = 0x40000000 (1024 MB)
INFO:    BL2 runs SP_MIN setup
INFO:    BL2: Loading image id 4
INFO:    Loading image id=4 at address 0x2fff0000
INFO:    Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO:    BL2: Loading image id 5
INFO:    Loading image id=5 at address 0xc0100000
INFO:    STM32 Image size : 753913
WARNING: Skip signature check (header option)
INFO:    Image id=5 loaded: 0xc0100000 - 0xc01b80f9
INFO:    read version 0 current version 0
NOTICE:  BL2: Booting BL32
INFO:    Entry point address = 0x2fff0000
INFO:    SPSR = 0x1d3
INFO:    PMIC version = 0x10
NOTICE:  SP_MIN: v2.0(debug):
NOTICE:  SP_MIN: Built : 13:13:37, Oct  2 2018
INFO:    ARM GICv2 driver initialized
INFO:    stm32mp HSI (18): Secure only
INFO:    stm32mp HSE (20): Secure only
INFO:    stm32mp PLL2 (27): Secure only
INFO:    stm32mp PLL2_R (30): Secure only
INFO:    SP_MIN: Initializing runtime services
INFO:    SP_MIN: Preparing exit to normal world


U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)

CPU: STM32MP157AAA Rev.B
Model: STMicroelectronics STM32MP157C eval daughter on eval mother
Board: stm32mp1 in trusted mode (st,stm32mp157c-ev1)
Board: MB1263 Var1 Rev.C-01
       Watchdog enabled
DRAM:  1 GiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
NAND:  1024 MiB
MMC:   STM32 SDMMC2: 0, STM32 SDMMC2: 1
In:    serial
Out:   serial
Err:   serial
Net:   eth0: ethernet@5800a000
Boot over mmc0!
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:4...
Found U-Boot script /boot.scr.uimg
1553 bytes read in 1 ms (1.5 MiB/s)
## Executing script at c4100000
Scanning mmc 0:4...
Found /mmc0_stm32mp157c-ev1_extlinux/extlinux.conf
Retrieving file: /mmc0_stm32mp157c-ev1_extlinux/extlinux.conf
616 bytes read in 0 ms
Retrieving file: /mmc0_stm32mp157c-ev1_extlinux/../splash.bmp
46180 bytes read in 3 ms (14.7 MiB/s)
Select the boot mode
1:      stm32mp157c-ev1-sdcard
2:      stm32mp157c-ev1-a7-examples-sdcard
3:      stm32mp157c-ev1-m4-examples-sdcard
Enter choice: 1:        stm32mp157c-ev1-sdcard
Retrieving file: /uImage
6569464 bytes read in 289 ms (21.7 MiB/s)
append: root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
Retrieving file: /stm32mp157c-ev1.dtb
74445 bytes read in 5 ms (14.2 MiB/s)
## Booting kernel from Legacy Image at c2000000 ...
   Image Name:   Linux-4.19.9
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    6569400 Bytes = 6.3 MiB
   Load Address: c2000040
   Entry Point:  c2000040
   Verifying Checksum ... OK
## Flattened Device Tree blob at c4000000
   Booting using the fdt blob at 0xc4000000
   XIP Kernel Image ... OK
   Using Device Tree in place at c4000000, end c40152cc
SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.19.9 (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Thu Dec 13 08:16:23 UTC 2018
[    0.000000] CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
[    0.000000] CPU: div instructions available: patching division code
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: STMicroelectronics STM32MP157C eval daughter on eval mother
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] Reserved memory: created DMA memory pool at 0x10000000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node mcuram2@0x10000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x10040000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev0vring0@10040000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x10042000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev0vring1@10042000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x10044000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node vdev0buffer@10044000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x30000000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node mcuram@0x30000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x38000000, size 0 MiB
[    0.000000] OF: reserved mem: initialized node retram@0x38000000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 128 MiB at 0xf0000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.0

...

[  OK  ] Reached target Login Prompts.
[  OK  ] Started Sound Service.
[  OK  ] Reached target Multi-User System.
         Starting Update UTMP about System Runlevel Changes...
[  OK  ] Started Update UTMP about System Runlevel Changes.
[   23.210644] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   23.263375] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'

ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-02-20 stm32mp1 ttySTM0

stm32mp1 login: root (automatic login)

root@stm32mp1:~# 

3. Basic commands[edit source]

3.1. Printing distribution specific information[edit source]

 lsb_release -a
LSB Version:    core-5.0-noarch:core-5.0-arm
Distributor ID: openstlinux-weston
Description:    ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-openstlinux-4.19-thud-mp1-19-02-20
Release:        2.6-openstlinux-4.19-thud-mp1-19-02-20
Codename:       thud

3.2. Printing system information[edit source]

For ecosystem release v1.1.0 More info.png:

 uname -a
Linux stm32mp1 4.19.49 #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019 armv7l armv7l armv7l GNU/Linux

For ecosystem release v1.0.0 More info.png:

 uname -a
Linux stm32mp1 4.19.9 #2 SMP PREEMPT Wed Feb 6 19:24:47 CET 2019 armv7l armv7l armv7l GNU/Linux

3.3. Printing Linux kernel and GCC versions[edit source]

 cat /proc/version
Linux version 4.19.9 (oe-user@oe-host) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Thu Dec 13 08:16:23 UTC 2018

3.4. Printing the amount of disk space available on all mounted file systems[edit source]

 df -h
Filesystem      Size  Used Avail Use% Mounted on
/dev/root       719M  360M  321M  53% /
devtmpfs        150M     0  150M   0% /dev
tmpfs           214M     0  214M   0% /dev/shm
tmpfs           214M   12M  203M   6% /run
tmpfs           214M     0  214M   0% /sys/fs/cgroup
tmpfs           214M  4.0K  214M   1% /tmp
/dev/mmcblk0p4   58M  8.2M   46M  16% /boot
tmpfs           214M   92K  214M   1% /var/volatile
/dev/mmcblk0p7  6.4G   68M  6.1G   2% /usr/local
/dev/mmcblk0p5   15M  8.2M  5.3M  61% /vendor
tmpfs            43M     0   43M   0% /run/user/0


3.5. ssh connection (only if Ethernet cable is connected)[edit source]

  • Get the IP address of your board
 ip addr show eth0                                                                           
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
    link/ether 00:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff
    inet xx.xx.xx.xx/22 brd xx.xx.xx.xx scope global dynamic eth0
       valid_lft 159045sec preferred_lft 159045sec
    inet6 xx::xx:xx:xx:xx/64 scope link 
       valid_lft forever preferred_lft forever
  • On the host computer connect the terminal to the board using ssh
 ssh root@xx.xx.xx.xx
root@stm32mp1:~#


Back button.png Overview button.png Next button.png