Unpack the STM32MP157x-EV1 board

Revision as of 16:12, 15 February 2019 by Registered User

Template:ArticleMainWriter


STM32MP157C-EV1.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1. Overview[edit source]

This first stage explains you the way to unpack the STM32MP157x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides you high level information about how to connect them together.

STM32MP1 connection block diagram

2. Out of the box[edit source]

STM32MP157x-EV1 recto
STM32MP157x-EV1 verso
STM32MP157x-EV1 with all delivered items

3. Equipment[edit source]

The following table lists the required equipment to start playing with your STM32MP157x-EV1 board.
Some of them are delivered with the STM32MP157x-EV1 Evaluation board. The others need to be purchased separately.

STM32MP157x-EV1 Evaluation board Full feature board for the STM32MP15 microprocessor device Delivered
MicroSD card To be populated with the OpenSTLinux Distribution (Linux software)
and providing extra storage capacity.
A 2-Gbyte minimum microSD card is needed
Delivered
Power Supply 5V/3A The power supply should be able to output 5V / 3A (15W) Delivered
Micro USB Type-B to USB Type-A cable Used to connect the STM32MP157x-EV1 Evaluation board to the PC
through the USB micro-B (ST-LINK/V2-1)
Not delivered
Micro USB Type-B to USB Type-A cable Used to connect the STM32MP157x-EV1 Evalutation board to an USB OTG device. Not delivered
Laptop Assumed a Linux PC running Ubuntu 16.04 Not delivered
Ethernet cable (optional) Used to connect the STM32MP157x-EV1 Evaluation board through ssh Not delivered

4. Connection[edit source]

  • Connect the micro USB Type-B to USB Type-A cable between your laptop and the ST-LINK/V2-1 port of the board
  • Connect the power supply
  • Connect the micro USB Type-B to USB Type-A between your laptop and the USB Type-COTG port of the board
  • Optionally connect the Ethernet cable between your Ethernet network and the Ethernet port of the board
STM32MP157x-EV1 Evaluation board connection
  • Remove jumper JP1 and place jumpers JP4 and JP5 as shown below to allow debug through ST-LINK/V2-1
STM32MP157x-EV1 Jumper configuration
Info white.png Information
Press with your fingers on the display to be sure it is well connected and screw the screws. The 3 LEDs at the right of the display should be green when the board is powered up.



Back button.png Overview button.png Next button.png