1. Usage[edit source]
The EcosystemRelease/Components template returns the version of all software components delivered by an ecosystem release revision.
Usage: {{EcosystemRelease/Components | revision=<revision>}}
Where:
- <revision> is the mandatory revision of the ecosystem release, for which the version of all software components is requested.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
The returned value is:
- a string that contains the version of all the software components delivered by the ecosystem release revision, in a form that is usable by a tooltip.
- "unknown revision", if <<revision> is not supported.
This template relies on the EcosystemRelease/Component template.
2. Basic examples[edit source]
You type | You get |
---|---|
Components version for v1.0.0 revision requested
{{EcosystemRelease/Components | revision=1.0.0}} |
Main software components: Linux kernel v4.19-stm32mp-r1 (v4.19.9) U-Boot v2018.11-stm32mp-r2 TF-A v2.0-stm32mp-r1 OP-TEE v3.3.0-stm32mp-r1 STM32CubeMP1 Package v1.0.0 OpenEmbedded v2.6 (Thud) |
3. More examples[edit source]
You type | You get |
---|---|
Components version for v1.2.0 revision requested
{{EcosystemRelease/Components | revision=1.2.0}} |
Main software components: Linux kernel v4.19-stm32mp-r3 (v4.19.94) U-Boot v2018.11-stm32mp-r4 TF-A v2.0-stm32mp-r3 OP-TEE v3.3.0-stm32mp-r3 STM32CubeMP1 Package v1.2.0 OpenEmbedded v2.6.4 (Thud) Android v10.0.0_r22 |
Components version for v1.1.0 revision requested
{{EcosystemRelease/Components | revision=1.1.0}} |
Main software components: Linux kernel v4.19-stm32mp-r2 (v4.19.49) U-Boot v2018.11-stm32mp-r3 TF-A v2.0-stm32mp-r2 OP-TEE v3.3.0-stm32mp-r2 STM32CubeMP1 Package v1.1.0 OpenEmbedded v2.6.3 (Thud) Android v9.0.0_r46 |
Unspecified revision
{{EcosystemRelease/Components}} |
Main software components: unknown revision |
Unknown revision
{{EcosystemRelease/Components | revision=0.0.1}} |
Main software components: unknown revision |
4. Code[edit source]
Main software components: unknown revision