This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Usage[edit source]
The EcosystemRelease/Component template returns the version of a software component delivered by an ecosystem release revision of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...).
<revision> | component=<component>}}Usage: {{EcosystemRelease/Component | revision=
Where:
- <revision> is the mandatory revision of the ecosystem release, for which the version of the software component is requested.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- <component> is the mandatory software component delivered by the ecosystem release revision, for which the version of the component is requested. The possible values are:
- Linux kernel
- U-Boot
- TF-A
- OP-TEE
- STM32CubeMPU
- OpenEmbedded
- Android
The returned value is:
- a string that contains the version of the software component delivered by the ecosystem release revision.
- an empty string, if the software component is not delivered by the ecosystem release revision.
- "unknown revision", if <<revision> is not supported.
- "unknown component", if <<component> is not supported.
2. Basic examples[edit source]
You type | You get |
---|---|
Linux kernel version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=Linux kernel}}
|
Linux kernel vx.y (example) |
U-Boot version for vx.0.0 revision requested
U-Boot}}{{EcosystemRelease/Component | revision=x.0.0 | component= |
U-Boot vx.y (example) |
TF-A version for vx.0.0 revision requested
TF-A}}{{EcosystemRelease/Component | revision=x.0.0 | component= |
TF-A vx.y (example) |
OP-TEE version for vx.0.0 revision requested
OP-TEE}}{{EcosystemRelease/Component | revision=x.0.0 | component= |
OP-TEE vx.y (example) |
STM32CubeMPU version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=STM32CubeMPU }}
|
STM32CubeMP1 Package vx.y (example) |
OpenEmbedded version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=OpenEmbedded}}
|
OpenEmbedded vx.y (example) |
Android version for vx.1.0 revision requested
{{EcosystemRelease/Component | revision=x.1.0 | component=Android}}
|
Android vx.y (example) |
3. More examples[edit source]
You type | You get |
---|---|
Linux kernel version for vx.2.0 revision requested
{{EcosystemRelease/Component | revision=x.2.0 | component=Linux kernel}}
|
Linux kernel vx.y (example) |
Linux kernel version for vx.1.0 revision requested
{{EcosystemRelease/Component | revision=x.1.0 | component=Linux kernel}}
|
Linux kernel vx.y (example) |
Android version for the vx.0.0 revision requested: Android is not supported by this ecosystem release revision
{{EcosystemRelease/Component | revision=x.0.0 | component=Android}}
|
|
U-Boot version for an unspecified revision requested
U-Boot}}{{EcosystemRelease/Component | component= |
unknown revision |
TF-A version for an unknown revision requested
TF-A}}{{EcosystemRelease/Component | revision=10.20.30 | component= |
unknown revision |
Unspecified component
{{EcosystemRelease/Component | revision=x.0.0}}
|
unknown component |
Unknown component
{{EcosystemRelease/Component | revision=x.0.0 | component=not supported}}
|
unknown component |
4. Code[edit source]
unknown component