- Last edited 4 months ago ago
STM32 Sniffer for BLE Setup guide
Contents
1 Introduction
The STM32 Sniffer for Bluetooth® Low Energy is composed of two main parts:
- The software part running on the computer: analyzes and displays packets.
- The firmware part running on the STM32WB MCU: intercepts over the air packets.
System Architecture |
---|
Download the necessary files on the STM32 hotspot.
2 Minimum requirements
The following software and hardware parts are needed.
2.1 Hardware
At least one of these development boards is needed:
2.2 Software
Operating system:
- Windows 10
- Version 4.0.3 or later
- During the setup, accept the installation of Ncap.
- Version 3.11.2 or later
- Add Python to your path (you can select “Add Python to environment variable.” during setup).
- Version 3.5 or later
- Make sure that PySerial is installed on the correct version of Python if you have multiple installations. Use pip3 for example to force install on Python3.
3 Programming the board
There are two files to flash:
- The sniffer application: stm32wb55_ble_sniffer_cm4_app_nucleo.hex or stm32wb55_ble_sniffer_cm4_app_dk.hex
- The sniffer Bluetooth® LE wireless stack: stm32wb55_ble_sniffer_cm0_stack.bin
1. Install STM32CubeProgrammer
2. Update the wireless stack:
- Use the stm32wb55_ble_sniffer_cm0_stack.bin file at the start address: 0x080CE000.
- Follow the part 3.2 of the tutorial to learn how to update the wireless stack.
3. Flash the application firmware:
- Use the stm32wb55_ble_sniffer_cm4_app_nucleo.hex or stm32wb55_ble_sniffer_cm4_app_dk.hex file.
- Follow the part 3.3 of the tutorial to learn how to flash the application firmware.
4 Installing Wireshark plugins
Launch Wireshark:
Finding the Wireshark plugins directories |
---|
4.1 Installing the plugins
- Copy the st_ble_sniffer_dissector.lua file into your Wireshark Personal Lua Plugins folder.
- Copy the st_ble_sniffer.py and st_ble_sniffer.bat files into your Wireshark Personal Extcap path folder.
Your folders should look like this:
Plugins folders |
---|
- Open a command prompt in your Personal Extcap path folder.
- Run: st_ble_sniffer.bat --extcap-interfaces
You should have an output similar to this:
Verifying that the extcap plugin runs |
---|
- Make sure that the board with the sniffer firmwares is plugged, and that no other programs use the com port such as the serial terminal.
- In Wireshark, refresh the capture interfaces list:
Verifying extcap plugin can run in Wireshark |
---|
You should now see the STM32WB sniffer interface like this:
Verifying that extcap plugin runs in Wireshark |
---|
4.2 Installing the profile
In Wireshark:
Finding the Wireshark profiles directory |
---|
Copy the ST_BLE_Sniffer_profile folder into your Wireshark Personal configuration/profiles folder.
Your folder should look like this:
Verifying that extcap plugin runs in Wireshark |
---|
5 Configuring Wireshark
5.1 Enabling the sniffer profile
In Wireshark:
Enabling the profile |
---|
5.2 Enabling the interface toolbar
Open Wireshark:
Enabling the interface toolbar |
---|
This toolbar should be visible:
Interface toolbar |
---|
5.3 Testing
Double click on the STM32WB sniffer interface to launch the capture.
Verifying that extcap plugin runs in Wireshark |
---|
If advertising packets are visible like in the graphic below, it means that the installation of the STM32 Sniffer for Bluetooth® Low Energy is successful.
Verifying the installation |
---|
Refer to the user guide to learn more about how to use the sniffer.