1. Introduction
The STM32 Sniffer for Bluetooth® Low Energy is composed of two main parts.
- The software part running on the computer : analyzes and displays packets
- The firmware part running on the STM32WB MCU : intercepts over the air packets
System Architecture |
---|
You can download necessary files on STM32 Hotspot.
2. Minimum requirements
The following software and hardware parts are needed.
2.1. Hardware
You will need at least one of these development boards:
2.2. Software
Operating system:
- Windows 10
- Version 4.0.3 or later
- During setup accept Ncap installation
- Version 3.11.2 or later
- Add python to your path
- Version 3.5 or later
- Make sure PySerial is installed on the correct version of Python if you have multiple installations (use pip3 for example to force install on Python3)
3. Programming the board
There is two files to flash:
- The sniffer application : stm32wb55_ble_sniffer_cm4_app_nucleo.hex or stm32wb55_ble_sniffer_cm4_app_dk.hex
- The sniffer Bluetooth® LE Wireless Stack : stm32wb55_ble_sniffer_cm0_stack.bin
1. Install STM32CubeProgrammer
2. Update the Wireless stack:
- Use the stm32wb55_ble_sniffer_cm0_stack.bin file at the start address: 0x080CE000.
- You can follow this tutorial part 3.2 to learn how to update the Wireless Stack.
3. Flash the application firmware:
- Use the stm32wb55_ble_sniffer_cm4_app_nucleo.hex or stm32wb55_ble_sniffer_cm4_app_dk.hex file
- You can follow this tutorial part 3.3 to learn how to flash the application firmware.
4. Installing Wireshark plugins
Launch Wireshark:
Finding the Wireshark plugins directories |
---|
4.1. Installing the plugins
- Copy the st_ble_sniffer_dissector.lua file into your Wireshark Personal Lua Plugins folder
- Copy the st_ble_sniffer.py and st_ble_sniffer.bat files into your Wireshark Personal Extcap path folder
Your folders should look like this:
Plugins folders |
---|
- Open a command prompt in your Personal Extcap path folder.
- Run : st_ble_sniffer.bat --extcap-interfaces
You should have an output similar to this:
Verifying extcap plugin can run |
---|
- Make sure a board with the sniffer firmwares is plugged (and no other program use the com port, e.g : serial terminal)
- In Wireshark, refresh the capture interfaces list:
Verifying extcap plugin can run in Wireshark |
---|
You should now see the STM32WB sniffer interface like this:
Verifying extcap plugin can run in Wireshark |
---|
4.2. Installing the profile
In Wireshark:
Finding the Wireshark profiles directory |
---|
Copy ST_BLE_Sniffer_profile folder into your Wireshark Personal configuration/profiles folder
Your folder should look lite this:
Verifying extcap plugin can run in Wireshark |
---|
5. Configuring Wireshark
5.1. Enabling the sniffer profile
In Wireshark :
Enabling the profile |
---|
5.2. Enabling the interface toolbar
Open Wireshark :
Enabling the interface toolbar |
---|
You should now see a toolbar like this:
Interface toolbar |
---|
5.3. Testing
Double click on the STM32WB Sniffer interface to launch the capture.
Verifying extcap plugin can run in Wireshark |
---|
You should now see advertising packets like below meaning that you successfully installed the STM32 Sniffer for Bluetooth® Low Energy 😉
Verifying the installation |
---|
You can now see the user guide to learn more about how to use the sniffer.