STM32 Sniffer for BLE User guide

Revision as of 10:47, 16 June 2023 by Registered User

This article provide help about how to use the STM32 Sniffer for Bluetooth® LE with Wireshark. It is supposed that you've already installed the sniffer, if it is not the case, you can follow this guide.

1. Starting the capture

Plug your sniffer board and open Wireshark.

1.1. Optional configuration

  • In Wireshark, click on the wheel on the left of the STM32 sniffer interface to open the interface configuration menu.
  • The channel index parameter is the channel on which the sniffer will listen when started. It can be changed later on the fly. By default it is channel index 39.
  • This is the channel index, not the frequency index. e.g (primary adverstising channels indexes are 37, 38 and 39).
Optional parameter
Connectivity Sniffer Optional Parameters.png


1.2. Launching the capture

To start the capture:

puce1.png
Click once to select the interface
puce2.png
Click on start capturing

or

puce1.png
Double click on the interface
Optional parameter
Connectivity Sniffer Start Capture.png


1.3. Sniffer started

You should now see the advertising packets on the channel you configured.

puce1.png
By default on startup the target BD address is set to 00:00:00:00:00:00, meaning that no target is set so packets from every devices are displayed.
Optional parameter
Connectivity Sniffer Started.png


2. Following a connection

Once the sniffer is started is reports advertising, scan requests and scan requests of all devices. You can then set the BD address of your target device that you want to follow when a connection to it occur.

puce1.png
Set the target BD address
puce2.png
Apply changes
Setting a target to follow
Connectivity Sniffer Target1.png
Connectivity Sniffer Target2.png


Now you should only see:

  • Advertising and scan responses packets from the target
  • Scan requests to the target
  • Connection packets from and to the target
Target set
Connectivity Sniffer Target3.png


If after setting the target there is no more packets incoming either:

  • There is no device with this BD address advertising on this channel
  • The sniffer has not received the command, set again the target (you will need to make a change to be able to apply changes. Just delete the last number and reenter it)

Now if a device connect to your target and the sniffer intercept the CONNECT_IND packet you will start to see the communications between the two devices.

Info white.png Information
As the sniffer only listen on one advertising channel it may not intercept the connection request on first try. In this case, reconnect to your target. You can also see the multiple interfaces capture to improve the connect request interception success rate.
Connection intercepted
Connectivity Sniffer Connected1.png


Now you have some additional data:

  • The direction column indicates the direction of the packets
  • The color of the lines is alternating for each connection event

If the connection is terminated or if the sniffer loose it, it will return to the advertising channel you have configured before.

No categories assignedEdit