Package

1. Usage[edit source]

The X-LINUXRelease/Package template returns either the name, the URL, or the installation path, of a software package or script delivered by an expansion package on top of an ecosystem release revision of the flow associated with this wiki.

Usage: {{X-LINUXRelease/Package | version=<version> | package=<package> | device=<device> | request=<request> |arch = <arch> }}

Where:

  • <version> is the mandatory version of the expansion package, for which the name, the URL, or the installation path of the software package or script is requested.
    • The possible values for this parameter can be found through the X-LINUXRelease/Revision template.
    • latest is also a possible value: the latest version of the expansion package is then considered.
  • <package> is the mandatory software package or script delivered by the expansion package version, for which the name, the URL, or the installation path is requested. The possible values are listed in the below table.
  • <device> is the optional parameter that specifies the microprocessor devices for which the piece of information is requested. The possible values are listed in the below table.
  • <request> is the mandatory request, i.e. either the name, the url, or the installation path, of the software package or script. The possible values are listed in the below table.
  • <arch> is the optional request. The possible values are listed in the below table, specific for QT.

The returned value is:

  • a string that contains either the name, the URL or the installation path, of the software package or script (see the below table for details).
  • an empty string, if the request is not applicable (e.g. requesting the URL of the AI SDK environment script makes no sense).
  • "unknown version", if <version> is not supported.
  • "unknown package or script", if <package> is not supported.
  • "unknown request", if <request> is not supported.
<package> <device> / <arch> <request> Description of the returned value
AI Debian package Not applicable name Name of the Debian package of the X-LINUX-AI expansion package
url URL (st.com) to the Debian package (non-clickable link)
path Nothing is returned (not applicable)
AI SDK package name Name of the tarball file that contains the SDK installation script for the X-LINUX-AI expansion package (x86_64 host architecture)
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
AI SDK installation script name Name of the SDK installation script for the X-LINUX-AI expansion package (x86_64 host architecture)
url Nothing is returned (not applicable)
path Path to the directory that contains the SDK installation script for the X-LINUX-AI expansion package, once the SDK package tarball file is uncompressed (x86_64 host architecture)
AI SDK setup script
  • MP1
  • MP2
name Name of the SDK setup script for the X-LINUX-AI expansion package (x86_64 host architecture)
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
QT Debian package Not applicable name Name of the Debian package of the X-LINUX-QT expansion package
url URL (st.com) to the Debian package (non-clickable link)
path Nothing is returned (not applicable)
QT SDK package
  • MP1 / aarch64
  • MP1 / x86_64
  • MP2 / aarch64
  • MP2 / x86_64
name Name of the QT SDK package of the X-LINUX-QT expansion package
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
QT SDK installation script
  • MP1 / aarch64
  • MP1 / x86_64
  • MP2 / aarch64
  • MP2 / x86_64
name Name of QT SDK installation script
url Nothing is returned (not applicable)
path Path to the directory that contains the QT SDK installation script for the X-LINUX-QT expansion package, once the SDK package tarball file is uncompressed (x86_64 host architecture)
QT SDK setup script
  • MP1
  • MP2 Default Value
name Name of the QT SDK setup script e of the X-LINUX-QT expansion package
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
  1. ↑ 1.0 1.1 If <device> is not set, the MP1 value is per default considered.
Warning white.png Warning
Read carefully the below information about the use of this template in preformatted text blocks.
  • It is not possible to use this template (as any template) in preformatted text blocks made with with <pre>...</pre>: use preformatted text blocks made with space at the beginning of the line.
  • If needed (especially in tables), limit the width of the blocks with <div style="max-width:60em;"> (adjust the value)
Do not use <pre>...</pre>
You type
<pre>
tar xvf {{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=name}}
</pre>
You get
tar xvf {{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=name}}
Use space at the beginning of the line
You type
tar xvf {{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=name}}
You get

tar xvf en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz

Limit the width of the block
You type
<div style="max-width:60em;">
This is a very long command that uses the template (tar xvf {{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=name}}) and its width might be a problem
</div>
You get

This is a very long command that uses the template (tar xvf en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz) and its width might be a problem

2. Basic examples[edit source]

2.1. Basic examples for latest version of the expansion packages[edit source]

2.1.1. For AI expansion package[edit source]

You type You get
"AI Debian package" name, URL and path for the latest version of the X-LINUX-AI expansion package requested
Name: {{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=path}}

Name: apt-openstlinux-ai_1.0_arm64.debTBD
URL: http://extra.packages.openstlinux.st.com/alpha/stm32mp2/AI/5.0/pool/config/a/apt-openstlinux-ai/TBD
Path: NA

"AI SDK package" name, URL and path for the latest version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=latest | package=AI SDK package | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=latest | package=AI SDK package | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=AI SDK package | request=path}}

Name (default): en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz
Name (MP1): en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz
Name (MP2): en.SDK-x86_64-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz
URL: [NA]
Path: NA

"AI SDK installation script" name, URL and path for the latest version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | device=MP2 |request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | request=url}}]<br>
Path (default): {{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | device=MP1 | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version=latest | package=AI SDK installation script | device=MP2 | request=path}}

Name (default): st-image-ai-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.sh
Name (MP1): st-image-ai-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.sh
Name (MP2): st-image-ai-openstlinux-weston-stm32mp2.rootfs-x86_64-toolchain-5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.sh
URL: [NA]
Path (default): stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0
Path (default): stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0
Path (default): stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0

"AI SDK setup script" name, URL and path for the latest version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest | package=AI SDK setup script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=latest | package=AI SDK setup script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=latest | package=AI SDK setup script | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=AI SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=AI SDK setup script | request=path}}

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP2): environment-setup-cortexa35-ostl-linux
URL: [NA]
Path: NA

2.1.2. For QT expansion package[edit source]

You type You get
"QT version" name, URL and path for the latest version of the X-LINUX-QT expansion package requested
Name: {{X-LINUXRelease/Package | version=latest | package=QT version | request=name}}<br>
URL: [{{#explode:{{X-LINUXRelease/Package | version=1.0.0 | package=QT version | request=url}}|,|0}}]<br>
Branch: [{{#explode:{{X-LINUXRelease/Package | version=1.0.0 | package=QT version | request=url}}|,|1}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=QT version | request=path}}

Name: 6.5.3
URL: https://github.com/meta-qt5/meta-qt5.git
Branch: scarthgap
Path: layers/meta-qt6

"QT Debian package" name, URL and path for the latest version of the X-LINUX-QT expansion package requested
Name: {{X-LINUXRelease/Package | version=latest | package=QT Debian package | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=QT Debian package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=QT Debian package | request=path}}

Name: packagegroup-x-linux-qt
URL: [1]
Path: ./apt-openstlinux-x-linux-qt_1.0_all.deb

"QT SDK package" name, URL and path for the latest version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest | package=QT SDK package | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=QT SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=QT SDK package | request=path}}

Name (default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP2 / default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP2 / aarch64): en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP2 / x86_64): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP1 / default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP1 / aarch64): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP1 / x86_64): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
URL: [NA]
Path: NA

"QT SDK installation script" name, URL and path for the latest version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | request=url}}]<br>
Path (MP2 / default): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP2 | request=path}}<br>
Path (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=path}}<br>
Path (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=path}}<br>
Path (MP1 / default): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP1 | request=path}}<br>
Path (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=path}}<br>
Path (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=path}}<br>

Name (default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP2 / default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP2 / aarch64): st-image-qt-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP2 / x86_64): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP1 / default): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP1 / aarch64): st-image-qt-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP1 / x86_64): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
URL: [NA]
Path (MP2 / default): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP2 / aarch64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP2 / x86_64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP1 / default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP1 / aarch64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP1 / x86_64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk

"QT SDK setup script" name, URL and path for the latest version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest | package=QT SDK setup script | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=latest | package=QT SDK setup script | device=MP2 | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=latest | package=QT SDK setup script | device=MP1 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=QT SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=QT SDK setup script | request=path}}

Name (default): environment-setup-cortexa35-ostl-linux
Name (MP2): environment-setup-cortexa35-ostl-linux
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
URL: [NA]
Path: NA

2.2. Basic examples for specified version of the expansion packages[edit source]

2.2.1. Basic examples for specified version of AI expansion package[edit source]

2.2.1.1. For 6.0.0 version of AI expansion package[edit source]
You type You get
"AI Debian package" name, URL and path for the 6.0.0 version of the X-LINUX-AI expansion package requested
Name: {{X-LINUXRelease/Package | version=6.0.0 | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=6.0.0 | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=6.0.0 | package=AI Debian package | request=path}}

Name: apt-openstlinux-ai_1.0_arm64.debTBD
URL: http://extra.packages.openstlinux.st.com/alpha/stm32mp2/AI/5.0/pool/config/a/apt-openstlinux-ai/TBD
Path: NA

"AI SDK package" name, URL and path for the 6.0.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK package | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK package | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK package | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK package | request=path}}

Name (default): en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz
Name (MP1): en.SDK-x86_64-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz
Name (MP2): en.SDK-x86_64-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.tar.gz
URL: [NA]
Path: NA

"AI SDK installation script" name, URL and path for the 6.0.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | device=MP2 |request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | request=url}}]<br>
Path (default): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | device=MP1 | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK installation script | device=MP2 | request=path}}

Name (default): st-image-ai-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.sh
Name (MP1): st-image-ai-openstlinux-weston-stm32mp1.rootfs-x86_64-toolchain-5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.sh
Name (MP2): st-image-ai-openstlinux-weston-stm32mp2.rootfs-x86_64-toolchain-5.0.3-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0.sh
URL: [NA]
Path (default): stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0
Path (default): stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0
Path (default): stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06-addon-x-linux-ai-v6.0.0

"AI SDK setup script" name, URL and path for the 6.0.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK setup script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK setup script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK setup script | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=6.0.0 | package=AI SDK setup script | request=path}}

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP2): environment-setup-cortexa35-ostl-linux
URL: [NA]
Path: NA

2.2.1.2. For 5.1.0 version of AI expansion package[edit source]
You type You get
"AI Debian package" name, URL and path for the 5.1.0 version of the X-LINUX-AI expansion package requested
Name: {{X-LINUXRelease/Package | version=5.1.0 | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=5.1.0 | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=5.1.0 | package=AI Debian package | request=path}}

Name: apt-openstlinux-ai_1.0_arm64.debTBD
URL: http://extra.packages.openstlinux.st.com/alpha/stm32mp2/AI/5.0/pool/config/a/apt-openstlinux-ai/TBD
Path: NA

"AI SDK package" name, URL and path for the 5.1.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK package | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK package | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK package | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK package | request=path}}

Name (default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.tar.gz
Name (MP1): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.tar.gz
Name (MP2): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.tar.gz
URL: [NA]
Path: NA

"AI SDK installation script" name, URL and path for the 5.1.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | device=MP2 |request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | request=url}}]<br>
Path (default): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | device=MP1 | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK installation script | device=MP2 | request=path}}

Name (default): st-image-ai-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.sh
Name (MP1): st-image-ai-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.sh
Name (MP2): st-image-ai-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.sh
URL: [NA]
Path (default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0
Path (default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0
Path (default): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0

"AI SDK setup script" name, URL and path for the 5.1.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK setup script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK setup script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK setup script | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=5.1.0 | package=AI SDK setup script | request=path}}

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP2): environment-setup-cortexa35-ostl-linux
URL: [NA]
Path: NA

2.2.1.3. For 5.0.0 version of AI expansion package[edit source]
You type You get
"AI Debian package" name, URL and path for the v5.0.0 version of the X-LINUX-AI expansion package requested
Name: {{X-LINUXRelease/Package | version=5.0.0 | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=5.0.0 | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=5.0.0 | package=AI Debian package | request=path}}

Name: apt-openstlinux-ai_1.0_armhf.deb
URL: http://extra.packages.openstlinux.st.com/AI/5.0/pool/config/a/apt-openstlinux-ai/
Path: NA

"AI SDK package" name, URL and path for the v5.0.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK package | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK package | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK package | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK package | request=path}}

Name (default): en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-addon-x-linux-ai-v5.0.0.tar.gz
Name (MP1): en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-addon-x-linux-ai-v5.0.0.tar.gz
Name (MP2): unknown device
URL: [2]
Path: NA

"AI SDK installation script" name, URL and path for the v5.0.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | device=MP2 |request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | request=url}}]<br>
Path (default): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | request=path}}<br>
Path (MP1): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | device=MP1 | request=path}}<br>
Path (MP2): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK installation script | device=MP2 | request=path}}

Name (default): st-image-ai-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-addon-x-linux-ai-v5.0.0.sh
Name (MP1): st-image-ai-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-addon-x-linux-ai-v5.0.0.sh
Name (MP2): unknown device
URL: [NA]
Path (default): stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-addon-x-linux-ai-v5.0.0
Path (MP1): stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21-addon-x-linux-ai-v5.0.0
Path (MP2): NA

"AI SDK setup script" name, URL and path for the v5.0.0 version of the X-LINUX-AI expansion package requested
Name (default): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK setup script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK setup script | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK setup script | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=5.0.0 | package=AI SDK setup script | request=path}}

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP2): unknown device
URL: [NA]
Path: NA


2.2.2. Basic examples for specified version of QT expansion package[edit source]

2.2.2.1. For 1.0.0 version of QT expansion package[edit source]
You type You get
"QT Debian package" name, URL and path for the 1.0.0 version of the X-LINUX-QT expansion package requested
Name: {{X-LINUXRelease/Package | version=1.0.0 | package=QT Debian package | device=MP2 | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=1.0.0 | package=QT Debian package | device=MP2 | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=1.0.0 | package=QT Debian package | device=MP2 | request=path}}

Name: packagegroup-x-linux-qt
URL: apt-openstlinux-qt
Path: NA

"QT SDK package" name, URL and path for the 1.0.0 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK package | request=path}}

Name (default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP2 / default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP2 / aarch64): en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP2 / x86_64): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP1 / default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP1 / aarch64): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP1 / x86_64): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
URL: [NA]
Path: NA

"QT SDK installation script" name, URL and path for the 1.0.0 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | request=url}}]<br>
Path (MP2 / default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP2 | request=path}}<br>
Path (MP2 / aarch64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=path}}<br>
Path (MP2 / x86_64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=path}}<br>
Path (MP1 / default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP1 | request=path}}<br>
Path (MP1 / aarch64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=path}}<br>
Path (MP1 / x86_64): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=path}}<br>

Name (default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP2 / default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP2 / aarch64): st-image-qt-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP2 / x86_64): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP1 / default): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP1 / aarch64): st-image-qt-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP1 / x86_64): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
URL: [NA]
Path (MP2 / default): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP2 / aarch64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP2 / x86_64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP1 / default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP1 / aarch64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP1 / x86_64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk

"QT SDK setup script" name, URL and path for the 1.0.0 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK setup script | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK setup script | device=MP2 | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK setup script | device=MP1 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=1.0.0 | package=QT SDK setup script | request=path}}

Name (default): environment-setup-cortexa35-ostl-linux
Name (MP2): environment-setup-cortexa35-ostl-linux
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
URL: [NA]
Path: NA

2.2.2.2. For latest_qt5 version of QT expansion package[edit source]
You type You get
"QT Debian package" name, URL and path for the latest_qt5 version of the X-LINUX-QT expansion package requested
Name: {{X-LINUXRelease/Package | version=latest_qt5 | package=QT Debian package | device=MP2 | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=latest_qt5 | package=QT Debian package | device=MP2 | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=latest_qt5 | package=QT Debian package | device=MP2 | request=path}}

Name: packagegroup-x-linux-qt
URL: apt-openstlinux-qt
Path: NA

"QT SDK package" name, URL and path for the latest_qt5 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK package | request=path}}

Name (default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP2 / default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP2 / aarch64): en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP2 / x86_64): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP1 / default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP1 / aarch64): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
Name (MP1 / x86_64): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0.tar.gz
URL: [NA]
Path: NA

"QT SDK installation script" name, URL and path for the latest_qt5 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | request=url}}]<br>
Path (MP2 / default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP2 | request=path}}<br>
Path (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=path}}<br>
Path (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=path}}<br>
Path (MP1 / default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP1 | request=path}}<br>
Path (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=path}}<br>
Path (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=path}}<br>

Name (default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP2 / default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP2 / aarch64): st-image-qt-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP2 / x86_64): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP1 / default): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP1 / aarch64): st-image-qt-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
Name (MP1 / x86_64): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v1.0.0.sh
URL: [NA]
Path (MP2 / default): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP2 / aarch64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP2 / x86_64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP1 / default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP1 / aarch64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk
Path (MP1 / x86_64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v1.0.0/sdk

"QT SDK setup script" name, URL and path for the latest_qt5 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK setup script | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK setup script | device=MP2 | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK setup script | device=MP1 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest_qt5 | package=QT SDK setup script | request=path}}

Name (default): environment-setup-cortexa35-ostl-linux
Name (MP2): environment-setup-cortexa35-ostl-linux
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
URL: [NA]
Path: NA

2.2.2.3. For latest_qt6 version of QT expansion package[edit source]
You type You get
"QT Debian package" name, URL and path for the latest_qt6 version of the X-LINUX-QT expansion package requested
Name: {{X-LINUXRelease/Package | version=latest_qt6 | package=QT Debian package | device=MP2 | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=latest_qt6 | package=QT Debian package | device=MP2 | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=latest_qt6 | package=QT Debian package | device=MP2 | request=path}}

Name: packagegroup-x-linux-qt
URL: http://extra.packages.openstlinux.st.com/Qt/5.1/pool/config/a/apt-openstlinux-x-linux-qt/apt-openstlinux-x-linux-qt_1.0_all.deb
Path: ./apt-openstlinux-x-linux-qt_1.0_all.deb

"QT SDK package" name, URL and path for the latest_qt6 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK package | request=path}}

Name (default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP2 / default): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP2 / aarch64): en.sdk-aarch64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP2 / x86_64): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP1 / default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP1 / aarch64): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
Name (MP1 / x86_64): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0.tar.gz
URL: [NA]
Path: NA

"QT SDK installation script" name, URL and path for the latest_qt6 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | request=url}}]<br>
Path (MP2 / default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP2 | request=path}}<br>
Path (MP2 / aarch64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=path}}<br>
Path (MP2 / x86_64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=path}}<br>
Path (MP1 / default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP1 | request=path}}<br>
Path (MP1 / aarch64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=path}}<br>
Path (MP1 / x86_64): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=path}}<br>

Name (default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP2 / default): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP2 / aarch64): st-image-qt-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP2 / x86_64): st-image-qt-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP1 / default): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP1 / aarch64): st-image-qt-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
Name (MP1 / x86_64): st-image-qt-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-qt-v2.0.0.sh
URL: [NA]
Path (MP2 / default): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP2 / aarch64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP2 / x86_64): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP1 / default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP1 / aarch64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk
Path (MP1 / x86_64): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-x-linux-qt-v2.0.0/sdk

"QT SDK setup script" name, URL and path for the latest_qt6 version of the X-LINUX-QT expansion package requested
Name (default): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK setup script | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK setup script | device=MP2 | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK setup script | device=MP1 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest_qt6 | package=QT SDK setup script | request=path}}

Name (default): environment-setup-cortexa35-ostl-linux
Name (MP2): environment-setup-cortexa35-ostl-linux
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
URL: [NA]
Path: NA

2.3. Basic examples for revisions of the ecosystem releases[edit source]

2.3.1. For AI expansion package[edit source]

You type You get
"AI Debian package" name, URL and path for the version of the X-LINUX-AI expansion package on top of the v5.1.0 ecosystem release requested
Name: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI Debian package | request=path}}

Name: apt-openstlinux-ai_1.0_arm64.debTBD
URL: http://extra.packages.openstlinux.st.com/alpha/stm32mp2/AI/5.0/pool/config/a/apt-openstlinux-ai/TBD
Path: NA

"AI SDK package" name, URL and path for the version of the X-LINUX-AI expansion package on top of the v5.1.0 ecosystem release requested
Name (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK package | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK package | device=MP1 | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK package | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK package | request=path}}

Name (default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.tar.gz
Name (MP1): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.tar.gz
Name (MP2): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.tar.gz
URL: [NA]
Path: NA

"AI SDK installation script" name, URL and path for the version of the X-LINUX-AI expansion package on top of the v5.1.0 ecosystem release requested
Name (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | device=MP1 |request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | request=url}}]<br>
Path (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | device=MP1 | request=path}}<br>
Path (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK installation script | device=MP2 | request=path}}

Name (default): st-image-ai-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.sh
Name (MP1): st-image-ai-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.sh
Name (MP2): st-image-ai-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0.sh
URL: [NA]
Path (default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0
Path (default): stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0
Path (default): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26-addon-x-linux-ai-v5.1.0

"AI SDK setup script" name, URL and path for the version of the X-LINUX-AI expansion package on top of the v5.1.0 ecosystem release requested
Name: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK setup script | 
request=name}}<br>
Name: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK setup script | device=MP1 | request=name}}<br>
Name: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK setup script | device=MP2 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=AI | type=release}} | package=AI SDK setup script | request=path}}
Name: environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

Name: environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name: environment-setup-cortexa35-ostl-linux
URL: [NA]
Path: NA


2.3.2. For QT expansion package[edit source]

You type You get
"QT Debian package" name, URL and path for the version of the X-LINUX-QT expansion package on top of the v5.1.0 ecosystem release
Name: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT Debian package | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT Debian package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT Debian package | request=path}}

Name: unknown version
URL: [unknown version]
Path: unknown version

"QT SDK package" name, URL and path ffor the version of the X-LINUX-QT expansion package on top of the v5.1.0 ecosystem release
Name (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK package | request=path}}

Name (default): unknown version
Name (MP2 / default): unknown version
Name (MP2 / aarch64): unknown version
Name (MP2 / x86_64): unknown version
Name (MP1 / default): unknown version
Name (MP1 / aarch64): unknown version
Name (MP1 / x86_64): unknown version
URL: [unknown version]
Path: unknown version

"QT SDK installation script" name, URL and path for the version of the X-LINUX-QT expansion package on top of the v5.1.0 ecosystem release
Name (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | request=name}}<br>
Name (MP2 / default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP2 | request=name}}<br>
Name (MP2 / aarch64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=name}}<br>
Name (MP2 / x86_64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=name}}<br>
Name (MP1 / default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP1 | request=name}}<br>
Name (MP1 / aarch64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=name}}<br>
Name (MP1 / x86_64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | request=url}}]<br>
Path (MP2 / default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP2 | request=path}}<br>
Path (MP2 / aarch64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP2 | arch = aarch64 | request=path}}<br>
Path (MP2 / x86_64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP2 | arch = x86_64 | request=path}}<br>
Path (MP1 / default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP1 | request=path}}<br>
Path (MP1 / aarch64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP1 | arch = aarch64 | request=path}}<br>
Path (MP1 / x86_64): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK installation script | device=MP1 | arch = x86_64 | request=path}}<br>

Name (default): unknown version
Name (MP2 / default): unknown version
Name (MP2 / aarch64): unknown version
Name (MP2 / x86_64): unknown version
Name (MP1 / default): unknown version
Name (MP1 / aarch64): unknown version
Name (MP1 / x86_64): unknown version
URL: [unknown version]
Path (MP2 / default): unknown version
Path (MP2 / aarch64): unknown version
Path (MP2 / x86_64): unknown version
Path (MP1 / default): unknown version
Path (MP1 / aarch64): unknown version
Path (MP1 / x86_64): unknown version

"QT SDK setup script" name, URL and path for the version of the X-LINUX-QT expansion package on top of the v5.1.0 ecosystem release
Name (default): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK setup script | request=name}}<br>
Name (MP2): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK setup script | device=MP2 | request=name}}<br>
Name (MP1): {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK setup script | device=MP1 | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK setup script | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version={{X-LINUXRelease/Revision | revision=5.1.0 | name=QT | type=release}} | package=QT SDK setup script | request=path}}

Name (default): unknown version
Name (MP2): unknown version
Name (MP1): unknown version
URL: [unknown version]
Path: unknown version


3. More examples[edit source]

You type You get
"AI Debian package" name, URL and path for an unspecified version requested
Name: {{X-LINUXRelease/Package | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | package=AI Debian package | request=path}}

Name: unknown version
URL: unknown version
Path: unknown version

"AI Debian package" name, URL and path for an unknown version requested
Name: {{X-LINUXRelease/Package | version=10.20.30 | package=AI Debian package | request=name}}<br>
URL: {{X-LINUXRelease/Package | version=10.20.30 | package=AI Debian package | request=url}}<br>
Path: {{X-LINUXRelease/Package | version=10.20.30 | package=AI Debian package | request=path}}

Name: unknown version
URL: unknown version
Path: unknown version

Unspecified package
Name: {{X-LINUXRelease/Package | version=latest | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | request=path}}

Name: unknown package
URL: [unknown package]
Path: unknown package

Unknown package
Name: {{X-LINUXRelease/Package | version=latest | package=not supported | request=name}}<br>
URL: [{{X-LINUXRelease/Package | version=latest | package=not supported | request=url}}]<br>
Path: {{X-LINUXRelease/Package | version=latest | package=not supported | request=path}}

Name: unknown package
URL: [unknown package]
Path: unknown package

Unspecified request
{{X-LINUXRelease/Package | version=latest | package=AI Debian package}}

unknown request

Unknown request
{{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=not supported}}

unknown request

Check that there's no space before and after the text
BEFORE{{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=name}}AFTER<br>
BEFORE[{{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=url}}]AFTER<br>
BEFORE{{X-LINUXRelease/Package | version=latest | package=AI Debian package | request=path}AFTER}

BEFOREapt-openstlinux-ai_1.0_arm64.debTBDAFTER
BEFORE[http://extra.packages.openstlinux.st.com/alpha/stm32mp2/AI/5.0/pool/config/a/apt-openstlinux-ai/TBD]AFTER
BEFORENAAFTER

4. Code[edit source]

unknown request

No categories assignedEdit