Approved version. Approved on: 15:59, 16 March 2023
- Last edited 2 weeks ago ago
U-Boot$
1 Usage[edit]
The U-Boot$ template is used to prefix a command that must be executed on the U-Boot console, with a U-Boot-specific prompt.
Thanks to the u-boot-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{U-Boot$}}
2 Basic examples[edit]
You type | You get |
---|---|
help env command executed on the U-Boot console
{{U-Boot$}}help env<br>
env - environment handling commands
|
help env |
3 More examples[edit]
You type | You get |
---|---|
2 commands executed on the U-Boot console and preformatted text block (space at the beginning of each line)
{{U-Boot$}}help env env - environment handling commands {{U-Boot$}}env default -a |
help env env - environment handling commands env default -a |
Command executed on the U-Boot console and preformatted text block (space at the beginning of each line)
{{U-Boot$}}help env
env - environment handling commands
|
help env env - environment handling commands |
Long command executed on the U-Boot console and preformatted text block (space at the beginning of each line)
{{U-Boot$}}this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed |
this is a so long command executed on the U-Boot console that a horizontal scrolling bar is needed
|
Template used within another public message box template
{{Info |
Message before the command
{{U-Boot$}}help env
env - environment handling commands
Message after the command
}}
|
|
Template used within another protected message box template
{{InternalInfo |
Message before the command
{{U-Boot$}}help env
env - environment handling commands
Message after the command
}}
|
4 Maintenance[edit]
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5 Code[edit]