1. Usage[edit source]
The STM32MP23Message template is used to insert a message about the usage of the STM32MP257F-DK Discovery kit to evaluate the STM32MP23x lines
.
Usage: {{STM32MP23Message}}
The returned value is the generic message to insert.
2. Basic examples[edit source]
You type | You get |
---|---|
Generic message
{{STM32MP23Message}} |
To help you get started with the evaluation of the STM32MP23x product lines, you can rely on the STM32MP257F-DK Discovery kit, and the applicable STM32 MPU embedded software, running with the STM32MP23 software configuration (peripherals, features, and performance). |
3. More examples[edit source]
You type | You get |
---|---|
Check that there's no space before and after the text
BEFORE{{STM32MP23Message}}AFTER |
BEFORETo help you get started with the evaluation of the STM32MP23x product lines, you can rely on the STM32MP257F-DK Discovery kit, and the applicable STM32 MPU embedded software, running with the STM32MP23 software configuration (peripherals, features, and performance).AFTER |
Check that the message can be used with an info box
Text completed by an info box<span title="{{STM32MP23Message}}"><sup>[[File:Info.png|13px]]</sup></span> |
|
Use the message in another template
{{Important|{{STM32MP23Message}}}} |
|
4. Code[edit source]
To help you get started with the evaluation of the STM32MP23x product lines, you can rely on the STM32MP257F-DK Discovery kit, and the applicable STM32 MPU embedded software, running with the STM32MP23 software configuration (peripherals, features, and performance).