- Last edited one year ago ago
STLightGreen
1 Usage
The STLightGreen template is used to color text in pages, with the STMicroelectronics corporate primary color shade of light green (█).
Usage: {{STLightGreen|<text to color>|tint=<tint>}}
Where:
- <text to color> is the text to format in light green. If this template is called with no text, the hexadecimal code of the color is returned.
- <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
- 75: 75% of the original color tint
- 50: 50% of the original color tint
- 25: 25% of the original color tint
2 Basic examples
You type | You get |
---|---|
Coloring text in light green
This is a {{STLightGreen|STMicroelectronics corporate color: shade of light green: █}} |
This is a STMicroelectronics corporate color: shade of light green: █ |
Coloring text in 75% tint of light green
This is a {{STLightGreen|STMicroelectronics corporate color: 75% tint of light green: █ | tint=75}} |
This is a STMicroelectronics corporate color: 75% tint of light green: █ |
Coloring text in 50% tint of light green
This is a {{STLightGreen|STMicroelectronics corporate color: 50% tint of light green: █ | tint=50}} |
This is a STMicroelectronics corporate color: 50% tint of light green: █ |
Coloring text in 25% tint of light green
This is a {{STLightGreen|STMicroelectronics corporate color: 25% tint of light green: █ | tint=25}} |
This is a STMicroelectronics corporate color: 25% tint of light green: █ |
Getting the hexadecimal code of the color
{{STLightGreen}} is the hexadecimal code of STMicroelectronics light green. |
#49B170 is the hexadecimal code of STMicroelectronics light green. |
Getting the hexadecimal code of the 75% tint of the color
{{STLightGreen | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of light green. |
#77C594 is the hexadecimal code of STMicroelectronics 75% tint of light green. |
Getting the hexadecimal code of the 50% tint of the color
{{STLightGreen | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of light green. |
#A4D8B7 is the hexadecimal code of STMicroelectronics 50% tint of light green. |
Getting the hexadecimal code of the 25% tint of the color
{{STLightGreen | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of light green. |
#C7E7D3 is the hexadecimal code of STMicroelectronics 25% tint of light green. |
3 More examples
You type | You get |
---|---|
light green and bold
This is a {{STLightGreen|'''STMicroelectronics'''}} corporate color: '''{{STLightGreen|shade of light green: █}}''' |
This is a STMicroelectronics corporate color: shade of light green: █ |
light green and italic
This is a {{STLightGreen|''STMicroelectronics''}} corporate color: ''{{STLightGreen|shade of light green: █}}'' |
This is a STMicroelectronics corporate color: shade of light green: █ |
4 Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5 Code
#49B170