- Last edited 7 months ago ago
STDarkBlue
1 Usage
The STDarkBlue template is used to color text in pages, with the STMicroelectronics corporate primary color shade of dark blue (█).
Where:
Usage: {{STDarkBlue|<text to color>|tint=<tint>}}
- <text to color> is the text to format in dark blue. If this template is called with no text, the hexadecimal code of the color is returned.
- <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
- 75: 75% of the original color tint
- 50: 50% of the original color tint
- 25: 25% of the original color tint
2 Basic examples
You type | You get |
---|---|
Coloring text in dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: shade of dark blue: █}} |
This is a STMicroelectronics corporate color: shade of dark blue: █ |
Coloring text in 75% tint of dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: 75% tint of dark blue: █ | tint=75}} |
This is a STMicroelectronics corporate color: 75% tint of dark blue: █ |
Coloring text in 50% tint of dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: 50% tint of dark blue: █ | tint=50}} |
This is a STMicroelectronics corporate color: 50% tint of dark blue: █ |
Coloring text in 25% tint of dark blue
This is a {{STDarkBlue|STMicroelectronics corporate color: 25% tint of dark blue: █ | tint=25}} |
This is a STMicroelectronics corporate color: 25% tint of dark blue: █ |
Getting the hexadecimal code of the color
{{STDarkBlue}} is the hexadecimal code of STMicroelectronics dark blue. |
#03234B is the hexadecimal code of STMicroelectronics dark blue. |
Getting the hexadecimal code of the 75% tint of the color
{{STDarkBlue | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of dark blue. |
#425A78 is the hexadecimal code of STMicroelectronics 75% tint of dark blue. |
Getting the hexadecimal code of the 50% tint of the color
{{STDarkBlue | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of dark blue. |
#8191A5 is the hexadecimal code of STMicroelectronics 50% tint of dark blue. |
Getting the hexadecimal code of the 25% tint of the color
{{STDarkBlue | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of dark blue. |
#BDC5D0 is the hexadecimal code of STMicroelectronics 25% tint of dark blue. |
3 More examples
You type | You get |
---|---|
Dark blue and bold
This is a {{STDarkBlue|'''STMicroelectronics'''}} corporate color: '''{{STDarkBlue|shade of dark blue: █}}''' |
This is a STMicroelectronics corporate color: shade of dark blue: █ |
Dark blue and italic
This is a {{STDarkBlue|''STMicroelectronics''}} corporate color: ''{{STDarkBlue|shade of dark blue: █}}'' |
This is a STMicroelectronics corporate color: shade of dark blue: █ |
4 Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5 Code
#03234B