This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 Usage[edit source]
The STM32CubeRelease/Revision template returns the status for an STM32Cube release revision , or the revision (x.y.z) of the latest STM32Cube release.
Usage: {{STM32CubeRelease/Revision | revision=<revision>}}
Where:
- <revision> is the mandatory revision of the STM32Cube release for which a status is requested. The possible values are:
- latest to get the revision (x.y.z) of the latest major STM32Cube release.
- 1.16.0 (Mar 2024 major STM32Cube release revision).
- 1.15.0 (Nov 2023 major STM32Cube release revision).
The returned value (aka status) is:
- x.y.z (revision of the latest STM32Cube release), if <revision> is set to latest.
- latest, if <revision> is the latest one, in the flow associated with this wiki.
- legacy, if <revision> is a legacy one, in the flow associated with this wiki.
- next, if <revision> is a planned one, in the flow associated with this wiki.
- former, if <revision> is part of a former flow that is not the one associated with this wiki.
- unknown, if <revision> is not supported.
2 Basic examples[edit source]
You type | You get |
---|---|
v1.16.0 revision (latest)
{{STM32CubeRelease/Revision | revision=1.16.0}} |
latest |
v1.15.0 revision
{{STM32CubeRelease/Revision | revision=1.15.0}} |
legacy |
Latest revision
{{STM32CubeRelease/Revision | revision=latest}} |
1.16.0 |
Former revisions
{{STM32CubeRelease/Revision | revision=0.1.0}}<br /> |
unknown |
3 More examples[edit source]
You type | You get |
---|---|
vx.0.0 revision (legacy)
{{STM32CubeRelease/Revision | revision=x.0.0}} |
legacy |
vx.1.0 revision (latest)
{{STM32CubeRelease/Revision | revision=x.1.0}} |
latest |
vx.2.0 revision (next)
{{STM32CubeRelease/Revision | revision=x.2.0}} |
next |
v0.y.0 revision (former)
{{STM32CubeRelease/Revision | revision=0.y.0}} |
former |
Unknown revision
{{STM32CubeRelease/Revision | revision=10.20.30}} |
unknown |
Unspecified revision
{{STM32CubeRelease/Revision}} |
unknown |
4 Code[edit source]
unknown