1 Usage
The STM32CubeRelease/Component template returns the version of a software/tool component delivered by an STM32Cube release revision.
Usage: {{STM32CubeRelease/Component | revision=<revision> | component=<component> | name=<name>}}
Where:
- <revision> is the mandatory revision of the STM32Cube release, for which the version of the software/tool component is requested.
- The possible values for this parameter are available in the STM32CubeRelease/Revision template.
- <component> is the mandatory software/tool component delivered by the STM32Cube release revision, for which the version of the component is requested. The possible values are:
- STM32CubeMP13
- STM32CubeMP1
- STM32CubeIDE
- STM32CubeMX
- STM32CubeProgrammer
- <name> is the optional parameter that allows to select the way the version is displayed. Per default (if <name> is not set), the software/tool component full name is displayed. The possible values for <name> are:
- tag: the software/tool component tag (e.g., "x.y.z") is displayed
- release: the software/tool component release (e.g., "x.y.z") is displayed
The returned value is:
- a string that contains the version of the software/tool component delivered by the STM32Cube release revision.
- an empty string, if the software/tool component is not delivered by the STM32Cube release revision.
- "unknown revision", if <revision> is not supported.
- "unknown component", if <component> is not supported.
2 Basic examples
You type | You get |
---|---|
All components for the v1.15.0 revision requested
Full names:<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMP1}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMP13}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeIDE}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeProgrammer}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMX}}<br /> Tag names:<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMP1 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMP13 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeIDE | name=tag}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeProgrammer | name=tag}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMX | name=tag}}<br /> Release names:<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMP1 | name=release}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMP13 | name=release}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeIDE | name=release}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeProgrammer | name=release}}<br /> {{STM32CubeRelease/Component | revision=1.15.0 | component=STM32CubeMX | name=release}}<br /> |
Full names: |
All components for the latest revision requested
{{STM32CubeRelease/Component | revision=latest| component=STM32CubeMP1}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMP13}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeIDE}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeProgrammer}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMX}}<br /> Tag names:<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMP1 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMP13 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeIDE | name=tag}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeProgrammer | name=tag}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMX | name=tag}}<br /> Release names:<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMP1 | name=release}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMP13 | name=release}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeIDE | name=release}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeProgrammer | name=release}}<br /> {{STM32CubeRelease/Component | revision=latest | component=STM32CubeMX | name=release}}<br /> |
STM32CubeMP1 Package v1.6.0 |
3 More examples
You type | You get |
---|---|
STM32CubeMP13 version for the vx.0.0 revision (legacy) requested
Full names:<br /> {{STM32CubeRelease/Component | revision=x.0.0 | component=STM32CubeMP13}}<br /> Tag names:<br /> {{STM32CubeRelease/Component | revision=x.0.0 | component=STM32CubeMP13 | name=tag}}<br /> Release names:<br /> {{STM32CubeRelease/Component | revision=x.0.0 | component=STM32CubeMP13 | name=release}}<br /> |
Full names: |
STM32CubeMP13 version for vx.1.0 revision (latest) requested
{{STM32CubeRelease/Component | revision=x.1.0 | component=STM32CubeMP13}}<br /> {{STM32CubeRelease/Component | revision=x.1.0 | component=STM32CubeMP13 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=x.1.0 | component=STM32CubeMP13 | name=release}} |
STM32CubeMP13 Package vx.y.z |
STM32CubeMP13 version for vx.2.0 revision (next) requested
{{STM32CubeRelease/Component | revision=x.2.0 | component=STM32CubeMP13}}<br /> {{STM32CubeRelease/Component | revision=x.2.0 | component=STM32CubeMP13 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=x.2.0 | component=STM32CubeMP13 | name=release}} |
STM32CubeMP13 Package vx.y.z |
STM32CubeMP13 version for v0.y.0 revision (former) requested
{{STM32CubeRelease/Component | revision=0.y.0 | component=STM32CubeMP13}}<br /> {{STM32CubeRelease/Component | revision=0.y.0 | component=STM32CubeMP13 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=0.y.0 | component=STM32CubeMP13 | name=release}} |
unknown revision |
STM32CubeMP13 version for an unspecified revision requested
Full names:<br /> {{STM32CubeRelease/Component | component=STM32CubeMP13}}<br /> Tag names:<br /> {{STM32CubeRelease/Component | component=STM32CubeMP13 | name=tag}}<br /> Release names:<br /> {{STM32CubeRelease/Component | component=STM32CubeMP13 | name=release}}<br /> |
Full names: |
STM32CubeMP13 version for an unknown revision requested
Full names:<br /> {{STM32CubeRelease/Component | revision=10.20.30 | component=STM32CubeMP13}}<br /> Tag names:<br /> {{STM32CubeRelease/Component | revision=10.20.30 | component=STM32CubeMP13 | name=tag}}<br /> Release names:<br /> {{STM32CubeRelease/Component | revision=10.20.30 | component=STM32CubeMP13 | name=release}}<br /> |
Full names: |
Unspecified component
{{STM32CubeRelease/Component | revision=x.0.0}}<br /> {{STM32CubeRelease/Component | revision=x.0.0 | name=tag}}<br /> {{STM32CubeRelease/Component | revision=x.0.0 | name=release}} |
unknown component |
Unknown component
{{STM32CubeRelease/Component | revision=x.0.0 | component=not supported}}<br /> {{STM32CubeRelease/Component | revision=x.0.0 | component=not supported | name=tag}}<br /> {{STM32CubeRelease/Component | revision=x.0.0 | component=not supported | name=release}} |
unknown component |
Unknown value for name: the full name is displayed
{{STM32CubeRelease/Component | revision=x.0.0 | component=STM32CubeMP13 | name=version}} |
STM32CubeMP13 Package vx.y.z |
4 Code
unknown component