Difference between revisions of "Subpart - STM32MP15 - Starter Package"
[quality revision] | [quality revision] |
m
|
Lionel Vitte (talk | contribs)
m
|
Contents
- 1 Article purpose
- 2 Checking the boot sequence
- 3 Mouse, keyboard and Ethernet hot-plugs
- 4 Remote and local Terminal programs
- 5 Executing basic commands
1 Article purpose[edit]
This article gathers the information that applies to any STM32MP15 board.
![]() |
To start efficiently the board, it's recommended to go through the Starter Package article relative to your board: Category:Starter Package |
That's the reason why the steps 2, 3 and 6 referenced in this article depend on the considered board:
- Step 2 is either STM32MP15 Evaluation boards - Starter Package#step2 or STM32MP15 Discovery kits - Starter Package#step2
- Step 3 is either STM32MP15 Evaluation boards - Starter Package#step3 or STM32MP15 Discovery kits - Starter Package#step3
- Step 6 is either STM32MP15 Evaluation boards - Starter Package#step6 or STM32MP15 Discovery kits - Starter Package#step6
2 Checking the boot sequence[edit]
Assuming you have performed the optional step 6 above, the information (coming successively from the U-Boot and the Linux operating system that is booting on the board), should be displayed on the host PC Terminal.
![]() |
The information displayed below might differ from that on your own application, and should just be considered an example. |
In parallel, a U-Boot splash screen picture is displayed on the DSI display (if one is connected to the board).
A user space graphical boot splash screen (PSplash) picture is then briefly displayed on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).
When the boot process is complete, the launcher application is shown on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).
More detail about this launcher application in GTK demo launcher page.
3 Mouse, keyboard and Ethernet hot-plugs[edit]
Let's assume that the optional step 2 and step 3 were not achieved when setting up the system above.
When connecting a USB mouse, the following information is displayed by the Terminal program:
[ 926.786326] usb 2-1.1: new low-speed USB device number 3 using ehci-platform [ 926.961413] input: Logitech Optical USB Mouse as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.1/2-1.1:1.0/0003:046D:C016.0001/input/input2 [ 926.975098] hid-generic 0003:046D:C016.0001: input: USB HID v1.10 Mouse [Logitech Optical USB Mouse] on usb-5800d000.usbh-ehci-1.1/input0
When connecting a USB keyboard, the following information is displayed by the Terminal program:
[ 1009.026567] usb 2-1.3: new low-speed USB device number 4 using ehci-platform [ 1009.193990] input: Dell Dell USB Keyboard as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.3:1.0/0003:413C:2003.0002/input/input3 [ 1009.280101] hid-generic 0003:413C:2003.0002: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-5800d000.usbh-ehci-1.3/input0
When connecting an Ethernet cable, the following information is displayed by the Terminal program:
[ 1215.356377] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx [ 1215.363377] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 1215.391068] Link is Up - 1000/Half
4 Remote and local Terminal programs[edit]
As already explained in the step 6 above, a remote Terminal program can be installed and configured on your host PC in order to communicate with the board through a serial link or an Ethernet link: see How to get Terminal.
The remote Terminal on your host PC can be used to enter command lines, as shown below with the ifconfig command to query the network interface parameters:
A local Terminal program can be launched directly on the board. Click on the small icon at the top left corner of the display (see the red arrow on the figure below):
Then the on-board Wayland Terminal can be used to directly enter command lines as shown below, still with the ip addr command to query the network interface parameters:
Consequently, unless an explicit restriction is mentioned, command lines can be run from both Terminals.
Note: in this article, any command executed on the board (through the remote Terminal or the Wayland Terminal) starts with , while any command executed on the host PC starts with .
5 Executing basic commands[edit]
![]() |
The outputs of the commands executed below are examples; the outputs obtained might differ. |
5.1 Having a look at the OpenSTLinux directory structure[edit]
The directory structure and directory contents in the OpenSTLinux distribution is standard. Some details are available in the OpenSTLinux directory structure article.
5.2 Identifying the software running on board[edit]
![]() |
Obviously, what you obtain might differ from what is displayed on the Output example column. |
5.2.1 For ecosystem release v1 v3.1.0
[edit]
Software | How to get its version | Output example |
---|---|---|
TF-A | TF-A Version number |
NOTICE: BL2: v2. |
4- |
r2. |
0(debug):v2. |
4- |
dirty |
|
U-Boot | See the version displayed in the console |
2020.10-stm32mp- |
r2 [...] |
||
Linux kernel |
cat /proc/version
|
Linux version |
5. |
10. |
61 (xxxx@yyyy) ( |
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) [...] |
||
GCC |
cat /proc/version
|
Linux version |
5. |
10. |
61 (xxxx@yyyy) ( |
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0) [...] |
|
Yocto Project |
|
grep DISTRO_ |
CODENAME /etc/build
|
DISTRO_CODENAME = dunfell |
|
Weston |
weston --version
|
weston |
8.0.0 |
||
GStreamer |
gst-play-1.0 --version
|
GStreamer 1. |
16. |
3 |
||
GPU |
cat /sys/kernel/debug/gc/version
|
6. |
4. |
3. |
279124 built [...] |
5.2.2 For ecosystem release
v1
v3.0.0
[edit]
Software | How to get its version | Output example |
---|---|---|
TF-A | TF-A Version number |
NOTICE: BL2: v2.4-r1.0(debug):v2. |
4-dirty |
|
U-Boot | See the version displayed in the console |
2020.10-stm32mp- |
r1 [...] |
||
Linux kernel |
cat /proc/version
|
Linux version |
5. |
10. |
10 (xxxx@yyyy) ( |
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) [...] |
||
GCC |
cat /proc/version
|
Linux version |
5. |
10. |
10 (xxxx@yyyy) ( |
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0) [...] |
|
Yocto Project |
|
grep DISTRO_ |
CODENAME /etc/build
|
DISTRO_CODENAME = dunfell |
|
Weston |
weston --version
|
weston |
8.0.0 |
||
GStreamer |
gst-play-1.0 --version
|
GStreamer 1. |
16. |
3 |
||
GPU |
cat /sys/kernel/debug/gc/version
|
6. |
4. |
3. |
279124 built [...] |
5.3 Configuration tips[edit]
5.4 Getting board IP address[edit]
Prerequisite: your board is connected to your local network through the Ethernet connector (see step 3).
- Get the IP address of your board with the ip Linux command line (recommended method):
ip addr show eth0
3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff
inet xx.xx.xx.xx/xx brd xx.xx.xx.xx scope global dynamic eth0
valid_lft 159045sec preferred_lft 159045sec
inet6 xxxx::xx:xx:xx:xx/xx scope link
valid_lft forever preferred_lft forever
- Get the IP address of your board with the ifconfig Linux command line (a deprecated but well-known command):
ifconfig eth0
eth0 Link encap:Ethernet HWaddr xx:xx:xx:xx:xx:xx
inet addr:xx.xx.xx.xx Bcast:xx.xx.xx.xx Mask:255.255.252.0
inet6 addr: xxxx::xx:xx:xx:xx/xx Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:2619 errors:0 dropped:0 overruns:0 frame:0
TX packets:1311 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:353250 (344.9 KiB) TX bytes:118305 (115.5 KiB)
Interrupt:247
5.5 Copying a file from your host PC to your board (and reciprocally)[edit]
- How to transfer a file over network (recommended method)
5.6 Miscellaneous commands[edit]
![]() |
The outputs of the commands executed below are examples; the outputs that you obtain might differ. |
5.6.1 Printing distribution specific information[edit]
lsb_release -a LSB Version: core-5.0-noarch:core-5.0-arm Distributor ID: openstlinux-weston Description: cat /etc/os-release ID=openstlinux-weston NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro)" 2.6-... Release: 2.6... Codename: thud
Where:
VERSION="3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)"
VERSION_ID=3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17
PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)"
Where:
ID | A lower-case string identifying the operating system |
NAME | A string identifying the operating system |
VERSION | A string identifying the operating system version, including a release code name |
VERSION_ID | A lower case string identifying the operating system version |
PRETTY_NAME | A full pretty name of the release |
5.6.2 Printing system information[edit]
uname -a Linux stm32mp1 45.1910.4961 #1 SMP PREEMPT SunThu JunAug 926 0712:1751:2521 UTC 20192021 armv7l armv7l armv7l GNU/Linux
Where:
Linux | Kernel name |
stm32mp1 | Network node hostname |
45.1910.4961 | Kernel release |
#1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019Thu Aug 26 12:51:21 UTC 2021 | Kernel version |
armv7l | Machine hardware name |
GNU/Linux | Operating system |
5.6.3 Printing Linux kernel and GCC versions[edit]
cat /proc/version Linux version 45.1910.4961 (xxxx@yyyyoe-user@oe-host) (arm-ostl-linux-gnueabi-gcc version(GCC) 89.23.0, (GCC)GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT SunThu JunAug 926 0712:1751:2521 UTC 20192021
Where:
Linux | Kernel name |
version 45.1910.4961 | Kernel release |
(xxxx@yyyy) | Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened |
(gcc version 8.2.0 (GCC) )arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) | Version of the GCC compiler used to compile the kernel |
#1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019Thu Aug 26 12:51:21 UTC 2021 | Kernel version; type of kernel (SMP) and date and time of the kernel compilation |
5.6.4 Printing the amount of disk space available on all mounted file systems[edit]
df -h Filesystem Size Used Avail Use% Mounted on /dev/root 719M 342M 339M 51% / devtmpfs 372M 0 372M 0% /dev tmpfs 436M 0 436M 0% /dev/shm tmpfs 436M 14M 423M 4% /run tmpfs 436M 0 436M 0% /sys/fs/cgroup tmpfs 436M 4.0K 436M 1% /tmp /dev/mmcblk0p4 58M 8.2M 46M 16% /boot /dev/mmcblk0p7 6.4G 68M 6.1G 2% /usr/local tmpfs 436M 128K 436M 1% /var/volatile /dev/mmcblk0p5 15M 8.2M 5.3M 61% /vendor tmpfs 88M 0 88M 0% /run/user/0
Where:
Filesystem | Source of the mount point, usually a device |
Size | Total size in human readable format (e.g. 1K, 234M, 2G) |
Used | Used size in human readable format |
Available | Available size in human readable format |
Use% | Percentage of used size divided by the total size |
Mounted on | Mount point |
Note: the user file system (userfs) and the boot file system (bootfs) are accessible respectively through the /usr/local mounting point, and the /boot mounting point (see Flash partitions for a description of the file systems).
<noinclude>__NOINDEX__ ==Article purpose== This article gathers the information that applies to any STM32MP15 board. {{Warning|To start efficiently the board, it's recommended to go through the Starter Package article relative to your board: [[:Category:Starter Package]]}} That's the reason why the steps 2, 3 and 6 referenced in this article depend on the considered board:{{UpdateNeededForNewBoard|Point to the steps of the new board Starter Package}} * <span id{{=}}"step2">'''Step 2'''</span> is either [[STM32MP15 Evaluation boards - Starter Package#step2]] or [[STM32MP15 Discovery kits - Starter Package#step2]] * <span id{{=}}"step3">'''Step 3'''</span> is either [[STM32MP15 Evaluation boards - Starter Package#step3]] or [[STM32MP15 Discovery kits - Starter Package#step3]] * <span id{{=}}"step6">'''Step 6'''</span> is either [[STM32MP15 Evaluation boards - Starter Package#step6]] or [[STM32MP15 Discovery kits - Starter Package#step6]]</noinclude> ==Checking the boot sequence== Assuming you have performed the optional [[#step6|step 6]] above, the information (coming successively from the U-Boot and the Linux operating system that is booting on the board), should be displayed on the host PC Terminal. {{Info|The information displayed below might differ from that on your own application, and should just be considered an example.}} [[File: STM32MP15_boot_information_1.png|thumb|upright=4|center|link=|First information scrolled on the remote Terminal during boot]] [[File: STM32MP15_boot_information_2.png|thumb|upright=4|center|link=|Last information scrolled on the remote Terminal during boot]] In parallel, a U-Boot splash screen picture is displayed on the DSI display (if one is connected to the board).[[File:DSI_U-Boot_splash_screen.png|link=]] A user space graphical boot splash screen (PSplash) picture is then briefly displayed on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board).[[File:DSI_user_splash_screen.png|link=]] When the boot process is complete, the launcher application is shown on the HDMI monitor if one is connected to the board, or otherwise on the DSI display (if one is connected to the board). [[File: STM32MP15_launcher_main_menu.png|thumb|upright=4|center|link=|launcher application layer shown on the HDMI monitor or on the DSI display]] More detail about this launcher application in [[GTK demo launcher]] page. ==Mouse, keyboard and Ethernet hot-plugs== Let's assume that the optional [[#step2|step 2]] and [[#step3|step 3]] were not achieved when setting up the system above. When connecting a USB mouse, the following information is displayed by the Terminal program: [ 926.786326] usb 2-1.1: new low-speed USB device number 3 using ehci-platform [ 926.961413] input: Logitech Optical USB Mouse as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.1/2-1.1:1.0/0003:046D:C016.0001/input/input2 [ 926.975098] hid-generic 0003:046D:C016.0001: input: USB HID v1.10 Mouse [Logitech Optical USB Mouse] on usb-5800d000.usbh-ehci-1.1/input0 <br> When connecting a USB keyboard, the following information is displayed by the Terminal program: [ 1009.026567] usb 2-1.3: new low-speed USB device number 4 using ehci-platform [ 1009.193990] input: Dell Dell USB Keyboard as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.3:1.0/0003:413C:2003.0002/input/input3 [ 1009.280101] hid-generic 0003:413C:2003.0002: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-5800d000.usbh-ehci-1.3/input0 <br> When connecting an Ethernet cable, the following information is displayed by the Terminal program: [ 1215.356377] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx [ 1215.363377] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready [ 1215.391068] Link is Up - 1000/Half ==Remote and local Terminal programs== As already explained in the [[#step6|step 6]] above, a '''remote Terminal''' program can be installed and configured on your host PC in order to communicate with the board through a serial link or an Ethernet link: see [[How to get Terminal]]. The remote Terminal on your host PC can be used to enter command lines, as shown below with the ''ifconfig'' command to query the network interface parameters: [[File: STM32MP15_example_command_remote_terminal.png|thumb|upright=4|center|link=|Example of command (''ifconfig'') executed on the remote Terminal program]]<br> A '''local Terminal''' program can be launched directly on the board. Click on the small icon at the top left corner of the display (see the red arrow on the figure below): [[File: STM32MP15_local_terminal_icon.png|thumb|upright=4|center|link=|Icon to launch a local Terminal program]] [[File: STM32MP15_wayland_terminal.png|thumb|upright=4|center|link=|Wayland Terminal program]]<br> Then the on-board Wayland Terminal can be used to directly enter command lines as shown below, still with the ''ip addr'' command to query the network interface parameters: [[File: STM32MP15_example_command_local_terminal.png|thumb|upright=4|center|link=|Example of command (''ip addr'') executed on the Wayland Terminal program]]<br> Consequently, unless an explicit restriction is mentioned, command lines can be run from both Terminals. Note: in this article, any command executed on the board (through the remote Terminal or the Wayland Terminal) starts with {{Board$}}, while any command executed on the host PC starts with {{PC$}}. ==Executing basic commands== {{Info|The outputs of the commands executed below are examples; the outputs obtained might differ.}} ===Having a look at the OpenSTLinux directory structure=== The directory structure and directory contents in the OpenSTLinux distribution is standard. Some details are available in the [[OpenSTLinux directory structure]] article. ===Identifying the software running on board=== {{Info|Obviously, what you obtain might differ from what is displayed on the ''Output example'' column.}} {{UpdateNeededForNewRelease|The "Output example" column below shall be updated periodically, even if the information banner specifies that this column might not be up-to-date}} ======For {{EcosystemRelease | revision=13.1.0 }}====== {| class="wikitable" ! Software !! st-table" ! style="text-align:center;" |Software !! style="text-align:center;" |How to get its version !! style="text-align:center;" |Output example |- | TF-A || [[TF-A - How to debug#TF-A How to debug TF-A BL2#TF-A Version number|TF-A Version number]] || NOTICE: BL2: v2.0-r1.54-r2.0(debug):{{Highlight|v2.0-r1.54-dirty}} |- | U-Boot || See the version displayed in the console || {{Highlight|U-Boot 2018.11-stm32mp-r32020.10-stm32mp-r2}} [...] |- | Linux kernel || {{Board$}} cat /proc/version || {{Highlight|Linux version 4.19.495.10.61}} (xxxx@yyyy) (gcc version 8.2.0 (GCC))arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) [...] |- | GCC || {{Board$}} cat /proc/version || Linux version 4.19.495.10.61 (xxxx@yyyy) ({{Highlight|gcc version 8.2.0 (GCC)}}) [...] |- | Yocto Project || {{Board$}} lsb_release -c || Codename: {{Highlight|thudarm-ostl-linux-gnueabi-gcc (GCC) 9.3.0}}) [...] |- | Yocto Project || {{Board$}} grep DISTRO_CODENAME /etc/build || DISTRO_CODENAME = {{Highlight|dunfell}} |- | Weston || {{Board$}} weston --version || {{Highlight|weston 58.0.0}} |- | GStreamer || {{Board$}} gst-play-1.0 --version || {{Highlight|GStreamer 1.14.416.3}} |- | GPU || {{Board$}} cat /sys/kernel/debug/gc/version || {{Highlight|6.2.4.p4.1900763.279124}} built [...] |}<div class="mw-collapsible mw-collapsed"> ======For {{EcosystemRelease | revision=13.0.0}}======<div class="mw-collapsible-content"> {| class="wikitable" ! Software !! }}====== {| class="st-table" ! style="text-align:center;" |Software !! style="text-align:center;" |How to get its version !! style="text-align:center;" |Output example |- | TF-A || [[TF-A - How to debug#TF-A How to debug TF-A BL2#TF-A Version number|TF-A Version number]] || NOTICE: BL2: v2.4-r1.0(debug):{{Highlight|v2.04-dirty}} |- | U-Boot || See the version displayed in the console || {{Highlight|U-Boot 2018.11-stm32mp-r22020.10-stm32mp-r1}} [...] |- | Linux kernel || {{Board$}} cat /proc/version || {{Highlight|Linux version 4.19.95.10.10}} (xxxx@yyyy) (gcc version 8.2.0 (GCC))arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) [...] |- | GCC || {{Board$}} cat /proc/version || Linux version 4.19.95.10.10 (xxxx@yyyy) ({{Highlight|gcc version 8.2.0 (GCC)}}) [...] |- | Yocto Project || {{Board$}} lsb_release -c || Codename: {{Highlight|thudarm-ostl-linux-gnueabi-gcc (GCC) 9.3.0}}) [...] |- | Yocto Project || {{Board$}} grep DISTRO_CODENAME /etc/build || DISTRO_CODENAME = {{Highlight|dunfell}} |- | Weston || {{Board$}} weston --version || {{Highlight|weston 58.0.0}} |- | GStreamer || {{Board$}} gst-play-1.0 --version || {{Highlight|GStreamer 1.14.216.3}} |- | GPU || {{Board$}} cat /sys/kernel/debug/gc/version || {{Highlight|6.2.4.p3.1743153.279124}} built [...] |} </div></div> ===Configuration tips=== * [[Wayland Weston overview#Configuration|Configure the keyboard layout (qwerty, azerty...)]] ===Getting board IP address=== Prerequisite: your board is connected to your local network through the Ethernet connector (see [[#step3|step 3]]). * Get the IP address of your board with the [[IP Linux command line|''ip'' Linux command line]] ({{highlight|recommended method}}): {{Board$}} ip addr show eth0 3: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000 link/ether xx:xx:xx:xx:xx:xx brd ff:ff:ff:ff:ff:ff inet {{highlight|xx.xx.xx.xx}}/xx brd xx.xx.xx.xx scope global dynamic eth0 valid_lft 159045sec preferred_lft 159045sec inet6 xxxx::xx:xx:xx:xx/xx scope link valid_lft forever preferred_lft forever * Get the IP address of your board with the [[Ifconfig|''ifconfig'']] Linux command line (a deprecated but well-known command): {{Board$}} ifconfig eth0 eth0 Link encap:Ethernet HWaddr xx:xx:xx:xx:xx:xx inet addr:{{highlight|xx.xx.xx.xx}} Bcast:xx.xx.xx.xx Mask:255.255.252.0 inet6 addr: xxxx::xx:xx:xx:xx/xx Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:2619 errors:0 dropped:0 overruns:0 frame:0 TX packets:1311 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:353250 (344.9 KiB) TX bytes:118305 (115.5 KiB) Interrupt:247 ===Copying a file from your host PC to your board (and reciprocally)=== * [[How to transfer a file over network]] ({{highlight|recommended method}}) * [[How to transfer a file over serial console]] ===Miscellaneous commands=== {{Info|The outputs of the commands executed below are examples; the outputs that you obtain might differ.}}{{UpdateNeededForNewRelease|The outputs of the commands below shall be updated periodically, even if the information banner specifies that these outputs might not be up-to-date}} ====Printing distribution specific information==== {{Board$}} lsb_release -a LSB Version: core-5.0-noarch:core-5.0-arm Distributor ID: openstlinux-weston Description: cat /etc/os-release ID=openstlinux-weston NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 2.6-... Release: 2.6... Codename: thud Where: {| | LSB Version || Version of LSB (Linux Standard Base) against which distribution is compliant |- | Distributor ID || String identifier of distributor |- | Description || Single line text description of distribution |- | Release || Release number of distribution |- | Codename || Codename according to distribution " VERSION="3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)" VERSION_ID=3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)" Where: {| | ID || A lower-case string identifying the operating system |- | NAME || A string identifying the operating system |- | VERSION || A string identifying the operating system version, including a release code name |- | VERSION_ID || A lower case string identifying the operating system version |- | PRETTY_NAME || A full pretty name of the release |} ====Printing system information==== {{Board$}} uname -a Linux stm32mp1 4.19.495.10.61 #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019 armv7l armv7l Thu Aug 26 12:51:21 UTC 2021 armv7l armv7l armv7l GNU/Linux Where: {| | Linux || Kernel name |- | stm32mp1 || Network node hostname |- | 4.19.495.10.61 || Kernel release |- | #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019Thu Aug 26 12:51:21 UTC 2021 || Kernel version |- | armv7l || Machine hardware name |- | GNU/Linux || Operating system |} ====Printing Linux kernel and GCC versions==== {{Board$}} cat /proc/version Linux version 4.19.49 (xxxx@yyyy) (gcc version 8.2.0 (GCC)) #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 20195.10.61 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 Where: {| | Linux || Kernel name |- | version 4.19.495.10.61 ||Kernel release |- | (xxxx@yyyy) || Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened |- | (gcc version 8.2.0 (GCC) ) arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) || Version of the GCC compiler used to compile the kernel |- | #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019Thu Aug 26 12:51:21 UTC 2021 || Kernel version; type of kernel (SMP) and date and time of the kernel compilation |} ====Printing the amount of disk space available on all mounted file systems==== {{Board$}} df -h Filesystem Size Used Avail Use% Mounted on /dev/root 719M 342M 339M 51% / devtmpfs 372M 0 372M 0% /dev tmpfs 436M 0 436M 0% /dev/shm tmpfs 436M 14M 423M 4% /run tmpfs 436M 0 436M 0% /sys/fs/cgroup tmpfs 436M 4.0K 436M 1% /tmp /dev/mmcblk0p4 58M 8.2M 46M 16% /boot /dev/mmcblk0p7 6.4G 68M 6.1G 2% /usr/local tmpfs 436M 128K 436M 1% /var/volatile /dev/mmcblk0p5 15M 8.2M 5.3M 61% /vendor tmpfs 88M 0 88M 0% /run/user/0 Where: {| | Filesystem || Source of the mount point, usually a device |- | Size || Total size in human readable format (e.g. 1K, 234M, 2G) |- | Used ||Used size in human readable format |- | Available || Available size in human readable format |- | Use% ||Percentage of used size divided by the total size |- | Mounted on || Mount point |} <br> Note: the user file system (userfs) and the boot file system (bootfs) are accessible respectively through the ''/usr/local'' mounting point, and the ''/boot'' mounting point (see [[STM32MP15 Flash mapping#Flash partitions|Flash partitions]] for a description of the file systems). <noinclude> {{NoIndex}}[[Category:Sub-articles]] </noinclude>
(13 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
− | <noinclude> |
+ | <noinclude> |
− | |||
==Article purpose== |
==Article purpose== |
||
This article gathers the information that applies to any STM32MP15 board. |
This article gathers the information that applies to any STM32MP15 board. |
||
Line 82: | Line 81: | ||
{{Info|Obviously, what you obtain might differ from what is displayed on the ''Output example'' column.}} {{UpdateNeededForNewRelease|The "Output example" column below shall be updated periodically, even if the information banner specifies that this column might not be up-to-date}} |
{{Info|Obviously, what you obtain might differ from what is displayed on the ''Output example'' column.}} {{UpdateNeededForNewRelease|The "Output example" column below shall be updated periodically, even if the information banner specifies that this column might not be up-to-date}} |
||
− | ======For {{EcosystemRelease | revision= |
+ | ======For {{EcosystemRelease | revision=3.1.0 }}====== |
− | {| class=" |
+ | {| class="st-table" |
− | ! Software !! How to get its version !! Output example |
+ | ! style="text-align:center;" |Software !! style="text-align:center;" |How to get its version !! style="text-align:center;" |Output example |
|- |
|- |
||
− | | TF-A || [[TF-A |
+ | | TF-A || [[How to debug TF-A BL2#TF-A Version number|TF-A Version number]] || |
− | NOTICE: BL2: v2. |
+ | NOTICE: BL2: v2.4-r2.0(debug):{{Highlight|v2.4-dirty}} |
|- |
|- |
||
| U-Boot || See the version displayed in the console || |
| U-Boot || See the version displayed in the console || |
||
− | {{Highlight| |
+ | {{Highlight|2020.10-stm32mp-r2}} [...] |
|- |
|- |
||
| Linux kernel || |
| Linux kernel || |
||
{{Board$}} cat /proc/version |
{{Board$}} cat /proc/version |
||
|| |
|| |
||
− | {{Highlight|Linux version |
+ | {{Highlight|Linux version 5.10.61}} (xxxx@yyyy) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) [...] |
|- |
|- |
||
| GCC || |
| GCC || |
||
{{Board$}} cat /proc/version |
{{Board$}} cat /proc/version |
||
|| |
|| |
||
− | Linux version |
+ | Linux version 5.10.61 (xxxx@yyyy) ({{Highlight|arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0}}) [...] |
|- |
|- |
||
| Yocto Project || |
| Yocto Project || |
||
− | {{Board$}} |
+ | {{Board$}} grep DISTRO_CODENAME /etc/build
|
|| |
|| |
||
− | + |
DISTRO_CODENAME = {{Highlight|dunfell}} |
|
|- |
|- |
||
| Weston || |
| Weston || |
||
{{Board$}} weston --version |
{{Board$}} weston --version |
||
|| |
|| |
||
− | {{Highlight|weston |
+ | {{Highlight|weston 8.0.0}} |
|- |
|- |
||
| GStreamer || |
| GStreamer || |
||
{{Board$}} gst-play-1.0 --version |
{{Board$}} gst-play-1.0 --version |
||
|| |
|| |
||
− | {{Highlight|GStreamer 1. |
+ | {{Highlight|GStreamer 1.16.3}} |
|- |
|- |
||
| GPU || |
| GPU || |
||
{{Board$}} cat /sys/kernel/debug/gc/version |
{{Board$}} cat /sys/kernel/debug/gc/version |
||
|| |
|| |
||
− | {{Highlight|6 |
+ | {{Highlight|6.4.3.279124}} built [...] |
|} |
|} |
||
− | |||
− | |||
− | |||
− | |||
− | {| class=" |
+ | ======For {{EcosystemRelease | revision=3.0.0 }}====== |
− | ! Software !! How to get its version !! Output example |
+ | {| class="st-table" |
+ | ! style="text-align:center;" |Software !! style="text-align:center;" |How to get its version !! style="text-align:center;" |Output example |
||
|- |
|- |
||
− | | TF-A || [[TF-A |
+ | | TF-A || [[How to debug TF-A BL2#TF-A Version number|TF-A Version number]] || |
− | NOTICE: BL2: v2.0(debug):{{Highlight|v2. |
+ | NOTICE: BL2: v2.4-r1.0(debug):{{Highlight|v2.4-dirty}} |
|- |
|- |
||
| U-Boot || See the version displayed in the console || |
| U-Boot || See the version displayed in the console || |
||
− | {{Highlight| |
+ | {{Highlight|2020.10-stm32mp-r1}} [...] |
|- |
|- |
||
| Linux kernel || |
| Linux kernel || |
||
{{Board$}} cat /proc/version |
{{Board$}} cat /proc/version |
||
|| |
|| |
||
− | {{Highlight|Linux version |
+ | {{Highlight|Linux version 5.10.10}} (xxxx@yyyy) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) [...] |
|- |
|- |
||
| GCC || |
| GCC || |
||
{{Board$}} cat /proc/version |
{{Board$}} cat /proc/version |
||
|| |
|| |
||
− | Linux version |
+ | Linux version 5.10.10 (xxxx@yyyy) ({{Highlight|arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0}}) [...] |
|- |
|- |
||
| Yocto Project || |
| Yocto Project || |
||
− | {{Board$}} |
+ | {{Board$}} grep DISTRO_CODENAME /etc/build
|
|| |
|| |
||
− | + |
DISTRO_CODENAME = {{Highlight|dunfell}} |
|
|- |
|- |
||
| Weston || |
| Weston || |
||
{{Board$}} weston --version |
{{Board$}} weston --version |
||
|| |
|| |
||
− | {{Highlight|weston |
+ | {{Highlight|weston 8.0.0}} |
|- |
|- |
||
| GStreamer || |
| GStreamer || |
||
{{Board$}} gst-play-1.0 --version |
{{Board$}} gst-play-1.0 --version |
||
|| |
|| |
||
− | {{Highlight|GStreamer 1. |
+ | {{Highlight|GStreamer 1.16.3}} |
|- |
|- |
||
| GPU || |
| GPU || |
||
{{Board$}} cat /sys/kernel/debug/gc/version |
{{Board$}} cat /sys/kernel/debug/gc/version |
||
|| |
|| |
||
− | {{Highlight|6 |
+ | {{Highlight|6.4.3.279124}} built [...] |
|} |
|} |
||
− | |||
− | |||
===Configuration tips=== |
===Configuration tips=== |
||
Line 205: | Line 199: | ||
====Printing distribution specific information==== |
====Printing distribution specific information==== |
||
− | {{Board$}} |
+ | {{Board$}} cat /etc/os-release
|
− | + | ID=openstlinux-weston
|
|
− | + |
NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro)"
|
|
− | + |
VERSION="3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)"
|
|
− | + | VERSION_ID=3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17
|
|
− | + | PRETTY_NAME="ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 (dunfell)"
|
|
Where: |
Where: |
||
{| |
{| |
||
− | | |
+ | | ID || A lower-case string identifying the operating system
|
|- |
|- |
||
− | | |
+ | | NAME || A string identifying the operating system
|
|- |
|- |
||
− | | |
+ | | VERSION || A string identifying the operating system version, including a release code name
|
|- |
|- |
||
− | | |
+ | | VERSION_ID || A lower case string identifying the operating system version
|
|- |
|- |
||
− | | |
+ | | PRETTY_NAME || A full pretty name of the release |
|} |
|} |
||
====Printing system information==== |
====Printing system information==== |
||
{{Board$}} uname -a |
{{Board$}} uname -a |
||
− | Linux stm32mp1 |
+ | Linux stm32mp1 5.10.61 #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 armv7l armv7l armv7l GNU/Linux |
Where: |
Where: |
||
Line 235: | Line 229: | ||
| stm32mp1 || Network node hostname |
| stm32mp1 || Network node hostname |
||
|- |
|- |
||
− | | |
+ | | 5.10.61 || Kernel release |
|- |
|- |
||
− | | #1 SMP PREEMPT |
+ | | #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 || Kernel version |
|- |
|- |
||
| armv7l || Machine hardware name |
| armv7l || Machine hardware name |
||
Line 246: | Line 240: | ||
====Printing Linux kernel and GCC versions==== |
====Printing Linux kernel and GCC versions==== |
||
{{Board$}} cat /proc/version |
{{Board$}} cat /proc/version |
||
− | Linux version |
+ | Linux version 5.10.61 (oe-user@oe-host) (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0, GNU ld (GNU Binutils) 2.34.0.20200220) #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021
|
Where: |
Where: |
||
Line 252: | Line 246: | ||
| Linux || Kernel name |
| Linux || Kernel name |
||
|- |
|- |
||
− | | version |
+ | | version 5.10.61 ||Kernel release |
|- |
|- |
||
| (xxxx@yyyy) || Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened |
| (xxxx@yyyy) || Person (xxxx) who compiled the kernel, and machine (yyyy) where it happened |
||
|- |
|- |
||
− | | (gcc |
+ | | (arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 ) || Version of the GCC compiler used to compile the kernel |
|- |
|- |
||
− | | #1 SMP PREEMPT |
+ | | #1 SMP PREEMPT Thu Aug 26 12:51:21 UTC 2021 || Kernel version; type of kernel (SMP) and date and time of the kernel compilation |
|} |
|} |
||
Line 294: | Line 288: | ||
Note: the user file system (userfs) and the boot file system (bootfs) are accessible respectively through the ''/usr/local'' mounting point, and the ''/boot'' mounting point (see [[STM32MP15 Flash mapping#Flash partitions|Flash partitions]] for a description of the file systems). |
Note: the user file system (userfs) and the boot file system (bootfs) are accessible respectively through the ''/usr/local'' mounting point, and the ''/boot'' mounting point (see [[STM32MP15 Flash mapping#Flash partitions|Flash partitions]] for a description of the file systems). |
||
+ | <noinclude> |
||
+ | {{NoIndex}} |
||
[[Category:Sub-articles]] |
[[Category:Sub-articles]] |
||
+ | </noinclude> |