This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Change propagation updates are pending (1 job estimated) and it is recommended to wait with modifications to a property until the process has been finalized to prevent intermediary interruptions or contradictory specifications.
"Media type" is a predefined property that describes the media type of an uploaded file and is provided by Semantic MediaWiki. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.