1. Usage
The EcosystemRelease/Revision template returns the status for an ecosystem release revision in the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), or the revision (x.y.z) of the latest ecosystem release.
Usage: {{EcosystemRelease/Revision | revision=<revision>}} Where:
- <revision> is the mandatory revision of the ecosystem release for which a status is requested. The possible values are:
- latest to get the revision (x.y.z) of the latest major ecosystem release.
- 5.0.0 (June 2023 major ecosystem release revision).
- 4.1.0 (November 2022 major ecosystem release revision): possible but not recommended.
- 4.0.2 (July 2022 minor ecosystem release revision): possible but not recommended.
- 4.0.0 (June 2022 major ecosystem release revision): possible but not recommended.
- 3.1.0 (November 2021 major ecosystem release revision): possible but not recommended.
- 3.0.0 (March 2021 major ecosystem release revision): possible but not recommended.
- 2.1.0 (November 2020 major ecosystem release revision) : possible but not recommended.
- 2.0.0 (June 2020 major ecosystem release revision) : possible but not recommended.
- x.0.0, x.1.0, x.2.0 and 0.y.0 values are reserved to the examples and the helper files.
The returned value is:
- x.y.z (revision of the latest ecosystem release), if <revision> is set to latest.
- latest, if <revision> is the latest one, in the flow associated with this wiki.
- legacy, if <revision> is a legacy one, in the flow associated with this wiki.
- next, if <revision> is a planned one, in the flow associated with this wiki.
- former, if <revision> is part of a former flow that is not the one associated with this wiki.
- unknown, if <revision> is not supported.
E.g.,
- At 3.1.0 deployment : next: none, legacy: 3.0.0, latest: 3.1.0, former: 1.x.y, 2.x.y
- During 3.1.0 preparation: next: 3.1.0, legacy: none, latest: 3.0.0, former: 1.x.y, 2.x.y.
- 3.0.0 deployed (initial situation): next: none, legacy: none, latest: 3.0.0, former: 1.x.y, 2.x.y.
2. Basic examples
You type | You get |
---|---|
v5.0.0 revision (latest)
{{EcosystemRelease/Revision | revision=5.0.0}} |
latest |
Latest revision
{{EcosystemRelease/Revision | revision=latest}} |
5.0.0 |
Former revisions
{{EcosystemRelease/Revision | revision=4.1.0}}<br /> {{EcosystemRelease/Revision | revision=4.0.2}}<br /> {{EcosystemRelease/Revision | revision=4.0.0}}<br /> {{EcosystemRelease/Revision | revision=3.1.0}}<br /> {{EcosystemRelease/Revision | revision=3.0.0}}<br /> {{EcosystemRelease/Revision | revision=2.1.0}}<br /> {{EcosystemRelease/Revision | revision=2.0.0}}<br /> {{EcosystemRelease/Revision | revision=1.2.0}}<br /> {{EcosystemRelease/Revision | revision=1.1.0}}<br /> {{EcosystemRelease/Revision | revision=1.0.0}} |
former |
3. More examples
You type | You get |
---|---|
vx.0.0 revision (legacy)
{{EcosystemRelease/Revision | revision=x.0.0}} |
legacy |
vx.1.0 revision (latest)
{{EcosystemRelease/Revision | revision=x.1.0}} |
latest |
vx.2.0 revision (next)
{{EcosystemRelease/Revision | revision=x.2.0}} |
next |
v0.y.0 revision (former)
{{EcosystemRelease/Revision | revision=0.y.0}} |
former |
Unknown revision
{{EcosystemRelease/Revision | revision=10.20.30}} |
unknown |
Unspecified revision
{{EcosystemRelease/Revision}} |
unknown |
4. Code
unknown