Wiki archives

Revision as of 17:50, 14 November 2022 by Registered User
Applicable for STM32MP15x lines

This page aims to provide links to archived wikis.
Each STM32 MPU ecosystem release flow has its corresponding wiki.

An ecosystem release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.

The most recent flow is associated with the latest wiki also known as flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").

The flagship wiki is for the v4 flow (v4.y.z ecosystem releases): if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to continue browsing the wiki that contains the latest major ecosystem release for STM32MP15.


However, if you need information about any previous ecosystem releases flow, browse the associated wiki thanks to the below table:

STM32 MPU v3 wiki by ST.png
STM32 MP15 archived wiki for the v3.y.z ecosystem releases
STM32 MPU v2 wiki by ST.png
STM32 MP15 archived wiki for the v2.y.z ecosystem releases
STM32 MPU v1 wiki by ST.png
STM32 MP15 archived wiki for the v1.y.z ecosystem releases
Wikis and software components
Wiki Major ecosystem releases Major software components (OpenSTLinux distribution)
This wiki dedicated to STM32MP1 v4 flow

v4.1.0
v4.0.0

Linux® kernel v5.15 (LTS)
U-Boot v2021.10
TF-A v2.6
OP-TEE v3.16.0
OpenEmbedded v4.0 (Kirkstone)

Archived wiki for the v3 flow

v3.1.0
v3.0.0

Linux® kernel v5.10 (LTS)
U-Boot v2020.10
TF-A v2.4
OP-TEE v3.12.0
OpenEmbedded v3.1 (Dunfell)

Archived wiki for the v2 flow

v2.1.0
v2.0.0

Linux® kernel v5.4 (LTS)
U-Boot v2020.01
TF-A v2.2
OP-TEE v3.9.0
OpenEmbedded v3.1 (Dunfell)

Archived wiki for the v1 flow

v1.2.0
v1.1.0
v1.0.0

Linux® kernel v4.19 (LTS)
U-Boot v2018.11
TF-A v2.0
OP-TEE v3.3.0
OpenEmbedded v2.6 (Thud)