1. Usage[edit source]
The EcosystemRelease template is used to indicate for which ecosystem release revision(s) of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{EcosystemRelease | revision=<revision> | range =<range> | revision2=<revision2>}}
Where:
- <revision> is the mandatory ecosystem release revision for which the article part is valid.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- The optional <range> and <revision2> parameters allow to define a range of revisions.
- <range> is the optional range of the ecosystem release revisions for which the article part is valid. The possible values are:
- and before: the article part is valid only for the revision(s) less than or equal to <revision>
- and after: the article part is valid only for the revision(s) greater than or equal to <revision>
- to: the article part is only valid from <revision> to <revision2>
- <revision2> is the mandatory ecosystem release upper revision for which the article part is valid, when <range> is set to "to"; in this case, <revision> becomes the lower revision for which the article part is valid.
- This parameter is ignored if <range> is either not set, or set to another value than "to".
If the mouse is left over a revision (or the icon), a popup window shows, for that revision:
- the versions of the Linux kernel, U-Boot, TF-A and OP-TEE
- the version of the STM32Cube MPU Package
- the version of OpenEmbedded
- the version of Android
This information comes from the EcosystemRelease/Components template.
2. Basic examples[edit source]
You type | You get |
---|---|
Another specific revision (revision 3.1.0.ALPHA): the next one
{{EcosystemRelease | revision=3.1.0.ALPHA}} |
ecosystem release unknown revision 3.1.0.ALPHA |
Another specific revision (revision 3.1.0): the next one
{{EcosystemRelease | revision=3.1.0}} |
ecosystem release v3.1.0 |
A specific revision (revision 3.0.0): a latest one
{{EcosystemRelease | revision=3.0.0}} |
ecosystem release v3.0.0 |
A specific revision (revision 2.1.0): a former one
{{EcosystemRelease | revision=2.1.0}} |
ecosystem release v2.1.0 |
Another specific revision (revision 2.0.0): a former one
{{EcosystemRelease | revision=2.0.0}} |
ecosystem release v2.0.0 |
Revisions that are lower than or equal to a revision
{{EcosystemRelease | revision=x.1.0 | range=and before}} |
ecosystem release ≤ vx.1.0 |
Revisions that are greater than or equal to a revision
{{EcosystemRelease | revision=x.1.0 | range=and after}} |
ecosystem release ≥ vx.1.0 |
Range of revisions
{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}} |
ecosystem release vx.0.0 to vx.1.0 |
3. More examples[edit source]
You type | You get |
---|---|
Revision x.1.0
{{EcosystemRelease | revision=x.1.0}} |
ecosystem release vx.1.0 |
Revision x.0.0
{{EcosystemRelease | revision=x.0.0}} |
ecosystem release vx.0.0 |
Former revision that is part of a flow that is not the one associated with this wiki.
{{EcosystemRelease | revision=0.y.0}}<br> {{EcosystemRelease | revision=0.y.0 | range=and before}}<br> {{EcosystemRelease | revision=0.y.0 | range=and after}} |
ecosystem release v0.y.0 |
Unspecified revision
{{EcosystemRelease}} |
ecosystem release unknown revision |
Unknown revision
{{EcosystemRelease | revision=10.20.30}} |
ecosystem release unknown revision 10.20.30 |
Unspecified revision2
{{EcosystemRelease | revision=x.1.0 | range=to}} |
ecosystem release vx.1.0 to unknown revision |
Unknown revision2
{{EcosystemRelease | revision=x.1.0 | range=to | revision2=10.20.30}} |
ecosystem release vx.1.0 to unknown revision 10.20.30 |
Former revision2 that is part of a flow that is not the one associated with this wiki.
{{EcosystemRelease | revision=x.0.0 | range=to | revision2=0.y.0}}<br> {{EcosystemRelease | revision=0.y.0 | range=to | revision2=0.y.0}} |
ecosystem release vx.0.0 to v0.y.0 |
Ignored revision2
{{EcosystemRelease | revision=x.0.0 | range=and after | revision2=x.1.0}} |
ecosystem release ≥ vx.0.0 |
Unknown range
{{EcosystemRelease | revision=x.1.0 | range=error}} |
ecosystem release vx.1.0 unknown range error |
Check that there's no space before and after the text
BEFORE{{EcosystemRelease | revision=x.0.0}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and before}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.1.0 | range=and after}}AFTER<br> BEFORE{{EcosystemRelease | revision=x.0.0 | range=to | revision2=x.1.0}}AFTER |
BEFOREecosystem release vx.0.0 AFTER |
4. Code[edit source]
ecosystem release unknown revision