1. Usage[edit source]
The EcosystemFlow/Warning template is used to insert a message about the current status of the article or chapter containing it.
Usage: {{EcosystemFlow/Warning| flow=<flow> }}
Where:
- <flow> is the identifier of the wiki. 2 values are possible:
- Current: the meaning of message associated to the Current flow (here v3 & v3.ALPHA) highlights the fact that the article or chapter has not been updated for the Current version (here v3 & v3.ALPHA). To be used when the article should have been updated for the Current version (here v3 & v3.ALPHA) but the update has not been done yet.
- Next : the meaning of message associated to the Next flow (here v4) highlights that the article has been updated for Next version (here v4) in Current version (here v3) . Consequently, this updated version must not be published yet.
Generally speaking, Current corresponds to current flow, and Next corresponds to the up coming flow.
The returned value is:
- a generic or custom message depending on the parameters
- "unknown flow", if <flow> is not supported.
2. Basic examples[edit source]
You type | You get |
---|---|
Generic message
{{EcosystemFlow/Warning}} |
unknown flow |
Message when flow is Current
{{EcosystemFlow/Warning | flow=Current}} |
|
Message when flow is Next
{{EcosystemFlow/Warning | flow=Next}} |
3. More examples[edit source]
You type | You get |
---|---|
Unknown flow
{{EcosystemFlow/Warning | flow=v0}} |
unknown flow |
Unspecified flow
{{EcosystemFlow/Warning}} |
unknown flow |
Check that there's no space before and after the text
BEFORE{{EcosystemFlow/Warning}}AFTER<br> BEFORE{{EcosystemFlow/Warning | flow=Current}}AFTER<br> BEFORE{{EcosystemFlow/Warning |flow=Next}}AFTER |
BEFOREunknown flow BEFOREAFTER |
4. Code[edit source]
unknown flow