1. Usage[edit source]
The STM32CubeRelease/Revision template returns the status for an STM32Cube release revision , or the revision (x.y.z) of the latest STM32Cube release.
Usage: {{STM32CubeRelease/Revision | revision=<revision>}}
Where:
- <revision> is the mandatory revision of the STM32Cube release for which a status is requested. The possible values are:
- latest to get the revision (x.y.z) of the latest major STM32Cube release.
- 1.17.0 (jun 2024 major STM32Cube release revision).
- 1.16.0 (Mar 2024 major STM32Cube release revision).
- 1.15.0 (Nov 2023 major STM32Cube release revision).
The returned value (aka status) is:
- x.y.z (revision of the latest STM32Cube release), if <revision> is set to latest.
- latest, if <revision> is the latest one, in the flow associated with this wiki.
- legacy, if <revision> is a legacy one, in the flow associated with this wiki.
- next, if <revision> is a planned one, in the flow associated with this wiki.
- former, if <revision> is part of a former flow that is not the one associated with this wiki.
- unknown, if <revision> is not supported.
2. Basic examples[edit source]
You type | You get |
---|---|
v1.17.0 revision (latest)
{{STM32CubeRelease/Revision | revision=1.17.0}} |
latest |
v1.16.0 revision
{{STM32CubeRelease/Revision | revision=1.16.0}} |
legacy |
v1.15.0 revision
{{STM32CubeRelease/Revision | revision=1.15.0}} |
legacy |
Latest revision
{{STM32CubeRelease/Revision | revision=latest}} |
1.16.0 |
Former revisions
{{STM32CubeRelease/Revision | revision=0.1.0}}<br /> |
unknown |
3. More examples[edit source]
You type | You get |
---|---|
vx.0.0 revision (legacy)
{{STM32CubeRelease/Revision | revision=x.0.0}} |
legacy |
vx.1.0 revision (latest)
{{STM32CubeRelease/Revision | revision=x.1.0}} |
latest |
vx.2.0 revision (next)
{{STM32CubeRelease/Revision | revision=x.2.0}} |
next |
v0.y.0 revision (former)
{{STM32CubeRelease/Revision | revision=0.y.0}} |
former |
Unknown revision
{{STM32CubeRelease/Revision | revision=10.20.30}} |
unknown |
Unspecified revision
{{STM32CubeRelease/Revision}} |
unknown |
4. Code[edit source]
unknown