Revision as of 12:08, 24 June 2024 by Registered User (→‎Code)

1. Usage[edit source]

The EcosystemRelease/Package template returns different information (name, URL or installation path) about a software package or script delivered by an ecosystem release revision of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...).

Usage: {{EcosystemRelease/Package | revision=<revision> | package=<package> | device=<device> | request=<request>}}

Where:

  • <revision> is the mandatory parameter that specifies the revision of the ecosystem release, for which a piece of information is requested.
    • The possible values for this parameter are available in the EcosystemRelease/Revision template.
    • latest is also a possible value: the latest revision of the ecosystem release is then considered.
  • <package> is the mandatory parameter that specifies the software package or script delivered by the ecosystem release revision, for which a piece of information is requested. The possible values are listed in the below table.
  • <device> is the optional parameter that specifies the microprocessor devices for which the piece of information is requested. The possible values are listed in the below table.
  • <request> is the mandatory parameter that specifies the requested piece of information about the software package or script. The possible values are listed in the below table.

The returned value is:

  • a string that contains either the requested piece of information about the software package or script (see the below table for details).
  • an empty string, if the request is not applicable (e.g. requesting the URL of the SDK environment script makes no sense).
  • "unknown revision", if <revision> is not supported.
  • "unknown package or script", if <package> is not supported.
  • "unknown request", if <request> is not supported.
<package> <device> <request> Description of the returned value
Images package
  • MP1 [1]
  • MP2_A35_TD
name Name of the tarball file that contains the binaries (Starter Package)
url Nothing is returned (not applicable)
path Path to the directory that contains the binaries (once the binaries tarball file is uncompressed)
SDK-x86 package [2] name Name of the tarball file that contains the SDK installation script for x86 architecture host (Developer Package)
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
SDK-x86 installation script [2] name Name of the SDK installation script for x86 architecture host (Developer Package)
url Nothing is returned (not applicable)
path Path to the directory that contains the SDK installation script (once the SDK package tarball file is uncompressed)
SDK-x86 setup script [2] name Name of the SDK setup script for x86 architecture host (Developer Package)
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
SDK-arm64 package name Name of the tarball file that contains the SDK installation script for arm64 architecture host (Developer Package)
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
SDK-arm64 installation script name Name of the SDK installation script (Developer Package) for arm64 architecture host
url Nothing is returned (not applicable)
path Path to the directory that contains the SDK installation script (once the SDK package tarball file is uncompressed)
SDK-arm64 setup script name Name of the SDK setup script for arm64 architecture host (Developer Package)
url Nothing is returned (not applicable)
path Nothing is returned (not applicable)
OpenSTLinux BSP package name Name of the tarball file that contains the OpenSTLinux BSP package (Developer Package)
url Nothing is returned (not applicable)
path Path to the OpenSTLinux BSP installation directory (once the OpenSTLinux BSP package tarball file is uncompressed)
Linux kernel package name Name of the installation directory that contains the Linux kernel package (Developer Package)
url Nothing is returned (not applicable)
path Path to the Linux kernel installation directory
Linux kernel source name Name of the tarball file that contains the Linux kernel source code
url Nothing is returned (not applicable)
path Path to the directory that contains the Linux kernel source code (from the Linux kernel installation directory and once the Linux kernel source tarball file is uncompressed)
U-Boot package name Name of the installation directory that contains the U-Boot package (Developer Package)
url Nothing is returned (not applicable)
path Path to the U-Boot installation directory
U-Boot source name Name of the tarball file that contains the U-Boot source code
url Nothing is returned (not applicable)
path Path to the directory that contains the U-Boot source code (from the U-Boot installation directory and once the U-Boot source tarball file is uncompressed)
TF-A package name Name of the installation directory file that contains the TF-A package (Developer Package)
url Nothing is returned (not applicable)
path Path to the TF-A installation directory
TF-A source name Name of the tarball file that contains the TF-A source code
url Nothing is returned (not applicable)
path Path to the directory that contains the TF-A source code (from the TF-A installation directory and once the TF-A package tarball file is uncompressed)
OP-TEE package name Name of the installation directory that contains the OP-TEE package (Developer Package)
url Nothing is returned (not applicable)
path Path to the OP-TEE installation directory (once the OP-TEE package tarball file is uncompressed)
OP-TEE source name Name of the tarball file that contains the OP-TEE source code
url Nothing is returned (not applicable)
path Path to the directory that contains the OP-TEE source code (from the OP-TEE installation directory)
SCP firmware Parameter ignored (MP2 only, not applicable) inst name Name of the installation directory that contains the System Control Processor (SCP) package (Developer Package)
name Name of the tarball file that contains the SCP source code
path Path to the directory that contains the SCP source code (from the SCP installation directory)
External DT Parameter ignored (MP2 only , not applicable) inst name Name of the installation directory that contains the external device tree (DT) package (Developer Package)
name Name of the tarball file that contains the external DT source code
path Path to the directory that contains the external DT source code (from the external DT installation directory)
gcnano-driver package name Name of the installation directory that contains the gcnano-driver package (Developer Package)
url Nothing is returned (not applicable)
path Path to the gcnano-driver installation directory
gcnano-driver source name Name of the tarball file that contains the gcnano-driver source code
url Nothing is returned (not applicable)
path Path to the directory that contains the gcnano-driver source code (from the gcnano-driver installation directory and once the gcnano-driver source tarball file is uncompressed)
STM32CubeMPU [3] name Name of the archive file that contains the STM32CubeMP1 package (Developer Package)
url Nothing is returned (not applicable)
path Path to the directory that contains the STM32CubeMP1 source code (once the STM32CubeMP1 package archive file is uncompressed)
TF-M Parameter ignored (MP2 only, not applicable) name Name of the archive file that contains the TF-M package (Developer Package)
path Path to the directory that contains the TF-M source code (once the TF-M package archive file is uncompressed)
Debug symbol files name Nothing is returned (not applicable)
url Nothing is returned (not applicable)
path Path to the directory that contains the debug symbol files (once the debug symbol files package archive file is uncompressed)
Licenses package Parameter ignored (not applicable) name Name of the tarball file that contains the licenses package (for the OpenSTLinux distribution)
url URL (st.com) to the tarball file that contains the licenses package
path Nothing is returned (not applicable)
OpenSTLinux distribution Parameter ignored (not applicable) name Name of the manifest (Distribution Package)
url URL (st.com) to the manifest
path Nothing is returned (not applicable)
Buildroot distribution Parameter ignored (not applicable) name Name of the tag
url URL to the Buildroot repository dedicated to supporting the STMicroelectronics STM32MPU platforms
path Nothing is returned (not applicable)
stm32mp-ddr-phy package name Name of the installation directory that contains the stm32mp-ddr-phy package
url Nothing is returned (not applicable)
path Path to the stm32mp-ddr-phy package installation directory
stm32mp-ddr-phy source name Name of the installation directory that contains the stm32mp-ddr-phy source
url Nothing is returned (not applicable)
path Path to the stm32mp-ddr-phy source installation directory
  1. 1.00 1.01 1.02 1.03 1.04 1.05 1.06 1.07 1.08 1.09 1.10 1.11 1.12 1.13 1.14 1.15 1.16 1.17 1.18 1.19 1.20 1.21 If <device> is not set, the MP1 value is per default considered.
  2. 2.0 2.1 2.2 The former values (SDK package, SDK installation script and SDK setup script) are kept compatible with the new values, until they are no more used.
  3. The former value (STM32CubeMP1) is kept compatible with the new value, until it is no more used.
Warning white.png Warning
Please read carefully the below information about the use of this template in preformatted text blocks.
  • It is not possible to use this template (as any template) in preformatted text blocks made with with <pre>...</pre>: use preformatted text blocks made with space at the beginning of the line.
  • If needed (especially in tables), limit the width of the blocks with <div style="max-width:60em;"> (adjust the value)
Do not use <pre>...</pre>
You type
<pre>
tar xvf {{EcosystemRelease/Package | revision=latest | package=Images package | device=MP2_A35_TD | request=name}}
</pre>
You get
tar xvf {{EcosystemRelease/Package | revision=latest | package=Images package | device=MP2_A35_TD | request=name}}
Use space at the beginning of the line
You type
tar xvf {{EcosystemRelease/Package | revision=latest | package=Images package | device=MP2_A35_TD | request=name}}
You get

tar xvf en.flash-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz

Limit the width of the block
You type
<div style="max-width:60em;">
This is a very long command that uses the template (tar xvf {{EcosystemRelease/Package | revision=latest | package=Images package | device=MP2_A35_TD | request=name}}) and its width might be a problem
</div>
You get

This is a very long command that uses the template (tar xvf en.flash-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz) and its width might be a problem

2. Basic examples[edit source]


2.1. Basic examples for v5.1.0 release[edit source]

You type You get
Information about "Images package" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=Images package | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=Images package | device =MP1 | request=name}}<br>
Name (MP2_A35_TD): {{EcosystemRelease/Package | revision=5.1.0 | package=Images package | device=MP2_A35_TD | request=name}}<br>
Path (MP2_A35_TD): {{EcosystemRelease/Package | revision=5.1.0 | package=Images package | device=MP2_A35_TD | request=path}}<br>
URL (MP2_A35_TD): [{{EcosystemRelease/Package | revision=5.1.0 | package=Images package | device=MP2_A35_TD | request=url}}]<br>

Name (default): en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP1): en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP2_A35_TD): en.flash-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path (MP2_A35_TD): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/images/stm32mp2
URL (MP2_A35_TD): [NA]

Information about "SDK-x86 package" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 package | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 package | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 package | device=MP2 | request=url}}]<br>

Name (default): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP1): en.sdk-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP2): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path: NA
URL: [NA]

Information about "SDK-x86 installation script" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 installation script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 installation script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 installation script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 installation script | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 installation script | device=MP2 | request=url}}]<br>

Name (default): st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Name (MP1): st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Name (MP2): st-image-weston-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sdk
URL: [NA]

Information about "SDK-x86 setup script" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 setup script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 setup script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 setup script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 setup script | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=SDK-x86 setup script | device=MP2 | request=url}}]<br>

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi(tbd)
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi(tbd)
Name (MP2): environment-setup-cortexa35-ostl-linux(tbd)
Path: NA
URL: [NA]

"SDK package", "SDK installation script" and "SDK setup script" temporarily kept for compatibility
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK package | device=MP2 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK installation script | device=MP2 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK setup script | device=MP2 | request=name}}<br>

Name (MP2): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP2): st-image-weston-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Name (MP2): environment-setup-cortexa35-ostl-linux(tbd)

Information about "SDK-arm64 package" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 package | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 package | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 package | device=MP2 | request=url}}]<br>

Name (default): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP1): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP2): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path: NA
URL: [NA]

Information about "SDK-arm64 installation script" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 installation script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 installation script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 installation script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 installation script | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 installation script | device=MP2 | request=url}}]<br>

Name (default): st-image-weston-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Name (MP1): st-image-weston-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Name (MP2): st-image-weston-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sdk
URL: [NA]

Information about "SDK-arm64 setup script" for v5.1.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 setup script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 setup script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 setup script | device=MP2 | request=name}}<br>
Path (MP2): {{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 setup script | device=MP2 | request=path}}<br>
URL (MP2) : [{{EcosystemRelease/Package | revision=5.1.0 | package=SDK-arm64 setup script | device=MP2 | request=url}}]<br>

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi (tbd)
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi (tbd)
Name (MP2): environment-setup-cortexa35-ostl-linux (tbd)
Path (MP2): NA
URL (MP2) : [NA]

Information about "OpenSTLinux BSP package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package |device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package |device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package |device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package |device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux BSP package |device=MP2 | request=url}}]<br>

Default:
Name: sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux
URL: [NA]

MP1:
Name: sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux
URL: [NA]

MP2:
Name: sources-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux
URL: [NA]

Information about "Linux kernel package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel package | device=MP2 | request=url}}]<br><br>

Default:
Name: linux-stm32mp-6.1.82-stm32mp-r2-r0
Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0
URL: [NA]

MP1:
Name: linux-stm32mp-6.1.82-stm32mp-r2-r0
Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0
URL: [NA]

MP2:
Name: linux-stm32mp-6.1.82-stm32mp-r2-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/linux-stm32mp-6.1.82-stm32mp-r2-r0
URL: [NA]

Information about "Linux kernel source" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Linux kernel source | device=MP2 | request=url}}]<br>

Default:
Name: linux-6.1.82.tar.xz
Path: linux-6.1.82
URL: [NA]

MP1:
Name: linux-6.1.82.tar.xz
Path: linux-6.1.82
URL: [NA]

MP2:
Name: linux-6.1.82.tar.xz
Path: linux-6.1.82
URL: [NA]

Information about "U-Boot package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot package | device=MP2 | request=url}}]<br>

Default:
Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2022.10-stm32mp-r2-r0
URL: [NA]

MP1:
Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2022.10-stm32mp-r2-r0
URL: [NA]

MP2:
Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/u-boot-stm32mp-v2022.10-stm32mp-r2-r0
URL: [NA]

Information about "U-Boot source" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=U-Boot source | device=MP2 | request=url}}]<br>

Default:
Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0.tar.xz
Path: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
URL: [NA]

MP1:
Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0.tar.xz
Path: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
URL: [NA]

MP2:
Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0.tar.xz
Path: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
URL: [NA]

Information about "TF-A package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A package | device=MP2 | request=url}}]<br>

Default:
Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
URL: [NA]

MP1:
Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
URL: [NA]

MP2:
Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
URL: [NA]

Information about "TF-A source" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=TF-A source | device=MP2 | request=url}}]<br>

Default:
Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0.tar.xz
Path: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
URL: [NA]

MP1:
Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0.tar.xz
Path: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
URL: [NA]

MP2:
Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0.tar.xz
Path: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
URL: [NA]

Information about "OP-TEE package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE package  | device=MP2 | request=url}}]<br>

Default:
Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0/
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/optee-os-stm32mp-3.19.0-stm32mp-r2-r0
URL: [NA]

MP1:
Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0/
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/optee-os-stm32mp-3.19.0-stm32mp-r2-r0
URL: [NA]

MP2:
Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/optee-os-stm32mp-3.19.0-stm32mp-r2-r0
URL: [NA]

Information about "OP-TEE source" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OP-TEE source | device=MP2 | request=url}}]<br>

Default:
Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0.tar.xz
Path: optee-os-stm32mp-3.19.0-stm32mp-r2-r0
URL: [NA]

MP1:
Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0.tar.xz
Path: optee-os-stm32mp-3.19.0-stm32mp-r2-r0
URL: [NA]

MP2:
Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0.tar.xz
Path: optee-os-stm32mp-3.19.0-stm32mp-r2-r0
URL: [NA]

Information about "SCP firmware" for v5.1.0 revision requested
Installation name: {{EcosystemRelease/Package | revision=5.1.0 | package=SCP firmware | request=inst name}}<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=SCP firmware | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=SCP firmware | request=path}}<br>

Installation name: scp-firmware-2.12-stm32mp-r1-r0(tbd)
Name: scp-firmware-2.12-stm32mp-r1-r0.tar.xz(tbd)
Path: scp-firmware-2.12-stm32mp-r1(tbd)

Information about "External DT" for v5.1.0 revision requested
Installation name: {{EcosystemRelease/Package | revision=5.1.0 | package=External DT | request=inst name}}<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=External DT | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=External DT | request=path}}<br>

Installation name: unknown package
Name: unknown package
Path: unknown package

Information about "gcnano-driver package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package| request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package| request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver package | device=MP2 | request=url}}]<br>

Default:
Name: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0/
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0
URL: [NA]

MP1:
Name: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0/
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0
URL: [NA]

MP2:
Name: gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0/
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0
URL: [NA]

Information about "gcnano-driver source" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=gcnano-driver source | device=MP2 | request=url}}]<br>

Default:
Name: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0.tar.xz
Path: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0
URL: [NA]

MP1:
Name: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0.tar.xz
Path: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0
URL: [NA]

MP2:
Name: gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0.tar.xz
Path: gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0
URL: [NA]

Information about "STM32CubeMPU" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMPU  | device=MP2 | request=url}}]<br>

Default:
Name: en.stm32cube_fw_mp1_v1.6.0.zip
Path: STM32Cube_FW_MP1_V1.6.0
URL: [NA]

MP1:
Name: en.stm32cube_fw_mp1_v1.6.0.zip
Path: STM32Cube_FW_MP1_V1.6.0
URL: [NA]

MP2:
Name: en.stm32cubemp2-v1.0.0TBD.zip
Path: STM32CubeMP2-mainTBD
URL: [NA]

"STM32CubeMP1" temporarily kept for compatibility, device parameter is ignored
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMP1 | request=name}}<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMP1 | device=MP1 | request=name}}<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=STM32CubeMP1 | device=MP2 | request=name}}<br>

Default:
Name: en.stm32cube_fw_mp1_v1.6.0.zip

MP1:
Name: en.stm32cube_fw_mp1_v1.6.0.zip

MP2:
Name: en.stm32cubemp2-v1.0.0TBD.zip

Information about "TF-M" for v5.1.0 revision requested only for MP2 =default
Default = MP2<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-M| request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-M| request=path}}<br><br>
MP1: (device parameter is ignored) <br> 
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-M| device=MP1 |request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-M| device=MP1 |request=path}}<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-M| device=MP2 |request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=TF-M| device=MP2 |request=path}}<br>

Default = MP2
Name: NA
Path: NA

MP1: (device parameter is ignored)
Name: NA
Path: NA

MP2:
Name: NA
Path: NA

Information about "Debug symbol files" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Debug symbol files | device=MP2 | request=url}}]<br>

Default:
Name: NA
Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/images/stm32mp25(tbd)
URL: [NA]

MP1:
Name: NA
Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/images/stm32mp25(tbd)
URL: [NA]

MP2:
Name: NA
Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/images/stm32mp25(tbd)
URL: [NA]

Information about "Licenses package" for v5.1.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.1.0| package=Licenses package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0| package=Licenses package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0| package=Licenses package | request=url}}]<br>

Name: LICENSES-world-openstlinux-weston-stm32mp1.tar.gz(tbd)
Path: NA
URL: [1]

Information about "OpenSTLinux distribution" for v5.1.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux distribution | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux distribution | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=OpenSTLinux distribution | request=url}}]<br>

Name: openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
Path: NA
URL: [2]

Information about "Buildroot distribution" for v5.1.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=Buildroot distribution | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=Buildroot distribution | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=Buildroot distribution | request=url}}]<br>

Name: unknown package
Path: unknown package
URL: [unknown package]

Information about "stm32mp-ddr-phy package" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy package | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phypackage | device=MP2 | request=url}}]<br>

Default:
Name: stm32mp-ddr-phy-A2022.11-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/stm32mp-ddr-phy-A2022.11-r0
URL: [NA]

MP1:
Name: stm32mp-ddr-phy-A2022.11-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/stm32mp-ddr-phy-A2022.11-r0
URL: [NA]

MP2:
Name: stm32mp-ddr-phy-A2022.11-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/stm32mp-ddr-phy-A2022.11-r0
URL: [NA]

Information about "stm32mp-ddr-phy source" for v5.1.0 revision requested
Default:<br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source| request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source| request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | request=url}}]<br><br>
MP1: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | device=MP1 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | device=MP1 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | device=MP1 | request=url}}]<br><br>
MP2: <br>
Name: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | device=MP2 | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.1.0 | package=stm32mp-ddr-phy source | device=MP2 | request=url}}]<br>

Default:
Name: stm32mp-ddr-phy-A2022.11-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/stm32mp-ddr-phy-A2022.11-r0
URL: [NA]

MP1:
Name: stm32mp-ddr-phy-A2022.11-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/stm32mp-ddr-phy-A2022.11-r0
URL: [NA]

MP2:
Name: stm32mp-ddr-phy-A2022.11-r0
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux/stm32mp-ddr-phy-A2022.11-r0
URL: [NA]

2.2. Basic examples for latest release[edit source]

You type You get
Information about "Images package" for latest revision
Name (MP2_A35_TD): {{EcosystemRelease/Package | revision=latest | package=Images package | device=MP2_A35_TD | request=name}}<br>
Path (MP2_A35_TD): {{EcosystemRelease/Package | revision=latest | package=Images package | device=MP2_A35_TD | request=path}}<br>

Name (MP2_A35_TD): en.flash-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path (MP2_A35_TD): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/images/stm32mp2

Information about "SDK-x86 package" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-x86 package | device=MP2 | request=name}}<br>

Name (MP2): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz

Information about "SDK-x86 installation script" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-x86 installation script | device=MP2 | request=name}}<br>
Path (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-x86 installation script | device=MP2 | request=path}}<br>

Name (MP2): st-image-weston-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Path (MP2): stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sdk

Information about "SDK-x86 setup script" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-x86 setup script | device=MP2 | request=name}}<br>

Name (MP2): environment-setup-cortexa35-ostl-linux(tbd)

"SDK package", "SDK installation script" and "SDK setup script" temporarily kept for compatibility
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK package | device=MP2 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK installation script | device=MP2 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK setup script | device=MP2 | request=name}}<br>

Name (MP2): en.sdk-x86_64-stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Name (MP2): st-image-weston-openstlinux-weston-stm32mp2-x86_64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Name (MP2): environment-setup-cortexa35-ostl-linux(tbd)

Information about "SDK-arm64 package" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-arm64 package | device=MP2 | request=name}}<br>

Name (MP2): en.sdk-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz

Information about "SDK-arm64 installation script" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-arm64 installation script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=SDK-arm64 installation script | device=MP2 | request=path}}<br>

Name (MP2): st-image-weston-openstlinux-weston-stm32mp2-aarch64-toolchain-4.2.4-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.sh
Path: stm32mp2-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sdk

Information about "SDK-arm64 setup script" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=SDK-arm64 setup script | device=MP2 | request=name}}<br>

Name (MP2): environment-setup-cortexa35-ostl-linux (tbd)

Information about "OpenSTLinux BSP package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=OpenSTLinux BSP package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=OpenSTLinux BSP package | request=path}}<br>

Name: sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26.tar.gz
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/aarch64-ostl-linux

Information about "Linux kernel package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=Linux kernel package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=Linux kernel package | request=path}}<br>

Name: linux-stm32mp-6.1.82-stm32mp-r2-r0
Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0

Information about "Linux kernel source" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=Linux kernel source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=Linux kernel source | request=path}}<br>

Name: linux-6.1.82.tar.xz
Path: linux-6.1.82

Information about "U-Boot package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=U-Boot package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=U-Boot package | request=path}}<br>

Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2022.10-stm32mp-r2-r0

Information about "U-Boot source" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=U-Boot source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=U-Boot source | request=path}}<br>

Name: u-boot-stm32mp-v2022.10-stm32mp-r2-r0.tar.xz
Path: u-boot-stm32mp-v2022.10-stm32mp-r2-r0

Information about "TF-A package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=TF-A package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=TF-A package | request=path}}<br>

Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-v2.8.15-stm32mp-r2-r0

Information about "TF-A source" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=TF-A source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=TF-A source | request=path}}<br>

Name: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0.tar.xz
Path: tf-a-stm32mp-v2.8.15-stm32mp-r2-r0

Information about "OP-TEE package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=OP-TEE package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=OP-TEE package | request=path}}<br>

Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0/
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/optee-os-stm32mp-3.19.0-stm32mp-r2-r0

Information about "OP-TEE source" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=OP-TEE source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=OP-TEE source  | request=path}}<br>

Name: optee-os-stm32mp-3.19.0-stm32mp-r2-r0.tar.xz
Path: optee-os-stm32mp-3.19.0-stm32mp-r2-r0

Information about "SCP firmware" for latest revision requested
Installation name: {{EcosystemRelease/Package | revision=latest | package=SCP firmware | request=inst name}}<br>
Name: {{EcosystemRelease/Package | revision=latest | package=SCP firmware | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=SCP firmware | request=path}}<br>

Installation name: scp-firmware-2.12-stm32mp-r1-r0(tbd)
Name: scp-firmware-2.12-stm32mp-r1-r0.tar.xz(tbd)
Path: scp-firmware-2.12-stm32mp-r1(tbd)

Information about "External DT" for latest revision requested
Installation name: {{EcosystemRelease/Package | revision=latest | package=External DT | request=inst name}}<br>
Name: {{EcosystemRelease/Package | revision=latest | package=External DT | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=External DT | request=path}}<br>

Installation name: unknown package
Name: unknown package
Path: unknown package

Information about "gcnano-driver package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=gcnano-driver package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=gcnano-driver package | request=path}}<br>

Name: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0/
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mpu-v24.06.26/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.15-stm32mp2-r1-r0

Information about "gcnano-driver source" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=gcnano-driver source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=gcnano-driver source | request=path}}<br>

Name: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0.tar.xz
Path: gcnano-driver-stm32mp-6.4.15-stm32mp1-r1-r0

Information about "STM32CubeMPU" for latest revision requested
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=STM32CubeMPU | device=MP2 | request=name}}<br>
Path (MP2): {{EcosystemRelease/Package | revision=latest | package=STM32CubeMPU | device=MP2 | request=path}}<br>

Name (MP2): en.stm32cubemp2-v1.0.0TBD.zip
Path (MP2): STM32CubeMP2-mainTBD

"STM32CubeMP1" temporarily kept for compatibility
Name (MP2): {{EcosystemRelease/Package | revision=latest | package=STM32CubeMP1 | device=MP2 | request=name}}<br>

Name (MP2): en.stm32cubemp2-v1.0.0TBD.zip

Information about "TF-M" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=TF-M| request=name}}<br>
Path: {{EcosystemRelease/Package | revision=latest | package=TF-M| request=path}}<br>

Name: NA
Path: NA

Information about "Debug symbol files" for latest revision requested
Path: {{EcosystemRelease/Package | revision=latest | package=Debug symbol files | request=path}}<br>

Path: stm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/images/stm32mp25(tbd)

Information about "Licenses package" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=Licenses package | request=name}}<br>
URL: [{{EcosystemRelease/Package | revision=latest | package=Licenses package | request=url}}]<br>

Name: LICENSES-world-openstlinux-weston-stm32mp1.tar.gz(tbd)
URL: [3]

Information about "OpenSTLinux distribution" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=OpenSTLinux distribution | request=name}}<br>
URL: [{{EcosystemRelease/Package | revision=latest | package=OpenSTLinux distribution | request=url}}]<br>

Name: openstlinux-6.1-yocto-mickledore-mpu-v24.06.26
URL: [4]

Information about "Buildroot distribution" for latest revision requested
Name: {{EcosystemRelease/Package | revision=latest | package=Buildroot distribution | request=name}}<br>
URL: [{{EcosystemRelease/Package | revision=latest | package=Buildroot distribution | request=url}}]<br>

Name: unknown package
URL: [unknown package]

2.3. Basic examples for v5.0.0 release[edit source]

You type You get
Information about "Images package" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=Images package | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=Images package | device =MP1 | request=name}}<br>
Name (MP2_A35_TD): {{EcosystemRelease/Package | revision=5.0.0 | package=Images package | device=MP2_A35_TD | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=Images package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=Images package | request=url}}]<br>

Name (default): en.FLASH-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (MP1): en.FLASH-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (MP2_A35_TD): unknown device
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/images/stm32mp1
URL: [NA]

Information about "SDK-x86 package" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 package | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 package | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 package | request=url}}]<br>

Name (default): en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (MP1): en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (MP2): unknown device
Path: NA
URL: [NA]

Information about "SDK-x86 installation script" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 installation script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 installation script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 installation script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 installation script | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 installation script | request=url}}]<br>

Name (default): st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.sh
Name (MP1): st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.sh
Name (MP2): unknown device
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk
URL: [NA]

Information about "SDK-x86 setup script" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 setup script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 setup script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 setup script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 setup script | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=SDK-x86 setup script | request=url}}]<br>

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP2): unknown device
Path: NA
URL: [NA]

"SDK package", "SDK installation script" and "SDK setup script" temporarily kept for compatibility
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK package | request=name}}<br>
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK installation script | request=name}}<br>
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK setup script | request=name}}<br>

Name (default): en.SDK-x86_64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (default): st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.sh
Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi

Information about "SDK-arm64 package" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 package | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 package | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 package | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 package | request=url}}]<br>

Name (default): en.SDK-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (MP1): en.SDK-aarch64-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Name (MP2): unknown device
Path: NA
URL: [NA]

Information about "SDK-arm64 installation script" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 installation script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 installation script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 installation script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 installation script | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 installation script | request=url}}]<br>

Name (default): st-image-weston-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.sh
Name (MP1): st-image-weston-openstlinux-weston-stm32mp1-aarch64-toolchain-4.2.1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.sh
Name (MP2): unknown device
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sdk
URL: [NA]

Information about "SDK-arm64 setup script" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 setup script | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 setup script | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 setup script | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 setup script | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=SDK-arm64 setup script | request=url}}]<br>

Name (default): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP1): environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
Name (MP2): unknown device
Path: NA
URL: [NA]

Information about "OpenSTLinux BSP package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux BSP package | request=url}}]<br>

Name: en.sources-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/
URL: [NA]

Information about "Linux kernel package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=Linux kernel package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=Linux kernel package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=Linux kernel package | request=url}}]<br>

Name: linux-stm32mp-6.1.28-stm32mp-r1-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.28-stm32mp-r1-r0
URL: [NA]

Information about "Linux kernel source" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=Linux kernel source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=Linux kernel source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=Linux kernel source | request=url}}]<br>

Name: linux-6.1.28.tar.xz
Path: linux-6.1.28
URL: [NA]

Information about "U-Boot package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=U-Boot package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=U-Boot package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=U-Boot package | request=url}}]<br>

Name: u-boot-stm32mp-v2022.10-stm32mp-r1-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-v2022.10-stm32mp-r1-r0
URL: [NA]

Information about "U-Boot source" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=U-Boot source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=U-Boot source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=U-Boot source | request=url}}]<br>

Name: u-boot-stm32mp-v2022.10-stm32mp-r1-r0.tar.xz
Path: u-boot-stm32mp-v2022.10-stm32mp-r1
URL: [NA]

Information about "TF-A package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=TF-A package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=TF-A package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=TF-A package | request=url}}]<br>

Name: tf-a-stm32mp-v2.8.6-stm32mp-r1-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-v2.8.6-stm32mp-r1-r0
URL: [NA]

Information about "TF-A source" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=TF-A source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=TF-A source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=TF-A source | request=url}}]<br>

Name: tf-a-stm32mp-v2.8.6-stm32mp-r1-r0.tar.xz
Path: tf-a-stm32mp-v2.8.6-stm32mp-r1
URL: [NA]

Information about "OP-TEE package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=OP-TEE package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=OP-TEE package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=OP-TEE package | request=url}}]<br>

Name: optee-os-stm32mp-3.19.0-stm32mp-r1-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/optee-os-stm32mp-3.19.0-stm32mp-r1-r0
URL: [NA]

Information about "OP-TEE source" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=OP-TEE source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=OP-TEE source  | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=OP-TEE source | request=url}}]<br>

Name: optee-os-stm32mp-3.19.0-stm32mp-r1-r0.tar.xz
Path: optee-os-stm32mp-3.19.0-stm32mp-r1
URL: [NA]

Information about "SCP firmware" for v5.0.0 revision requested
Installation name: {{EcosystemRelease/Package | revision=5.0.0 | package=SCP firmware | request=inst name}}<br>
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=SCP firmware | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=SCP firmware | request=path}}<br>

Installation name: unknown package
Name: unknown package
Path: unknown package

Information about "External DT" for v5.0.0 revision requested
Installation name: {{EcosystemRelease/Package | revision=5.0.0 | package=External DT | request=inst name}}<br>
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=External DT | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=External DT | request=path}}<br>

Installation name: unknown package
Name: unknown package
Path: unknown package

Information about "gcnano-driver package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=gcnano-driver package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=gcnano-driver package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=gcnano-driver package | request=url}}]<br>

Name: gcnano-driver-stm32mp-6.4.13-stm32mp-r1-r0
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/sources/arm-ostl-linux-gnueabi/gcnano-driver-stm32mp-6.4.13-stm32mp-r1-r0
URL: [NA]

Information about "gcnano-driver source" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=gcnano-driver source | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=gcnano-driver source | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=gcnano-driver source | request=url}}]<br>

Name: gcnano-driver-stm32mp-6.4.13-stm32mp-r1-r0.tar.xz
Path: gcnano-driver-6.4.13
URL: [NA]

Information about "STM32CubeMPU" for v5.0.0 revision requested
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMPU | request=name}}<br>
Name (MP1): {{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMPU | device=MP1 | request=name}}<br>
Name (MP2): {{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMPU | device=MP2 | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMPU | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMPU | request=url}}]<br>

Name (default): en.STM32Cube_FW_MP1_V1.6.0.zip
Name (MP1): en.STM32Cube_FW_MP1_V1.6.0.zip
Name (MP2): unknown device
Path: STM32Cube_FW_MP1_V1.6.0
URL: [NA]

"STM32CubeMP1" temporarily kept for compatibility
Name (default): {{EcosystemRelease/Package | revision=5.0.0 | package=STM32CubeMP1 | request=name}}<br>

Name (default): en.STM32Cube_FW_MP1_V1.6.0.zip

Information about "TF-M" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=TF-M| request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=TF-M| request=path}}<br>

Name: unknown package
Path: unknown package

Information about "Debug symbol files" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=Debug symbol files | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=Debug symbol files | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=Debug symbol files | request=url}}]<br>

Name: NA
Path: stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/images/stm32mp1
URL: [NA]

Information about "Licenses package" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=Licenses package | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=Licenses package | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=Licenses package | request=url}}]<br>

Name: LICENSES-world-openstlinux-weston-stm32mp1.tar.gz
Path: NA
URL: [5]

Information about "OpenSTLinux distribution" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux distribution | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux distribution | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=OpenSTLinux distribution | request=url}}]<br>

Name: openstlinux-6.1-yocto-mickledore-mp1-v23.06.21
Path: NA
URL: [6]

Information about "Buildroot distribution" for v5.0.0 revision requested
Name: {{EcosystemRelease/Package | revision=5.0.0 | package=Buildroot distribution | request=name}}<br>
Path: {{EcosystemRelease/Package | revision=5.0.0 | package=Buildroot distribution | request=path}}<br>
URL: [{{EcosystemRelease/Package | revision=5.0.0 | package=Buildroot distribution | request=url}}]<br>

Name: openstlinux-6.1-buildroot-2023.02-mp1-v23.06.21
Path: NA
URL: [7]

2.4. Basic examples for legacy release[edit source]

Currently, there is no legacy release in the scope of the v5 ecosystem release flow.

2.5. Basic examples for former releases[edit source]

Currently, there is no former release in the scope of the v5 ecosystem release flow.

3. More examples[edit source]

You type You get
Information about "Linux kernel package" for an unspecified revision requested
Name: {{EcosystemRelease/Package | package=Linux kernel package | request=name}}<br>
URL: [{{EcosystemRelease/Package | package=Linux kernel package | request=url}}]<br>
Path: {{EcosystemRelease/Package | package=Linux kernel package | request=path}}

Name: unknown revision
URL: [unknown revision]
Path: unknown revision

Information about "Linux kernel package" for an unknown revision requested
Name: {{EcosystemRelease/Package | revision=10.20.30 | package=Linux kernel package | request=name}}<br>
URL: [{{EcosystemRelease/Package | revision=10.20.30 | package=Linux kernel package | request=url}}]<br>
Path: {{EcosystemRelease/Package | revision=10.20.30 | package=Linux kernel package | request=path}}

Name: unknown revision
URL: [unknown revision]
Path: unknown revision

Unspecified package
Name: {{EcosystemRelease/Package | revision=latest | request=name}}<br>
URL: [{{EcosystemRelease/Package | revision=latest | request=url}}]<br>
Path: {{EcosystemRelease/Package | revision=latest | request=path}}

Name: unknown package
URL: [unknown package]
Path: unknown package

Unknown package
Name: {{EcosystemRelease/Package | revision=latest | package=not supported | request=name}}<br>
URL: [{{EcosystemRelease/Package | revision=latest | package=not supported | request=url}}]<br>
Path: {{EcosystemRelease/Package | revision=latest | package=not supported | request=path}}

Name: unknown package
URL: [unknown package]
Path: unknown package

Unspecified request
{{EcosystemRelease/Package | revision=latest | package=Linux kernel package}}

unknown request

Unknown request
{{EcosystemRelease/Package | revision=latest | package=Linux kernel package | request=not supported}}

unknown request

Check that there's no space before and after the text
BEFORE{{EcosystemRelease/Package | revision=latest | package=Linux kernel package | request=name}}AFTER<br>
BEFORE[{{EcosystemRelease/Package | revision=latest | package=Linux kernel package | request=url}}]AFTER<br>
BEFORE{{EcosystemRelease/Package | revision=latest | package=Linux kernel package | request=path}}AFTER

BEFORElinux-stm32mp-6.1.82-stm32mp-r2-r0AFTER
BEFORE[NA]AFTER
BEFOREstm32mp25-openstlinux-6.1-yocto-mickledore-mp2-v23.12.06/sources/arm-ostl-linux-gnueabi/linux-stm32mp-6.1.82-stm32mp-r2-r0AFTER

4. Code[edit source]

unknown request