"Width (Exif:Image width)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1118previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.SSTM32CubeIDE Edit Run Config.png +967 +STM32CubeIDE Import.png +602 +STM32CubeIDE M33 Project Build complete.png +1154 +STM32CubeIDE M33 Project Build.png +581 +STM32CubeIDE M33 project structure.png +581 +STM32CubeIDE Run configurations run.png +1225 +STM32CubeIDE Run configurations.png +396 +STM32CubeIDE Serial widget Stopped.png +315 +STM32CubeIDE Serial widget.png +196 +STM32CubeIDE Starter.png +775 +STM32CubeIDE debug without download debug as.png +384 +STM32CubeIDE import project.png +598 +STM32CubeIDE info.png +2451 +STM32CubeIDE prompt close active console.png +610 +STM32CubeIDE prompt.png +1285 +STM32CubeIDE run with download run as.png +387 +STM32CubeIDE serial preferred device.png +991 +STM32CubeIDE v1 13 Import.png +602 +STM32CubeIDE-MPU-logo.png +369 +STM32CubeMP1.png +532 +