"Width (Exif:Image width)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1117previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.NNO-init-3.png +560 +CCDTExeCreationCProject.png +563 +TThreadX application initialization.png +565 +CCDTExeCreationCProjectNext.png +569 +CDTExeCreationCProjectNextNext.png +569 +LLogical-analyser-example.png +570 +DDevice manager DFU driver not installed.png +571 +XX-LINUX-RT.png +575 +X-LINUX-AI.png +575 +X-LINUX-NFC.png +575 +X-LINUX-AWS.svg +575 +SSTM32CubeIDE M33 project structure.png +581 +STM32CubeIDE M33 Project Build.png +581 +OOSTL-SDK-Embed-External.png +582 +NNO-after-1.png +585 +EEM-after-2.png +586 +SSTM32 header.png +587 +EEM-before-2.png +587 +NNA-after-2.png +588 +AAdc calib kernel.png +588 +