"Width (Exif:Image width)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1117previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.FFirmware update states.png +432 +AAuthentication software overview.png +4349 +OOSTL-CA7-Menu.png +437 +OTP write command for OTP structure v2.png +438 +MMPUAzureRTOSOverview.png +4400 +SSTM32CubeMPU MW overview.png +4400 +XX-LINUX-QT-Expansion Package-logo.png +4400 +OOpenSTLinux BSP SW Overview.png +445 +TTFMPS-13-run-error.png +448 +SSTM32Cube MPU packages.png +4490 +DDeviceresources.png +450 +IImage classification logo.png +454 +OObject detection logo.png +454 +FFace recognition logo.png +454 +PPose estimation logo.png +454 +SSemantic segmentation logo.png +454 +BBackToNavigationTree button.png +461 +DDeep dive in STM32MPU embedded software.png +462 +OOSTL-install-Secu-Warning.png +463 +SSTM32MPU Expansion Package.png +471 +