"Width (Exif:Image width)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1118previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.OOP-TEE BSEC PTA.png +964 +OP-TEE Calibration.png +1053 +OP-TEE NVMEM TA.png +969 +OSTL-CA7-Menu.png +437 +OSTL-FIP-Prj-Structure.png +599 +OSTL-Linux-Prj-Structure.png +520 +OSTL-Project-Structure-Annotated.png +391 +OSTL-SDK-Embed-External.png +582 +OSTL-SDK-Install-Success.png +534 +OSTL-SDK-Menu.png +499 +OSTL-SDK-Mgr.png +833 +OSTL-SRC-Linux-DTMX-Build.png +1778 +OSTL-SRC-Linux-Deployment-DT.png +511 +OSTL-SRC-Linux-Deployment.png +861 +OSTL-Sdk-Install.png +1077 +OSTL-Src-Prj-Menu.png +685 +OSTL-install-Secu-Warning.png +463 +OTP write command for OTP structure v2.png +438 +Object detection application screenshot.png +800 +Object detection logo.png +454 +