"Height (Exif:Image length)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1118previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.EExample of required definitions for HID application 1.png +451 +SSampletree.png +452 +55.1.2.png +452 +SSysdig exemples.png +453 +LLaunch python tfl object detection.png +453 +Launch python tfl edgetpu image classification.png +453 +Launch cpp tfl face recognition.png +453 +Lvgl conf1.png +453 +Launch python onnx object detection.png +453 +IIDE ExampleConsole.png +454 +Image classification logo.png +454 +OObject detection logo.png +454 +FFace recognition logo.png +454 +PPose estimation logo.png +454 +SSemantic segmentation logo.png +454 +Sai configuration.png +455 +LLvgl configurations.png +455 +MMP1 ROM code wakeup.png +456 +RROMCodeOverviewWakeUp.png +458 +CCpp tfl face recognition dataflow.png +458 +