"Width (Exif:Image width)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1118previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.MMp15 dk main soundcard.png +840 +Mp15 ev main soundcard.png +840 +Multiple model benchmark mp1.png +750 +Multiple model benchmark mp2.png +750 +Myteamspace.jpg +1664 +NNA-after-1.png +554 +NA-after-2.png +588 +NA-before-1.png +621 +NA-before-2.png +621 +NA-before-3.png +599 +NA-init-1.png +1483 +NA-init-2.png +1194 +NA-init-3.png +515 +NA-init-4.png +1851 +NA-init-5.png +952 +NAND mapping.png +800 +NFC05A1 and STM32MP157F-DK2 dock.png +592 +NFC06A1 and STM32MP157F-DK2 dock.jpg +3770 +NO-after-1.png +585 +NO-after-2.png +593 +