"Height (Exif:Image length)" is a predefined property of type Number. This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage1118previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.CCubeProgrammer GUI Flashing 9.png +1020 +CubeProgrammer GUI Flashing 13.png +1021 +BBuild.png +1024 +CCubeProgrammer GUI Flashing 15.png +1024 +CubeProgrammer GUI Flashing 16.png +1025 +SSSP secret UI.png +1039 +Secret generation MP25.png +1040 +EEMMC Flash Completed.png +1041 +EMMC File Loading.png +1041 +BBackup memory file.png +1041 +PPayload interfacce MP25.png +1041 +EEMMC File Loading USB.png +1042 +EMMC Flash Completed USB.png +1042 +CCubeProgrammer eMMC Flashing 5.png +1042 +SSD-init-4.png +1045 +TTA-Project-Structure.png +1045 +PPrevas.png +105 +DDMA transfer.png +1054 +NNO-init-4.png +1057 +XX-LINUX-AWS-Connectivity.png +1057 +