The number of approved revisions in the page history This property is pre-deployed (also known as special property) and comes with additional administrative privileges but can be used just like any other user-defined property.Usage2452previous 202050100250500next 20Filter<p>The <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Property_page/Filter">search filter</a> allows the inclusion of <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Help:Query_expressions">query expressions</a> such as <code>~</code> or <code>!</code>. The selected <a target="_blank" rel="nofollow noreferrer noopener" class="external text" href="https://www.semantic-mediawiki.org/wiki/Query_engine">query engine</a> might also support case insensitive matching or other short expressions like:</p><ul><li><code>in:</code> result should include the term, e.g. '<code>in:Foo</code>'</li></ul><ul><li><code>not:</code> result should to not include the term, e.g. '<code>not:Bar</code>'</li></ul>Showing 20 pages using this property.SSTM32CubeIDE Build complete.png +1 +STM32CubeIDE Build.png +1 +STM32CubeIDE ConsoleButton.png +1 +STM32CubeIDE Debug Suspend.png +1 +STM32CubeIDE Debug conf numbered.png +2 +STM32CubeIDE Default.png +2 +STM32CubeIDE Edit Debug Config add edit.png +1 +STM32CubeIDE Edit Debug Config download false.png +1 +STM32CubeIDE Edit Debug Config start up.png +1 +STM32CubeIDE Edit Debug conf.png +1 +STM32CubeIDE Edit Run Config.png +1 +STM32CubeIDE Import.png +2 +STM32CubeIDE M33 Project Build complete.png +1 +STM32CubeIDE M33 Project Build.png +1 +STM32CubeIDE M33 project structure.png +1 +STM32CubeIDE Run configurations run.png +1 +STM32CubeIDE Run configurations.png +1 +STM32CubeIDE Serial widget Stopped.png +1 +STM32CubeIDE Serial widget.png +1 +STM32CubeIDE Starter.png +1 +