1. Overview[edit source]
This stage explains how to install the STM32CubeMP1 package.
2. Install STM32CubeMP1 package[edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
- Download [NA/en.stm32cube_fw_mp1_v1.6.0.zip en.stm32cube_fw_mp1_v1.6.0.zip] to the following directory:
$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v5.0.0/Developer-Package - Uncompress the archive file to get the STM32CubeMP1 Package
unzip en.stm32cube_fw_mp1_v1.6.0.zip
3. STM32CubeMP1 package structure[edit source]
The STM32CubeMP1 Package is located in your $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Developer-Package directory. It is named unknown revision:
unknown revision ├── Drivers │ ├── BSP BSP drivers for the supported STM32MP1 boards │ │ └── [...] │ ├── CMSIS │ │ └── [...] │ └── STM32MP1xx_HAL_Driver HAL drivers for the supported STM32MP1 devices │ └── [...] ├── _htmresc │ └── [...] ├── License.md ├── Middlewares │ └── [...] ├── package.xml ├── Projects │ ├── STM32CubeProjectsList.html List of examples and applications for STM32CubeMP1 package │ ├── STM32MP157C-DK2 Set of examples and applications → STM32MP15 Discovery kits │ │ └── [...] │ └── STM32MP157C-EV1 Set of examples and applications → STM32MP15 Evaluation boards │ └── [...] ├── Readme.md ├── Release_Notes.html Release note for STM32CubeMP1 package └── Utilities └── [...]