1. Overview[edit source]
This stage explains how to install the SDK.
The SDK for OpenSTLinux distribution provides a standalone cross-development toolchain and libraries tailored to the contents of the specific image flashed onto the board.
2. Host computer configuration[edit source]
2.1. Install extra packages[edit source]
Additional Ubuntu packages must be installed to perform basic development tasks, basic cross-compilation (via Developer Package) or more complex cross-compilation such as OpenEmbedded does (via Distribution Package):
- Packages required by OpenEmbedded/Yocto (details here):
sudo apt-get update sudo apt-get install gawk wget git git-lfs diffstat unzip texinfo gcc-multilib chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev pylint xterm bsdmainutils sudo apt-get install libssl-dev libgmp-dev libmpc-dev lz4 zstd
- Packages needed for some "Developer Package" use cases:
sudo apt-get install build-essential libncurses-dev libncurses5 libyaml-dev libssl-dev
- Package for repo (used to download the "Distribution Package" source code):
First set python3 as default: sudo apt install python-is-python3 Then follow the installation instructions described in repo.
- Useful tools:
sudo apt-get install coreutils bsdmainutils sed curl bc lrzsz corkscrew cvs subversion mercurial nfs-common nfs-kernel-server libarchive-zip-perl dos2unix texi2html libxml2-utils
2.2. Additional configurations[edit source]
Additional configurations have to be installed to support up to 16 partitions per MMC. By default, on Linux® systems, a maximum of 8 partitions are allowed on MMC. All Packages (Starter Package, ...) need more than 10 partitions for the storage device. In order to extend the number of partitions per device to 16, the following options must be added to modprobe:
echo 'options mmc_block perdev_minors=16' > /tmp/mmc_block.conf sudo mv /tmp/mmc_block.conf /etc/modprobe.d/mmc_block.conf
3. Download the SDK[edit source]
The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.
For ecosystem release v3.1.0 :
- Download the [unknown revision/unknown revision Developer Package SDK] into the following directory: $HOME/STM32MPU_workspace/tmp
- Uncompress the tarball file to get the SDK installation script
cd $HOME/STM32MPU_workspace/tmp
tar xvf unknown revision
For ecosystem release v3.0.0 :
- Download the [unknown revision/unknown revision Developer Package SDK] into the following directory: $HOME/STM32MPU_workspace/tmp
- Uncompress the tarball file to get the SDK installation script
cd $HOME/STM32MPU_workspace/tmp
tar xvf unknown revision
4. Run the SDK installation script[edit source]
For ecosystem release v3.1.0 :
- Create your STM32MP15 Developer Package SDK directory on your host computer
mkdir -p $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/SDK
- Change the permissions of the SDK installation script so that it is executable
chmod +x unknown revision/unknown revision
- Execute the SDK installation script
./unknown revision/unknown revision -d <working directory absolute path>/Developer-Package/SDK
- The following log is output when the installation is successful:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17 =========================================================================================================================== You are about to install the SDK to "/home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/SDK". Proceed [Y/n]? y Extracting SDK.........................................................................................................................................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script e.g. $ . /home/osboxes/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
For ecosystem release v3.0.0 :
- Create your STM32MP15 Developer Package SDK directory on your host computer
mkdir -p $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/SDK
- Change the permissions of the SDK installation script so that it is executable
chmod +x unknown revision/unknown revision
- Execute the SDK installation script
./unknown revision/unknown revision -d <working directory absolute path>/Developer-Package/SDK
- The following log is output when the installation is successful:
ST OpenSTLinux - Weston - (A Yocto Project Based Distro) SDK installer version 3.1-openstlinux-5.10-dunfell-mp1-21-03-31 ======================================================================================================================== Enter the target directory for SDK (default: $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/SDK): You are about to install the SDK to "$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package/SDK". Proceed [Y/n]? Y Extracting SDK......................................................................................................................................................................................................................done Setting it up...done SDK has been successfully set up and is ready to be used. Each time you wish to use the SDK in a new shell session, you need to source the environment setup script for example $ . /home/osboxes/MCD/DV3.0/Dev/SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
5. Start the SDK up[edit source]
For ecosystem release v3.1.0 :
cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package source SDK/unknown revision
The following checks ensure that the environment is correctly set up:
- Check the target architecture
echo $ARCH arm
- Check the toolchain binary prefix for the target tools
echo $CROSS_COMPILE arm-ostl-linux-gnueabi-
- Check the C compiler version
$CC --version arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 Copyright (C) 2019 Free Software Foundation, Inc. This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
echo $OECORE_SDK_VERSION
- Check that the SDK version is the expected one
3.1.11-unknown revision
If any of these commands fails or does not return the expected result, try to reinstall the SDK.
For ecosystem release v3.0.0 :
cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Developer-Package source SDK/unknown revision
The following checks ensure that the environment is correctly set up:
- Check the target architecture
echo $ARCH arm
- Check the toolchain binary prefix for the target tools
echo $CROSS_COMPILE arm-ostl-linux-gnueabi-
- Check the C compiler version
$CC --version arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0 Copyright (C) 2019 Free Software Foundation, Inc. This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
- Check that the SDK version is the expected one
echo $OECORE_SDK_VERSION 3.1-unknown revision
If any of these commands fails or does not return the expected result, try to reinstall the SDK.