Components

1. Usage[edit source]

The EcosystemRelease/Components template returns the version of all software components delivered by an ecosystem release revision of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...).

Usage: {{EcosystemRelease/Components | revision=<revision>}}

Where:

  • <revision> is the mandatory revision of the ecosystem release, for which the version of all software components is requested.

The returned value is:

  • a string that contains the version of all the software components delivered by the ecosystem release revision, in a form that is usable by a tooltip.
  • "unknown revision", if <revision> is not supported.

This template relies on the EcosystemRelease/Component template.

2. Basic examples[edit source]

You type You get
Components version for vx.0.0 revision requested
{{EcosystemRelease/Components | revision=x.0.0}}

Main software components: Linux kernel vx.y (example) U-Boot vx.y (example) TF-A vx.y (example) OP-TEE vx.y (example) STM32CubeMP1 Package vx.y (example) OpenEmbedded vx.y (example)

Components version for v3.0.0 revision requested
{{EcosystemRelease/Components | revision=3.0.0}}

Main software components: Linux kernel v5.10-stm32mp-r1 (v5.10.10) U-Boot v2020.10-stm32mp-r1 TF-A v2.4-stm32mp-r1 OP-TEE v3.12.0-stm32mp-r1 STM32CubeMP1 Package v1.4.0 OpenEmbedded v3.1.5 (Dunfell)

Components version for v3.1.0 revision requested
{{EcosystemRelease/Components | revision=3.1.0}}

Main software components: Linux kernel v5.10-stm32mp-r2 (v5.10.61) U-Boot v2020.10-stm32mp-r2 TF-A v2.4-stm32mp-r2 OP-TEE v3.12.0-stm32mp-r2 STM32CubeMP1 Package v1.5.0 OpenEmbedded v3.1.11 (Dunfell)

Components version for v3.1.0.ALPHA revision requested
{{EcosystemRelease/Components | revision=3.1.0.ALPHA }}

Main software components: Linux kernel v5.10-stm32mp13-r4 (v5.10.61) U-Boot v2020.10-stm32mp13-r4 TF-A v2.4-stm32mp13-r3 OP-TEE v3.12.0-stm32mp13-r3 OpenEmbedded v3.1.11 (Dunfell)

3. More examples[edit source]

You type You get
Components version for vx.2.0 revision requested
{{EcosystemRelease/Components | revision=x.2.0}}

Main software components: Linux kernel vx.y (example) U-Boot vx.y (example) TF-A vx.y (example) OP-TEE vx.y (example) STM32CubeMP1 Package vx.y (example) OpenEmbedded vx.y (example) Android vx.y (example)

Components version for vx.1.0 revision requested
{{EcosystemRelease/Components | revision=x.1.0}}

Main software components: Linux kernel vx.y (example) U-Boot vx.y (example) TF-A vx.y (example) OP-TEE vx.y (example) STM32CubeMP1 Package vx.y (example) OpenEmbedded vx.y (example) Android vx.y (example)

Unspecified revision
{{EcosystemRelease/Components}}

Main software components: unknown revision

Unknown revision
{{EcosystemRelease/Components | revision=10.20.30}}

Main software components: unknown revision

4. Code[edit source]

Main software components: unknown revision

No categories assignedEdit