1. Article purpose[edit source]
The purpose of this article is to explain how to integrate the IKS01Ax expansion board with STM32MP157C-DK2, managed by Linux on Cortex®-A7.
The IKS01Ax boards are expansion boards that includes several motion MEMS like HTS221 and LSM6DSx.
Sensors available on IKS01A2 expansion board:
- LSM6DSL MEMS 3D accelerometer (±2/±4/±8/±16 g) and 3D gyroscope (±125/±245/±500/±1000/±2000 dps)
- LSM303AGR MEMS 3D accelerometer (±2/±4/±8/±16 g) and MEMS3D magnetometer (±50 gauss)
- LPS22HB MEMS pressure sensor, 260-1260 hPa absolute digital output barometer
- HTS221: capacitive digital relative humidity and temperature
Sensors available on IKS01A3 expansion board:
- LSM6DSO: MEMS 3D accelerometer (±2/±4/±8/±16 g) + 3D gyroscope (±125/±250/±500/±1000/±2000 dps)
- LIS2MDL: MEMS 3D magnetometer (±50 gauss)
- LIS2DW12: MEMS 3D accelerometer (±2/±4/±8/±16 g)
- LPS22HH: MEMS pressure sensor, 260-1260 hPa absolute digital output barometer
- HTS221: capacitive digital relative humidity and temperature
- STTS751: Temperature sensor (–40 °C to +125 °C)
This article provides step-by-step instructions to:
- configure Linux software to support IKS01A2 expansion board,
- activate/use several motion MEMS such as HTS221 and LSM6DSL.
2. Prerequisites[edit source]
2.1. Hardware prerequisites[edit source]
- STM32MP157C-DK2
For more information about the STM32 discovery board and how to start it up, jump to this section Getting_started/STM32MP1_boards/STM32MP157x-DK2
- IKS01A2 expansion board
2.2. Software prerequisites[edit source]
The STM32MP157C-DK2 board must be downloaded with appropriate software in order to support IKS01A2 expansion board. For proceeding, follow the step-by-step instructions provided at STM32MP157C-DK2 Let's start.
3. Software customization to support IKS01A2 expansion board[edit source]
The STM32MP157C-DK2 Linux software must be configured to activate the IKS01A2 board connected on top of the STM32MP157C-DK2 board.
The configuration consists in modifying the STM32MP157C-DK2 Linux kernel and managing some new device tree elements.
3.1. Kernel configuration[edit source]
By default, the motion MEMS drivers present on IKS01A2 expansion board are enabled in STM32MP1 kernel configuration: hts221, pressure(lp22hb) and lsm6dsl. The device tree must be updated to declare and activate them.
To check whether associated drivers are enabled inside the kernel, type the commands provided here below :
cat /proc/config.gz | gunzip | grep HTS221 CONFIG_HTS221=y CONFIG_HTS221_I2C=y CONFIG_HTS221_SPI=y
cat /proc/config.gz | gunzip | grep ST_PRESS CONFIG_IIO_ST_PRESS=m CONFIG_IIO_ST_PRESS_I2C=m CONFIG_IIO_ST_PRESS_SPI=m
cat /proc/config.gz | gunzip | grep ST_LSM6DS CONFIG_IIO_ST_LSM6DSX=m CONFIG_IIO_ST_LSM6DSX_I2C=m CONFIG_IIO_ST_LSM6DSX_SPI=m
3.2. Kernel device tree configuration[edit source]
3.2.1. Hardware / software interface[edit source]
The HTS221 and LSM6DSL motion MEMS present on IKS01A2 expansion board are involved in the following use case.
According to IKS01A2 user manual[1], both motion MEMS are controlled by I2C bus.
In the schematics of IKS01A2 [2] and STM32MP157C-DK2[3] presented below, the pins that are interconnected are highlighted.
- IKS01A2 schematic (Arduino connector) [2]
- Pins 10 and 9 of CN5 are used for I2C Bus (SDA and SCL) (I2C1 and I2C2 bus instances are mixed via JP7 and JP8 jumpers)
- Pins 6 and 5 of CN9 are used to manage interruptions on LSM6DSL motion MEMS (indicated for information: not used on kernel configuration).
- STM32MP157C-DK2 schematic (Arduino connector) [3]
- Pins 10 and 9 of CN5 are used for I2C Bus (I2C5_SDA and I2C5_SCL)
- Pins 6 and 5 of CN14 are used to manage interruptions on LSM6DSL motion MEMS (indicated for information: not used on kernel configuration)
3.2.2. Kernel device tree configuration[edit source]
As indicated in previous section, the IKS01A2 expansion board is controlled via I2C bus. On STM32MP157C-DK2, the associated I2C bus is I2C5.
The I2C5 bus must be activated into STM32MP157C-DK2 device tree and a node must be added for each hardware to be supported (see entries like hts221, as shown in the device tree content example below).
For that, add following content into stm32mp157c-dk2.dts file:
&i2c5 { status = "okay"; hts221@5f { compatible = "st,hts221"; reg = <0x5f>; }; lsm6dsl@6b { compatible = "st,lsm6dsl"; reg = <0x6b>; }; };
3.3. Activate the new configuration in the STM32MP157C-DK2 board[edit source]
- Prerequisites: The device tree and the Linux kernel must have been regenerated. If not done yet, follow the indications given in Modify, rebuild and reload the Linux® kernel
- Add the two generated files in the board file system, precisely in the bootfs partition (/boot directory)
ls -1 /boot/stm32*dk2* /boot/stm32mp157c-dk2-a7-examples.dtb /boot/stm32mp157c-dk2-iks01a2.dtb /boot/stm32mp157c-dk2-m4-examples.dtb /boot/stm32mp157c-dk2.dtb
- Add a new entry in stm32mp157c-dk2_extlinux.conf file located in /boot/mmc0_extlinux/. If the mmc0_<something> directory is not available, add the new entry in /boot/mmc0_extlinux/extlinux.conf.
# Generic Distro Configuration file generated by OpenEmbedded
menu title Select the boot mode
MENU BACKGROUND ../splash.bmp
TIMEOUT 20
DEFAULT stm32mp157c-dk2-iks01a2
LABEL OpenSTLinux
KERNEL /uImage
FDTDIR /
INITRD /uInitrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
LABEL stm32mp157c-dk2-a7-examples
KERNEL /uImage
FDT /stm32mp157c-dk2-a7-examples.dtb
INITRD /uInitrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
LABEL stm32mp157c-dk2-m4-examples
KERNEL /uImage
FDT /stm32mp157c-dk2-m4-examples.dtb
INITRD /uInitrd
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
LABEL stm32mp157c-dk2-iks01a2
KERNEL /uImage
FDT /stm32mp157c-dk2-iks01a2.dtb
APPEND root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200
- Reboot the board
3.4. Verify the new configuration on board[edit source]
- Verify if i2c5 is enabled:
cat /proc/device-tree/soc/i2c\@40015000/status okay
- Verify if the motion MEMS drivers are declared in the device tree node:
ls -l /proc/device-tree/soc/i2c\@40015000/
total 0 -r--r--r-- 1 root root 4 Feb 7 15:56 #address-cells -r--r--r-- 1 root root 4 Feb 7 15:56 #size-cells -r--r--r-- 1 root root 4 Feb 7 15:56 clock-frequency -r--r--r-- 1 root root 8 Feb 7 15:56 clocks -r--r--r-- 1 root root 17 Feb 7 15:56 compatible drwxr-xr-x 2 root root 0 Feb 7 15:51 hts221@5f -r--r--r-- 1 root root 4 Feb 7 15:56 i2c-scl-falling-time-ns -r--r--r-- 1 root root 4 Feb 7 15:56 i2c-scl-rising-time-ns -r--r--r-- 1 root root 12 Feb 7 15:56 interrupt-names -r--r--r-- 1 root root 28 Feb 7 15:56 interrupts-extended drwxr-xr-x 2 root root 0 Feb 7 15:51 lsm6dsl@6b -r--r--r-- 1 root root 4 Feb 7 15:56 name -r--r--r-- 1 root root 4 Feb 7 15:56 pinctrl-0 -r--r--r-- 1 root root 4 Feb 7 15:56 pinctrl-1 -r--r--r-- 1 root root 14 Feb 7 15:56 pinctrl-names -r--r--r-- 1 root root 4 Feb 7 15:56 power-domains -r--r--r-- 1 root root 8 Feb 7 15:56 reg -r--r--r-- 1 root root 8 Feb 7 15:56 resets -r--r--r-- 1 root root 12 Feb 7 15:56 st,syscfg-fmp -r--r--r-- 1 root root 5 Feb 7 15:56 status -r--r--r-- 1 root root 0 Feb 7 15:56 wakeup-source
- Verify if the motion MEMS drivers are correctly probed and if the system provides access to the associated hardware:
grep OF_NAME /sys/bus/iio/devices/iio\:device*/uevent /sys/bus/iio/devices/iio:device0/uevent:OF_NAME=hts221 /sys/bus/iio/devices/iio:device1/uevent:OF_NAME=lsm6dsl /sys/bus/iio/devices/iio:device2/uevent:OF_NAME=lsm6dsl
4. Read motion MEMS via bash script[edit source]
The goal of this section is to read the informations provided by the Linux kernel interface and to process it with a bash script.
4.1. List of sensor entries[edit source]
The IKS01A2 expansion board provides several MEMS like HTS221, LSM6DSL, LPS22HB.
The list of hardware MEMS detected by Linux via the IIO framework can be verified in the sysfs.
grep OF_NAME /sys/bus/iio/devices/iio\:device*/uevent /sys/bus/iio/devices/iio:device0/uevent:OF_NAME=hts221 /sys/bus/iio/devices/iio:device1/uevent:OF_NAME=lsm6dsl /sys/bus/iio/devices/iio:device2/uevent:OF_NAME=lsm6dsl
This list provides the association between entries and MEMS drivers. In the rest of the article, this list is used a as reference.
4.2. HTS221: Temperature/Humidity[edit source]
The HTS221 is a capacitive digital sensor for relative humidity and temperature.
In this example, hts221 entry is /sys/bus/iio/devices/iio:device0/. In case the user has a different setup, the entry should be adapted accordingly in the scripts provided hereafter.
4.2.1. Temperature[edit source]
- Read IIO entries associated to the temperature for HTS221 driver
cat /sys/bus/iio/devices/iio\:device0/in_temp_raw cat /sys/bus/iio/devices/iio\:device0/in_temp_offset cat /sys/bus/iio/devices/iio\:device0/in_temp_scale
- Calculate real temperature according with the following formula
Temperature = ( Raw value + Offset value) * Scale value)
- Calculate temperature by shell script : static IIO entries
Content of hts221_read_temperature_on_device0.sh:
#!/bin/sh
raw=`cat /sys/bus/iio/devices/iio\:device0/in_temp_raw`
offset=`cat /sys/bus/iio/devices/iio\:device0/in_temp_offset`
scale=`cat /sys/bus/iio/devices/iio\:device0/in_temp_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
temperature=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Temperature $temperature"
printf "Temperature %.01f\n" $temperature
- Calculate temperature by shell script: auto detection of IIO entries
Content of hts221_read_temperature_with_entry_detection.sh:
#!/bin/sh
DRIVER_NAME=hts221
for d in `ls -d1 /sys/bus/iio/devices/*device*`;
do
if grep -q $DRIVER_NAME $d/name ;
then
raw=`cat $d/in_temp_raw`
offset=`cat $d/in_temp_offset`
scale=`cat $d/in_temp_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
temperature=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Temperature $temperature"
printf "Temperature %.01f\n" $temperature
break;
fi
done
- Test on board
./hts221_read_temperature_on_device0.sh Value read: raw 563.000000 Value read: offset 1036.674817 Value read: scale 0.019172 Temperature 30.668765624 Temperature 30.7
4.2.2. Humidity[edit source]
- Read IIO entries associated to humidity for HTS221 driver
cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_raw cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_offset cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_scale
- Calculate real humidity according with the following formula
Humidity = ( Raw value + Offset value) * Scale value)
- Calculate humidity by shell script: static IIO entries
Content of hts221_read_humidity_on_device0.sh:
#!/bin/sh
raw=`cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_raw`
offset=`cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_offset`
scale=`cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
humidity=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Humidity $humidity"
printf "Humidity %.01f\n" $humidity
- Calculate humidity by shell script: auto detection of IIO entries
Content of hts221_read_humidity_with_entry_detection.sh:
#!/bin/sh
DRIVER_NAME=hts221
for d in `ls -d1 /sys/bus/iio/devices/*device*`;
do
if grep -q $DRIVER_NAME $d/name ;
then
raw=`cat $d/in_humidityrelative_raw`
offset=`cat $d/in_humidityrelative_offset`
scale=`cat $d/in_humidityrelative_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
humidity=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Humidity $humidity"
printf "Humidity %.01f\n" $humidity
break;
fi
done
- Test on board
./hts221_read_humidity_on_device0.sh Value read: raw 2669.000000 Value read: offset -10661.500000 Value read: scale -0.003000 Humidity 23.977500000 Humidity 24.0
4.3. LSM6DSL: accelerometer/gyroscope[edit source]
The LSM6DSL is an inertial measurement unit (IMU) with ultra-low power and high accuracy, for smartphones and battery operated IoT, gaming, wearables and consumer electronics.
In this example, lsm6dsl entries are /sys/bus/iio/devices/iio:device1/ and /sys/bus/iio/devices/iio:device2/.
The device2 entry is dedicated to accelerometer and the device1 one to gyroscope.
4.3.1. Accelerometer[edit source]
- Read IIO entries associated to accelerometer for LSM6DSL driver
cat /sys/bus/iio/devices/iio\:device2/in_accel_scale cat /sys/bus/iio/devices/iio\:device2/in_accel_x_raw cat /sys/bus/iio/devices/iio\:device2/in_accel_y_raw cat /sys/bus/iio/devices/iio\:device2/in_accel_z_raw
- Calculate accelerometer values according with the following formula
X = Raw value * scale value * (256.0 / 9.81) Y = Raw value * scale value * (256.0 / 9.81) Z = Raw value * scale value * (256.0 / 9.81)
- Calculate accelerometer value by shell script: static IIO entries
Content of lsm6dsl_accel_read_on_device2.sh:
#!/bin/sh
rscale=`cat /sys/bus/iio/devices/iio\:device2/in_accel_scale`
xraw=`cat /sys/bus/iio/devices/iio\:device2/in_accel_x_raw`
yraw=`cat /sys/bus/iio/devices/iio\:device2/in_accel_y_raw`
zraw=`cat /sys/bus/iio/devices/iio\:device2/in_accel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Accelerometer value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
- Calculate accelerometer value by shell script: auto detection of IIO entries
Content of lsm6dsl_accel_read_with_entry_detection.sh:
#!/bin/sh
DRIVER_NAME=lsm6dsl_accel
for d in `ls -d1 /sys/bus/iio/devices/*device*`;
do
if grep -q $DRIVER_NAME $d/name ;
then
rscale=`cat $d/in_accel_x_scale`
xraw=`cat $d/in_accel_x_raw`
yraw=`cat $d/in_accel_y_raw`
zraw=`cat $d/in_accel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Accelerometer value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
break;
fi
done
- Test on board
./lsm6dsl_accel_read_on_device2.sh Value read: X (raw/scale) 104 / 0.000598 Value read: Y (raw/scale) -16378 / 0.000598 Value read: Z (raw/scale) -1117 / 0.000598 Accelerometer value: [ 1.62, -255.53, -17.43 ]
4.3.2. Gyroscope[edit source]
- Read IIO entries associated to gyroscope for LSM6DSL driver
cat /sys/bus/iio/devices/iio\:device1/in_anglvel_scale cat /sys/bus/iio/devices/iio\:device1/in_anglvel_x_raw cat /sys/bus/iio/devices/iio\:device1/in_anglvel_y_raw cat /sys/bus/iio/devices/iio\:device1/in_anglvel_z_raw
- Calculate gyroscope values according following formula
X = Raw value * scale value * (256.0 / 9.81) Y = Raw value * scale value * (256.0 / 9.81) Z = Raw value * scale value * (256.0 / 9.81)
- Calculate gyroscope value by shell script: static IIO entries
Content of lsm6dsl_gyro_read_on_device1.sh:
#!/bin/sh
rscale=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_scale`
xraw=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_x_raw`
yraw=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_y_raw`
zraw=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Gyroscope value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
- Calculate gyroscope value by shell script: auto detection of IIO entries
Content of lsm6dsl_gyro_read_with_entry_detection.sh:
#!/bin/sh
DRIVER_NAME=lsm6dsl_gyro
for d in `ls -d1 /sys/bus/iio/devices/*device*`;
do
if grep -q $DRIVER_NAME $d/name ;
then
rscale=`cat $d/in_anglvel_scale`
xraw=`cat $d/in_anglvel_x_raw`
yraw=`cat $d/in_anglvel_y_raw`
zraw=`cat $d/in_anglvel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Gyroscope value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
break;
fi
done
- Test on board
./lsm6dsl_gyro_read_on_device1.sh Value read: X (raw/scale) -2293 / 0.000153 Value read: Y (raw/scale) 150 / 0.000153 Value read: Z (raw/scale) -111 / 0.000153 Gyroscope value: [ -9.15, 0.60, -0.44 ]
4.4. BASH: script with all the measurements[edit source]
- Content of iks01a2.sh
#!/bin/sh
echo "============================="
echo "=== HTS221 ==="
echo "=== (temperature) ==="
echo "============================="
raw=`cat /sys/bus/iio/devices/iio\:device0/in_temp_raw`
offset=`cat /sys/bus/iio/devices/iio\:device0/in_temp_offset`
scale=`cat /sys/bus/iio/devices/iio\:device0/in_temp_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
temperature=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Temperature $temperature"
printf "Temperature %.02f\n" $temperature
echo "============================="
echo "=== HTS221 ==="
echo "=== (humidity) ==="
echo "============================="
raw=`cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_raw`
offset=`cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_offset`
scale=`cat /sys/bus/iio/devices/iio\:device0/in_humidityrelative_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
humidity=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Humidity $humidity"
printf "Humidity %.02f\n" $humidity
echo "============================="
echo "=== LSM6DSL ==="
echo "=== (accelerometer) ==="
echo "============================="
rscale=`cat /sys/bus/iio/devices/iio\:device2/in_accel_scale`
xraw=`cat /sys/bus/iio/devices/iio\:device2/in_accel_x_raw`
yraw=`cat /sys/bus/iio/devices/iio\:device2/in_accel_y_raw`
zraw=`cat /sys/bus/iio/devices/iio\:device2/in_accel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Accelerometer value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
echo "============================="
echo "=== LSM6DSL ==="
echo "=== (gyroscope) ==="
echo "============================="
xscale=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_scale`
xraw=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_x_raw`
yraw=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_y_raw`
zraw=`cat /sys/bus/iio/devices/iio\:device1/in_anglvel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Gyroscope value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
- Content of iks01a2_with_auto_detection.sh
#!/bin/sh
for d in `ls -d1 /sys/bus/iio/devices/*device*`;
do
# for hts221: Temperature + Humidity
if grep -q hts221 $d/name ;
then
echo "============================="
echo "=== HTS221 ==="
echo "=== (temperature) ==="
echo "============================="
raw=`cat $d/in_temp_raw`
offset=`cat $d/in_temp_offset`
scale=`cat $d/in_temp_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
temperature=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Temperature $temperature"
printf "Temperature %.02f\n" $temperature
echo "============================="
echo "=== HTS221 ==="
echo "=== (humidity) ==="
echo "============================="
raw=`cat $d/in_humidityrelative_raw`
offset=`cat $d/in_humidityrelative_offset`
scale=`cat $d/in_humidityrelative_scale`
printf "Value read: raw %0f\n" $raw
printf "Value read: offset %0f\n" $offset
printf "Value read: scale %0f\n" $scale
humidity=`echo "scale=2;$raw*$scale + $offset*$scale" | bc`
echo "Humidity $humidity"
printf "Humidity %.02f\n" $humidity
fi
# for lsm6dsl: accelerometer
if grep -q lsm6dsl_accel $d/name ;
then
echo "============================="
echo "=== LSM6DSL ==="
echo "=== (accelerometer) ==="
echo "============================="
rscale=`cat $d/in_accel_scale`
xraw=`cat $d/in_accel_x_raw`
yraw=`cat $d/in_accel_y_raw`
zraw=`cat $d/in_accel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Accelerometer value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
fi
# for lsm6dsl: gyroscope
if grep -q lsm6dsl_gyro $d/name ;
then
echo "============================="
echo "=== LSM6DSL ==="
echo "=== (gyroscope) ==="
echo "============================="
rscale=`cat $d/in_anglvel_scale`
xraw=`cat $d/in_anglvel_x_raw`
yraw=`cat $d/in_anglvel_y_raw`
zraw=`cat $d/in_anglvel_z_raw`
printf "Value read: X (raw/scale) %d / %.06f \n" $xraw $rscale
printf "Value read: Y (raw/scale) %d / %.06f \n" $yraw $rscale
printf "Value read: Z (raw/scale) %d / %.06f \n" $zraw $rscale
factor=`echo "scale=2;256.0 / 9.81" | bc`
xval=`echo "scale=2;$xraw*$rscale*$factor" | bc`
yval=`echo "scale=2;$yraw*$rscale*$factor" | bc`
zval=`echo "scale=2;$zraw*$rscale*$factor" | bc`
printf "Gyroscope value: [ %.02f, %.02f, %.02f ]\n" $xval $yval $zval
fi
done
5. Read motion MEMS via Python script[edit source]
The goal of this section is to read the informations provided by Linux kernel interface and process it with a python script.
The python displays the calculated value through a graphic user interface.
5.1. Display a window with Python and weston/wayland[edit source]
#!/usr/bin/python3
import gi
gi.require_version('Gtk', '3.0')
from gi.repository import Gtk
from gi.repository import GObject
from gi.repository import Gdk
from gi.repository import GLib
from gi.repository import GdkPixbuf
import cairo
import random
import math
import os
from time import sleep, time
# -------------------------------------------------------------------
# -------------------------------------------------------------------
class MainUIWindow(Gtk.Window):
def __init__(self):
Gtk.Window.__init__(self, title="Sensor usage")
#self.set_decorated(False)
self.maximize()
self.screen_width = self.get_screen().get_width()
self.screen_height = self.get_screen().get_height()
self.set_default_size(self.screen_width, self.screen_height)
print("[DEBUG] screen size: %dx%d" % (self.screen_width, self.screen_height))
self.set_position(Gtk.WindowPosition.CENTER)
self.connect('destroy', Gtk.main_quit)
def destroy(self, widget, data=None):
Gtk.main_quit()
# -------------------------------------------------------------------
# -------------------------------------------------------------------
# Main
if __name__ == "__main__":
# add signal to catch CRTL+C
import signal
signal.signal(signal.SIGINT, signal.SIG_DFL)
win = MainUIWindow()
win.connect("delete-event", Gtk.main_quit)
win.show_all()
Gtk.main()
5.2. Read temperature[edit source]
Part of code for reading temperature with HTS221 driver:
def found_iio_device_with_name(data, name):
prefix = "/sys/bus/iio/devices/"
of_name = 'OF_NAME=' + name
try:
for filefolder in os.listdir(prefix):
with open(prefix + '/' + filefolder + '/uevent') as f:
for line in f:
if line.split('\n')[0] == of_name:
''' return directory which contains "data" '''
if os.path.exists(prefix + '/' + filefolder + '/' + data):
return (prefix + '/' + filefolder + '/')
except OSError:
pass
except Exception as exc:
pass
return None
prefix_path = found_iio_device_with_name("in_temp_raw", "hts221")
try:
with open(prefix_path + "in_temp_" + 'raw', 'r') as f:
raw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_temp_" + 'raw', exc)
raw = 0.0
try:
with open(prefix_path + "in_temp_" + 'scale', 'r') as f:
scale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_temp_" + 'scale', exc)
scale = 0.0
try:
with open(prefix_path + "in_temp_" + 'offset', 'r') as f:
offset = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_temp_" + 'offset', exc)
offset = 0.0
temp = (offset + raw) * scale
5.3. Read humidity[edit source]
Part of code for reading humidity with HTS221 driver:
def found_iio_device_with_name(data, name):
prefix = "/sys/bus/iio/devices/"
of_name = 'OF_NAME=' + name
try:
for filefolder in os.listdir(prefix):
with open(prefix + '/' + filefolder + '/uevent') as f:
for line in f:
if line.split('\n')[0] == of_name:
''' return directory which contains "data" '''
if os.path.exists(prefix + '/' + filefolder + '/' + data):
return (prefix + '/' + filefolder + '/')
except OSError:
pass
except Exception as exc:
pass
return None
prefix_path = found_iio_device_with_name("in_humidityrelative_raw", "hts221")
try:
with open(prefix_path + "in_humidityrelative_" + 'raw', 'r') as f:
raw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_humidityrelative_" + 'raw', exc)
raw = 0.0
try:
with open(prefix_path + "in_humidityrelative_" + 'scale', 'r') as f:
scale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_humidityrelative_" + 'scale', exc)
scale = 0.0
try:
with open(prefix_path + "in_humidityrelative_" + 'offset', 'r') as f:
offset = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_humidityrelative_" + 'offset', exc)
offset = 0.0
humidity = (offset + raw) * scale
5.4. Read accelerometer[edit source]
Part of code for reading accelerometer with LSM6DSL driver:
def found_iio_device_with_name(data, name):
prefix = "/sys/bus/iio/devices/"
of_name = 'OF_NAME=' + name
try:
for filefolder in os.listdir(prefix):
with open(prefix + '/' + filefolder + '/uevent') as f:
for line in f:
if line.split('\n')[0] == of_name:
''' return directory which contains "data" '''
if os.path.exists(prefix + '/' + filefolder + '/' + data):
return (prefix + '/' + filefolder + '/')
except OSError:
pass
except Exception as exc:
pass
return None
prefix_path = found_iio_device_with_name("in_accel_x_raw", "lsm6dsl")
try:
with open(prefix_path + "in_accel_" + 'x_raw', 'r') as f:
xraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'x_raw', exc)
xraw = 0.0
try:
with open(prefix_path + "in_accel_" + 'scale', 'r') as f:
rscale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'scale', exc)
rscale = 0.0
accel_x = int(xraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_accel_" + 'y_raw', 'r') as f:
yraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'y_raw', exc)
yraw = 0.0
accel_y = int(yraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_accel_" + 'z_raw', 'r') as f:
zraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'z_raw', exc)
zraw = 0.0
accel_z = int(zraw * rscale * 256.0 / 9.81)
5.5. Read gyroscope[edit source]
Part of code for reading gyroscope with LSM6DSL driver:
def found_iio_device_with_name(data, name):
prefix = "/sys/bus/iio/devices/"
of_name = 'OF_NAME=' + name
try:
for filefolder in os.listdir(prefix):
with open(prefix + '/' + filefolder + '/uevent') as f:
for line in f:
if line.split('\n')[0] == of_name:
''' return directory which contains "data" '''
if os.path.exists(prefix + '/' + filefolder + '/' + data):
return (prefix + '/' + filefolder + '/')
except OSError:
pass
except Exception as exc:
pass
return None
prefix_path = found_iio_device_with_name("in_anglvel_x_raw", "lsm6dsl")
try:
with open(prefix_path + "in_anglvel_" + 'scale', 'r') as f:
rscale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'scale', exc)
rscale = 0.0
try:
with open(prefix_path + "in_anglvel_" + 'x_raw', 'r') as f:
xraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'x_raw', exc)
xraw = 0.0
gyro_x = int(xraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_anglvel_" + 'y_raw', 'r') as f:
yraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'y_raw', exc)
yraw = 0.0
gyro_y = int(yraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_anglvel_" + 'z_raw', 'r') as f:
zraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'z_raw', exc)
zraw = 0.0
gyro_z = int(zraw * rscale * 256.0 / 9.81)
5.6. Full script with information displayed in a graphic user interface[edit source]
#!/usr/bin/python3
import gi
gi.require_version('Gtk', '3.0')
from gi.repository import Gtk
from gi.repository import GObject
from gi.repository import Gdk
from gi.repository import GLib
from gi.repository import GdkPixbuf
import cairo
import random
import math
import os
from time import sleep, time
# time between each sensor mesearuement (1s)
TIME_UPATE = 2000
class Sensors():
def __init__(self):
''' '''
self.sensor_dictionnary = {}
def found_iio_device_with_name(self, data, name):
prefix = "/sys/bus/iio/devices/"
of_name = 'OF_NAME=' + name
try:
for filefolder in os.listdir(prefix):
with open(prefix + '/' + filefolder + '/uevent') as f:
for line in f:
if line.split('\n')[0] == of_name:
''' return directory which contains "data" '''
if os.path.exists(prefix + '/' + filefolder + '/' + data):
return (prefix + '/' + filefolder + '/')
except OSError:
pass
except Exception as exc:
pass
return None
def found_all_sensor_path(self):
self.sensor_dictionnary['temperature'] = self.found_iio_device_with_name("in_temp_raw", "hts221")
self.sensor_dictionnary['humidity'] = self.found_iio_device_with_name("in_humidityrelative_raw", "hts221")
self.sensor_dictionnary['accelerometer'] = self.found_iio_device_with_name("in_accel_x_raw", "lsm6dsl")
self.sensor_dictionnary['gyroscope'] = self.found_iio_device_with_name("in_anglvel_x_raw", "lsm6dsl")
print("[DEBUG] temperature -> ", self.sensor_dictionnary['temperature'], "<")
print("[DEBUG] humidity -> ", self.sensor_dictionnary['humidity'], "<")
print("[DEBUG] accelerometer -> ", self.sensor_dictionnary['accelerometer'], "<")
print("[DEBUG] gyroscope -> ", self.sensor_dictionnary['gyroscope'], "<")
def temperature_read(self):
prefix_path = self.sensor_dictionnary['temperature']
try:
with open(prefix_path + "in_temp_" + 'raw', 'r') as f:
raw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_temp_" + 'raw', exc)
raw = 0.0
try:
with open(prefix_path + "in_temp_" + 'scale', 'r') as f:
scale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_temp_" + 'scale', exc)
scale = 0.0
try:
with open(prefix_path + "in_temp_" + 'offset', 'r') as f:
offset = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_temp_" + 'offset', exc)
offset = 0.0
return (offset + raw) * scale
def humidity_read(self):
prefix_path = self.sensor_dictionnary['humidity']
try:
with open(prefix_path + "in_humidityrelative_" + 'raw', 'r') as f:
raw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_humidityrelative_" + 'raw', exc)
raw = 0.0
try:
with open(prefix_path + "in_humidityrelative_" + 'scale', 'r') as f:
scale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_humidityrelative_" + 'scale', exc)
scale = 0.0
try:
with open(prefix_path + "in_humidityrelative_" + 'offset', 'r') as f:
offset = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_humidityrelative_" + 'offset', exc)
offset = 0.0
return (offset + raw) * scale
def accelerometer_read(self):
prefix_path = self.sensor_dictionnary['accelerometer']
try:
with open(prefix_path + "in_accel_" + 'scale', 'r') as f:
rscale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'scale', exc)
rscale = 0.0
try:
with open(prefix_path + "in_accel_" + 'x_raw', 'r') as f:
xraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'x_raw', exc)
xraw = 0.0
accel_x = int(xraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_accel_" + 'y_raw', 'r') as f:
yraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'y_raw', exc)
yraw = 0.0
accel_y = int(yraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_accel_" + 'z_raw', 'r') as f:
zraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_accel_" + 'z_raw', exc)
zraw = 0.0
accel_z = int(zraw * rscale * 256.0 / 9.81)
return [ accel_x, accel_y, accel_z]
def gyroscope_read(self):
prefix_path = self.sensor_dictionnary['gyroscope']
try:
with open(prefix_path + "in_anglvel_" + 'scale', 'r') as f:
rscale = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'scale', exc)
rscale = 0.0
try:
with open(prefix_path + "in_anglvel_" + 'x_raw', 'r') as f:
xraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'x_raw', exc)
xraw = 0.0
gyro_x = int(xraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_anglvel_" + 'y_raw', 'r') as f:
yraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'y_raw', exc)
yraw = 0.0
gyro_y = int(yraw * rscale * 256.0 / 9.81)
try:
with open(prefix_path + "in_anglvel_" + 'z_raw', 'r') as f:
zraw = float(f.read())
except Exception as exc:
print("[ERROR] read %s " % prefix_path + "in_anglvel_" + 'z_raw', exc)
zraw = 0.0
gyro_z = int(zraw * rscale * 256.0 / 9.81)
return [ gyro_x, gyro_y, gyro_z]
# -------------------------------------------------------------------
# -------------------------------------------------------------------
class MainUIWindow(Gtk.Window):
def __init__(self):
Gtk.Window.__init__(self, title="Sensor usage")
#self.set_decorated(False)
self.maximize()
self.screen_width = self.get_screen().get_width()
self.screen_height = self.get_screen().get_height()
self.set_default_size(self.screen_width, self.screen_height)
print("[DEBUG] screen size: %dx%d" % (self.screen_width, self.screen_height))
self.set_position(Gtk.WindowPosition.CENTER)
self.connect('destroy', Gtk.main_quit)
# search sensor interface
self.sensors = Sensors()
self.sensors.found_all_sensor_path()
sensor_box = Gtk.VBox(homogeneous=False, spacing=0)
# temperature
temp_label = Gtk.Label()
temp_label.set_markup("<span font_desc='LiberationSans 25'>Temperature</span>")
self.temp_value_label = Gtk.Label()
self.temp_value_label.set_markup("<span font_desc='LiberationSans 25'>--.-- °C</span>")
temp_box = Gtk.HBox(homogeneous=False, spacing=0)
temp_box.add(temp_label)
temp_box.add(self.temp_value_label)
sensor_box.add(temp_box)
# humidity
humidity_label = Gtk.Label()
humidity_label.set_markup("<span font_desc='LiberationSans 25'>Humidity</span>")
self.humidity_value_label = Gtk.Label()
self.humidity_value_label.set_markup("<span font_desc='LiberationSans 25'>--.-- %c</span>" % '%')
humidity_box = Gtk.HBox(homogeneous=False, spacing=0)
humidity_box.add(humidity_label)
humidity_box.add(self.humidity_value_label)
sensor_box.add(humidity_box)
# Accel
accel_label = Gtk.Label()
accel_label.set_markup("<span font_desc='LiberationSans 25'>Accelerometer</span>")
self.accel_value_label = Gtk.Label()
self.accel_value_label.set_markup("<span font_desc='LiberationSans 25'> [ --.--, --.--, --.--]</span>")
accel_box = Gtk.HBox(homogeneous=False, spacing=0)
accel_box.add(accel_label)
accel_box.add(self.accel_value_label)
sensor_box.add(accel_box)
# Gyroscope
gyro_label = Gtk.Label()
gyro_label.set_markup("<span font_desc='LiberationSans 25'>Gyroscope</span>")
self.gyro_value_label = Gtk.Label()
self.gyro_value_label.set_markup("<span font_desc='LiberationSans 25'> [ --.--, --.--, --.--]</span>")
gyro_box = Gtk.HBox(homogeneous=False, spacing=0)
gyro_box.add(gyro_label)
gyro_box.add(self.gyro_value_label)
sensor_box.add(gyro_box)
self.add(sensor_box)
# Add a timer callback to update
# this takes 2 args: (how often to update in millisec, the method to run)
GLib.timeout_add(TIME_UPATE, self.update_ui)
def destroy(self, widget, data=None):
Gtk.main_quit()
def update_ui(self, user_data):
# temperature
temp = self.sensors.temperature_read()
self.temp_value_label.set_markup("<span font_desc='LiberationSans 25'>%.02f °C</span>" % temp)
# humidity
hum = self.sensors.humidity_read()
self.humidity_value_label.set_markup("<span font_desc='LiberationSans 25'>%.02f %c</span>" % (hum, '%'))
# accel
accel = self.sensors.accelerometer_read()
self.accel_value_label.set_markup("<span font_desc='LiberationSans 25'>[ %.02f, %.02f, %.02f]</span>" % (accel[0], accel[1], accel[2]))
# gyro
gyro = self.sensors.gyroscope_read()
self.gyro_value_label.set_markup("<span font_desc='LiberationSans 25'>[ %.02f, %.02f, %.02f]</span>" % (gyro[0], gyro[1], gyro[2]))
# As this is a timeout function, return True so that it
# continues to get called
return True
# -------------------------------------------------------------------
# -------------------------------------------------------------------
# Main
if __name__ == "__main__":
# add signal to catch CRTL+C
import signal
signal.signal(signal.SIGINT, signal.SIG_DFL)
win = MainUIWindow()
win.connect("delete-event", Gtk.main_quit)
win.show_all()
Gtk.main()
- Screenshot showing the results in the graphic user interface
5.7. More screenshot examples with results displayed in a graphic user interface[edit source]
6. References[edit source]