1. Usage[edit source]
The EcosystemRelease template is used to indicate for which ecosystem release revision(s), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all ecosystem release revisions for which the entire article is valid.
It outputs a "standardized" string that might be used to name an article part.
Usage: {{EcosystemRelease | revision=<revision> | range =<range> | revision2=<revision2>}}
Where:
- <revision> is the mandatory ecosystem release revision for which the article part is valid.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- The optional <range> and <revision2> parameters allow to define a range of revisions.
- <range> is the optional range of the ecosystem release revisions for which the article part is valid. The possible values are:
- and before: the article part is valid only for the revision(s) less than or equal to <revision>
- and after: the article part is valid only for the revision(s) greater than or equal to <revision>
- to: the article part is only valid from <revision> to <revision2>
- <revision2> is the optional ecosystem release upper revision for which the article part is valid. If this parameter is set, <range> must be set to "to", and <revision> becomes the lower revision for which the article part is valid.
- If this parameter is not set, and <range> is set to "to", the article part is valid from <revision> to the latest revision.
If the mouse is left over a revision, a popup window shows, for that revision:
- the versions of the Linux kernel, U-Boot, TF-A and OP-TEE
- the version of the STM32Cube MPU Package
- the version of OpenEmbedded
- the version of Android
This information comes from the EcosystemRelease/Components template.
2. Basic examples[edit source]
You type | You get |
---|---|
A specific revision
{{EcosystemRelease | revision=1.0.0}} |
ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.0.0 |
Revisions that are lower than or equal to a revision
{{EcosystemRelease | revision=1.1.0 | range=and before}} |
ecosystem release ≤ <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.1.0 |
Revisions that are greater than or equal to a revision
{{EcosystemRelease | revision=1.1.0 | range=and after}} |
ecosystem release ≥ <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.1.0 |
Range of revisions
{{EcosystemRelease | revision=1.0.0 | range=to | revision2=1.1.0}} |
ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.0.0 |
3. More examples[edit source]
You type | You get |
---|---|
Another specific revision
{{EcosystemRelease | revision=1.1.0}} |
ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.1.0 |
Unspecified revision
{{EcosystemRelease}} |
ecosystem release unknown revision |
Unknown revision
{{EcosystemRelease | revision=0.0.1}} |
ecosystem release unknown revision |
Any revision2
{{EcosystemRelease | revision=1.1.0 | range=to}} |
ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.1.0 |
Unknown revision2
{{EcosystemRelease | revision=1.1.0 | range=to | revision2=10.20.30}} |
ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.1.0 |
Unknown range
{{EcosystemRelease | revision=1.1.0 | range=error}} |
ecosystem release <span title="Main software components:
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision
unknown revision">1.1.0 |
4. Code[edit source]
ecosystem release unknown revision