Last edited 5 years ago

UpdateNeededForNewBoard

1. Usage

The UpdateNeededForNewBoard template is used to tag either a file, an article, a template, a chapter or a sentence that needs to be updated when a new board is added in the wiki.

It doesn't put anything seen by the reader in the page: it is only a kind of "phantom" tag. To retrieve all the pages that contain this tag (and so that need to be updated because a new board is added in the wiki), it is enough to display the pages that links this template. Then, searching for "UpdateNeededForNewBoard" in each page gives all the places where updates are needed.

Usage:  {{UpdateNeededForNewBoard | <comment>}}

Where <comment> is the optional comment to help updating .

2. Basic examples

You type You get
Update needed for new board without comment
Here is the list of the supported boards:{{UpdateNeededForNewBoard}}
* B1
* B2

Here is the list of the supported boards:

  • B1
  • B2
Update needed for new board with comment
The camera sensor is connected the CN7 camera connector of the STM32MP157C-EV1 board.{{UpdateNeededForNewBoard|Point to the camera connector (if any) of the new board}}

The camera sensor is connected the CN7 camera connector of the STM32MP157C-EV1 board.

3. Code

No categories assignedEdit