Modify, rebuild and reload a firmware

Revision as of 19:33, 13 February 2019 by Registered User

Template:ArticleMainWriter Template:ArticleProposedVersion



1. Overview[edit source]

This stage will explain you how to modify, rebuild and reload a STM32MP1 Arm® Cortex®-M4 coprocessor firmware.

2. Open SW4STM32 IDE[edit source]

  • Open System Workbench for STM32 IDE
File:SW4STM32 workspace.png
SW4STM32 workspace

3. Disconnect the built in SW4STM32 serial device[edit source]

  • For convenience and as you already have a Linux console connected to the board using minicom, please disconnect the console serial device embedded inside System Workbench for STM32.
File:SW4STM32 workspace serial disconnect 1.png
SW4STM32 disconnect the serial device by clicking this item
File:SW4STM32 workspace serial disconnect 2.png
SW4STM32 disconnect the serial device by clicking this item
  • It will avoid the following repetitive pattern in your Linux console
root@stm32mp1:~# ifconfig; echo __END__:$?
eth0      Link encap:Ethernet  HWaddr 00:80:E1:42:45:69  
          inet addr:10.48.1.143  Bcast:10.48.3.255  Mask:255.255.252.0
          inet6 addr: fe80::280:e1ff:fe42:4569/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:37 errors:0 dropped:1 overruns:0 frame:0
          TX packets:26 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:5776 (5.6 KiB)  TX bytes:3146 (3.0 KiB)
          Interrupt:63 Base address:0xc000 

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          inet6 addr: ::1/128 Scope:Host
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:344 errors:0 dropped:0 overruns:0 frame:0
          TX packets:344 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:22880 (22.3 KiB)  TX bytes:22880 (22.3 KiB)

usb0      Link encap:Ethernet  HWaddr 4A:06:6C:16:19:EC  
          inet addr:192.168.7.2  Bcast:192.168.7.255  Mask:255.255.255.0
          inet6 addr: fe80::4806:6cff:fe16:19ec/64 Scope:Link
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:396 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:115397 (112.6 KiB)

__END__:0

4. Import an existing example in SW4STM32 IDE[edit source]

  • Open the import screen File > Import... and select Existing Project into Workspace
File:SW4STM32 import.png
SW4STM32 import screen
  • Browse and select OpenAMP_TTY_echo application example
  • If you are using STM32MP157C-DK2 Discovery kit
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo
  • If you are using STM32MP157x-EV1 Evaluation board
$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo
  • Click finish
  • The OpenAMP_TTY_echo project is open and you can browse inside using the left pan
File:SW4STM32 workspace project open.png
SW4STM32 workspace with project open

5. Build the firmware[edit source]

  • Click the build button (the little hammer in the toolbar)
  • If the following screen appear, click OK
File:SW4STM32 workspace project warning.png
SW4STM32 Warning: This board already exists
  • Build is finished with no error
File:SW4STM32 workspace project build finished.png
SW4STM32 build finished with no error

6. Upload the firmware[edit source]

  • If you are using STM32MP157C-DK2 Discovery kit
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • If you are using STM32MP157x-EV1 Evaluation board
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • Upload your firmware example into the board
 scp Debug/OpenAMP_TTY_echo.elf root@<board ip address>:/lib/firmware

7. Start the firmware[edit source]

  • Verify that no firmware is currently runnig
 cat /sys/class/remoteproc/remoteproc0/state
offline

If offline is displayed, that means that no firmware is currently running. If running is displayed, a firmware is currently running. You shoul then stop it using the following command

 echo stop > /sys/class/remoteproc/remoteproc0/state
  • Set the firmware name to be executed
 echo -n OpenAMP_TTY_echo.elf > /sys/class/remoteproc/remoteproc0/firmware
  • Start the firmware
 echo start > /sys/class/remoteproc/remoteproc0/state
  • Verify that the firmware is runnig
 cat /sys/class/remoteproc/remoteproc0/state
running

8. Test the firmware[edit source]

The OpenAMP_TTY_echo firmware do the following:

  • CPU2(CM4) initialize OPenAMP MW which initializes/configures IPCC peripheral through HAL and setup openamp-rpmsg framwork infrastructure
  • CPU2(CM4) creates 2 rpmsg channels for 2 virtual UART instance UART0 and UART1
  • CPU2(CM4) is waiting for messages from CPU1(CA7) on these both channels
  • When CPU2(CM4) receives a message on 1 Virtual UART instance/rpmsg channel, it sends the message back to CPU1(CA7) on the same Virtual UART instance


  • Initialize the ttyRPMSG0 configuration
 stty -onlcr -echo -F /dev/ttyRPMSG0
  • Read constantly the ttyRPMSG0 channels in background
 cat /dev/ttyRPMSG0 &
  • Send a message on one ttyRPMSG0 channel and recieve the echo on the same ttyRPMSG0 channel
 echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
  • You can perform the same steps with the ttyRPMSG1 channel


  • After playing a while you can stop the firmware
 echo stop > /sys/class/remoteproc/remoteproc0/state

9. Modify the firmware[edit source]

The original firmware example receive a message for the host on one channel end sent back the same message to the host on the same channel.
As this is not so obvious on which channel the message is received, we propose to modify the firmware in order to add an indication to know what is the channel that is receiving the message.
Please modify main.c original code as follow:

File:SW4STM32 workspace project modification.png
SW4STM32 main.c file modification
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {

    OPENAMP_check_for_message();

    /* USER CODE END WHILE */
    if (VirtUart0RxMsg) {
      VirtUart0RxMsg = RESET;
      VIRT_UART_Transmit(&huart1/*&huart0*/, VirtUart1ChannelBuffRx, VirtUart1ChannelRxSize);
    }

    if (VirtUart1RxMsg) {
      VirtUart1RxMsg = RESET;
      VIRT_UART_Transmit(&huart0/*&huart1*/, VirtUart1ChannelBuffRx, VirtUart1ChannelRxSize);
    }
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
  • Save your modifications

10. Rebuild, reload and test the modified firmware[edit source]

10.1. Rebuild[edit source]

  • Click the build button (the little hammer in the toolbar)
  • Wait the end of the build

10.2. Reload[edit source]

  • If you are using STM32MP157C-DK2 Discovery kit
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-DK2/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • If you are using STM32MP157x-EV1 Evaluation board
 cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Developer-Package/STM32Cube_FW_MP1_V1.0.0/Projects/STM32MP157C-EV1/Applications/OpenAMP/OpenAMP_TTY_echo/SW4STM32/OpenAMP_TTY_echo/
  • Upload your firmware example into the board
 scp Debug/OpenAMP_TTY_echo.elf root@<board ip address>:/lib/firmware

10.3. Start[edit source]

  • Verify that no firmware is currently runnig
 cat /sys/class/remoteproc/remoteproc0/state
offline

If offline is displayed, that means that no firmware is currently running. If running is displayed, a firmware is currently running. You shoul then stop it using the following command

 echo stop > /sys/class/remoteproc/remoteproc0/state
  • Set the firmware name to be executed
 echo -n OpenAMP_TTY_echo.elf > /sys/class/remoteproc/remoteproc0/firmware
  • Start the firmware
 echo start > /sys/class/remoteproc/remoteproc0/state
  • Verify that the firmware is runnig
 cat /sys/class/remoteproc/remoteproc0/state
running

10.4. Test[edit source]

  • Initialize the ttyRPMSG0 configuration
 stty -onlcr -echo -F /dev/ttyRPMSG0
  • Read constantly the ttyRPMSG1 channels in background
 cat /dev/ttyRPMSG1 &
  • Send a message on one ttyRPMSG0 channel and recieve the echo on the same ttyRPMSG1 channel
 echo "Hello Virtual UART0" > /dev/ttyRPMSG0
Hello Virtual UART0
  • You can perform the same steps by inverting ttyRPMSG0 and ttyRPMSG1 channel


  • After playing a while you can stop the firmware
 echo stop > /sys/class/remoteproc/remoteproc0/state